![]() |
![]() |
RF_ratCompare parameter structure. More...
#include <RF.h>
Data Fields | |
RF_RatCallback | callback |
Callback function to be invoked upon a capture event (optional). More... | |
RF_RatHandle | channel |
RF_RatHandle identifies the channel to be allocated. More... | |
uint32_t | timeout |
RF_ratCompare parameter structure.
RF_RatCompare parameters are used with the RF_ratCompare() call.
RF_RatCallback RF_RatConfigCompare::callback |
Callback function to be invoked upon a capture event (optional).
RF_RatHandle RF_RatConfigCompare::channel |
RF_RatHandle identifies the channel to be allocated.
uint32_t RF_RatConfigCompare::timeout |
Timeout value in RAT ticks to be programmed in the timer as the trigger of compare event.