Kernel Configuration¶
A TI-RTOS application configures the TI-RTOS kernel using a configuration
(.cfg
file) that is found within the project. In IAR and
CCS projects, this file is found in the application project workspace
under the TOOLS
folder.
The configuration is accomplished by selectively including or using
RTSC modules available to the kernel. To use a module, the .cfg
calls xdc.useModule()
after which it can set various options as defined in
the TI-RTOS Kernel User Guide.
Some of the option that can be configured in the .cfg
file include but are
not limited to:
- Boot options
- Number of Hwi, Swi, and Task priorities
- Exception and Error handling
- The duration of a System tick (the most fundamental unit of time in the TI-RTOS kernel).
- Defining the application’s entry point and interrupt vector
- TI-RTOS heaps and stacks
- Including pre-compiled kernel and TI-RTOS driver libraries
- System providers (for
System_printf()
)
Whenever a change in the .cfg
file is made, you will rerun the XDCTools’
configuro
tool. This step is already handled for you as a pre-build step in
the provided IAR and CCS examples.
For the CC2640R2, a TI-RTOS kernel exists in ROM. Typically for flash
footprint savings, the .cfg
will include the kernel’s ROM module as
shown in Listing 1.
/* ================ ROM configuration ================ */
/*
* To use BIOS in flash, comment out the code block below.
*/
var ROM = xdc.useModule('ti.sysbios.rom.ROM');
if (Program.cpu.deviceName.match(/CC26X2/)) {
ROM.romName = ROM.CC26X2;
}
else if (Program.cpu.deviceName.match(/CC13X2/)) {
ROM.romName = ROM.CC13X2;
}
The TI-RTOS kernel in ROM is optimized for performance. If additional instrumentation is required in your application (typically for debugging), you must include the TI-RTOS kernel in flash which will increase flash memory consumption. Shown below is a short list of requirements to use the TI-RTOS kernel in ROM.
BIOS.assertsEnabled
must be set tofalse
BIOS.logsEnabled
must be set tofalse
BIOS.taskEnabled
must be set totrue
BIOS.swiEnabled
must be set totrue
BIOS.runtimeCreatesEnabled
must be set totrue
- BIOS must use the
ti.sysbios.gates.GateMutex
module Clock.tickSource
must be set toClock.TickSource_TIMER
Semaphore.supportsPriority
must befalse
- Swi, Task, and Hwi hooks are not permitted
- Swi, Task, and Hwi name instances are not permitted
- Task stack checking is disabled
Hwi.disablePriority
must be set to0x20
Hwi.dispatcherAutoNestingSupport
must be set to true
For additional documentation in regards to the list described above, see the TI-RTOS Kernel User Guide.
Creating vs. Constructing¶
Most TI-RTOS modules commonly have _create()
and _construct()
APIs to
initialize primitive instances. The main runtime differences between the
two APIs are memory allocation and error handling.
Create APIs perform a memory allocation from the default TI-RTOS heap before initialization. As a result, the application must check the return value for a valid handle before continuing.
1 2 3 4 5 6 7 8 9 10 | Semaphore_Handle sem;
Semaphore_Params semParams;
Semaphore_Params_init(&semParams);
sem = Semaphore_create(0, &semParams, NULL); /* Memory allocated in here */
if (sem == NULL) /* Check if the handle is valid */
{
System_abort("Semaphore could not be created");
}
|
Construct APIs are given a data structure with which to store the instance’s variables. As the memory has been pre-allocated for the instance, error checking may not be required after constructing.
1 2 3 4 5 6 7 8 9 | Semaphore_Handle sem;
Semaphore_Params semParams;
Semaphore_Struct structSem; /* Memory allocated at build time */
Semaphore_Params_init(&semParams);
Semaphore_construct(&structSem, 0, &semParams);
/* It's optional to store the handle */
sem = Semaphore_handle(&structSem);
|