Creating a Voice Enabled Application¶
“Voice” in this section means “voice quality audio” or any sound with a similar bandwidth. Voice can be compressed into a data stream that can easily be transmitted over a low-bandwidth radio protocol. TI offers a voice solution based on sampling a Pulse Density Modulation (PDM) microphone.
This section aims to describe the firmware that implements the TI voice solution.
In addition to voice solution provided by the SDK, experimental development is also being done on TI’s SimpleLink Github Page in the following areas:
- LaunchPad based voice receiver (simple_central_audio_receiver on the ble_examples-2.2 branch)
- Includes additional compression methods such as mSBC
- External Codec support for line in/analog mic
- Voice over HID-over-GATT-Profile receiver Python script (voice.py on the simplelink_sdk-1.40 branch)
- Captures voice frames via HID reports
Note
Currently the ble_examples
repo contains sample applications in various
development branches. Check back often for examples using other wireless
technologies, or improvements to the BLE examples.
Table of contents