![]() |
![]() |
TI BLE5-Stack API Documentation
1.01.12.00
|
Macros | |
#define | OAD_IMG_TYPE_APP 1 |
#define | OAD_IMG_TYPE_APP_STACK 3 |
#define | OAD_IMG_TYPE_APPSTACKLIB 7 |
#define | OAD_IMG_TYPE_BIM 6 |
#define | OAD_IMG_TYPE_FACTORY 5 |
#define | OAD_IMG_TYPE_HOST_BEGIN 32 |
#define | OAD_IMG_TYPE_HOST_END 63 |
#define | OAD_IMG_TYPE_NP 4 |
#define | OAD_IMG_TYPE_PERSISTENT_APP 0 |
#define | OAD_IMG_TYPE_RSVD_BEGIN 64 |
#define | OAD_IMG_TYPE_RSVD_END 255 |
#define | OAD_IMG_TYPE_STACK 2 |
#define | OAD_IMG_TYPE_USR_BEGIN 16 |
#define | OAD_IMG_TYPE_USR_END 31 |
#define OAD_IMG_TYPE_APP 1 |
OAD user application image
A user application of split app/stack type
#define OAD_IMG_TYPE_APP_STACK 3 |
OAD app + stack merge
An OAD enabled image that is a merge of both app and stack that are of split image type.
#define OAD_IMG_TYPE_APPSTACKLIB 7 |
OAD app + stack library image
An OAD enabled executable where the app and stack are built and linked together as one image.
#define OAD_IMG_TYPE_BIM 6 |
OAD Boot Image Manager (BIM) image
A BIM image
#define OAD_IMG_TYPE_FACTORY 5 |
OAD network processor image
A network processor image. This image is intended to run an external processor
#define OAD_IMG_TYPE_HOST_BEGIN 32 |
OAD Host image type begin
An image for a host processor
#define OAD_IMG_TYPE_HOST_END 63 |
OAD Host image type end
An image for a host processor
#define OAD_IMG_TYPE_NP 4 |
OAD network processor image
A network processor image. This image is intended to run an external processor
#define OAD_IMG_TYPE_PERSISTENT_APP 0 |
OAD on-chip persistent application image
The persistent app is the permanently resident app used in on-chip OAD The persistent app is responsible for updating the user application
#define OAD_IMG_TYPE_RSVD_BEGIN 64 |
OAD reserved image type begin
#define OAD_IMG_TYPE_RSVD_END 255 |
OAD reserved image type end
#define OAD_IMG_TYPE_STACK 2 |
OAD stack image
An OAD enabled stack image of split image type
#define OAD_IMG_TYPE_USR_BEGIN 16 |
OAD User defined image type begin
This is the beginning of the range of image types reserved for the user. OAD applications will not attempt to use or load images with this type
#define OAD_IMG_TYPE_USR_END 31 |
OAD User defined image type end
This is the end of the range of image types reserved for the user. OAD applications will not attempt to use or load images with this type