CC26xx Driver Library
aon_event.c File Reference
#include "aon_event.h"

Functions

void AONEventMcuWakeUpSet (uint32_t ui32MCUWUEvent, uint32_t ui32EventSrc)
 Select event source for the specified MCU wake-up programmable event. More...
 
uint32_t AONEventMcuWakeUpGet (uint32_t ui32MCUWUEvent)
 Get event source for the specified MCU wake-up programmable event. More...
 
void AONEventAuxWakeUpSet (uint32_t ui32AUXWUEvent, uint32_t ui32EventSrc)
 Select event source for the specified AUX wake-up programmable event. More...
 
uint32_t AONEventAuxWakeUpGet (uint32_t ui32AUXWUEvent)
 Get event source for the specified AUX wake-up programmable event. More...
 
void AONEventMcuSet (uint32_t ui32MCUEvent, uint32_t ui32EventSrc)
 Select event source for the specified programmable event forwarded to the MCU event fabric. More...
 
uint32_t AONEventMcuGet (uint32_t ui32MCUEvent)
 Get source for the specified programmable event forwarded to the MCU event fabric. More...