TI BLE-Stack for Bluetooth API Documentation
3.03.05.00
|
Modules | |
Micro GAP Broadcaster Callbacks | |
Micro GAP Broadcaster Structures | |
Micro GAP Constants | |
Micro GAP Monitor Callbacks | |
Micro GAP Monitor Structures | |
Files | |
file | ugap.h |
Micro BLE GAP API. | |
Functions | |
bStatus_t | ugap_bcastInit (ugapBcastCBs_t *pCBs) |
Initialize Micro Broadcaster. More... | |
bStatus_t | ugap_bcastSetDuty (uint16 dutyOnTime, uint16 dutyOffTime) |
Set Broadcaster Duty On/Off time. More... | |
bStatus_t | ugap_bcastStart (uint16 numAdvEvent) |
Start Broadcaster. Proceed the state from either Initialized or IDLE to Advertising. More... | |
bStatus_t | ugap_bcastStop (void) |
Stop Broadcaster. Proceed the state from either Advertising or Waiting to IDLE. More... | |
bStatus_t | ugap_monitorInit (ugapMonitorCBs_t *pCBs) |
Initialize Micro Monitor. More... | |
bStatus_t | ugap_monitorRequest (uint8_t channel, uint32_t accessAddr, uint32_t startTime, uint16_t duration, uint32_t crcInit) |
uGAP monitor request More... | |
bStatus_t | ugap_monitorStart (void) |
Start Monitor scanning. Proceed the state from either Initialized or Idle to Monitoring. More... | |
bStatus_t | ugap_monitorStop (void) |
Stop Monitor scanning. Proceed the state from Monitoring to Idle. More... | |
bStatus_t ugap_bcastInit | ( | ugapBcastCBs_t * | pCBs | ) |
Initialize Micro Broadcaster.
pCBs | - a set of application callbacks for Broadcaster |
bStatus_t ugap_bcastSetDuty | ( | uint16 | dutyOnTime, |
uint16 | dutyOffTime | ||
) |
Set Broadcaster Duty On/Off time.
dutyOnTime | - Time period during which the Broadcaster is in Advertising state. 100 ms unit. This cannot be 0 unless dutyOffTime is also 0. |
dutyOffTime | - Time period during which the Broadcaster is in Waiting state. 100 ms unit. If this is 0, Duty Control is disabled regardless of dutyOnTime. |
bStatus_t ugap_bcastStart | ( | uint16 | numAdvEvent | ) |
Start Broadcaster. Proceed the state from either Initialized or IDLE to Advertising.
numAdvEvent | - # of Advertising events to be performed before the Broadcaster state goes to IDLE. If this is 0, the Broadcaster will keep staying in Advertising or Advertising and Waiting alternately unless an error happens or the application requests to stop. |
bStatus_t ugap_bcastStop | ( | void | ) |
Stop Broadcaster. Proceed the state from either Advertising or Waiting to IDLE.
bStatus_t ugap_monitorInit | ( | ugapMonitorCBs_t * | pCBs | ) |
Initialize Micro Monitor.
pCBs | - a set of application callbacks for Monitor |
bStatus_t ugap_monitorRequest | ( | uint8_t | channel, |
uint32_t | accessAddr, | ||
uint32_t | startTime, | ||
uint16_t | duration, | ||
uint32_t | crcInit | ||
) |
uGAP monitor request
channel | - Channels to monitor. |
accessAddr | - Access address. 0xFFFFFFFF is used as a wildcard access address. An error status will be returned if the channel is one of 37, 38, or 39 but the accessAddr is not 0x8E89BED6. |
startTime | - Absolute start time in RAT ticks. |
duration | - Scan window per scanChanIndexchanIndex. A monitor complete time-out statuscallback will be sent to the application. A zero indicates a continuous scan. Unit in 0.625 ms; range from 2.5 ms to 40.959375 s. |
crcInit | - crcInit value for this connection |
bStatus_t ugap_monitorStart | ( | void | ) |