TI BLE-Stack for Bluetooth API Documentation  3.03.02.00
Modules | Files | Data Structures | Macros | Typedefs | Enumerations | Functions
RTLS_CTRL

This module implements Real Time Localization System (RTLS) Control module. More...

Modules

 RTLS Control Structures
 

Files

file  rtls_ble.h
 Stack specific BLE structures needed for RTLS Control.
 
file  rtls_ctrl.h
 RTLS Control module interface.
 
file  rtls_ctrl.h
 RTLS Control module interface.
 
file  rtls_ctrl_api.h
 This file contains the RTLS Control API's.
 
file  rtls_ctrl_tof.h
 This file contains the functions and structures specific to ToF post processing.
 
file  rtls_host.h
 This file contains the host abstraction layer for a RTLS Host.
 

Data Structures

struct  rtlsConfiguration_t
 RTLS Configuration structure. More...
 
struct  rtlsCtrlReq_t
 RTLS Control request. More...
 
struct  rtlsPacket_t
 RTLS Packet - Generic structure that will be translated to a specific command. More...
 

Macros

#define CHIP_ID_ADDR   ((uint8_t *)(0x50001000 + 0x2E8))
 Chip Identifier Address.
 
#define CHIP_ID_SIZE   6
 Chip Identifier Size.
 
#define HAL_ASSERT_CAUSE_OUT_OF_MEMORY   0x04
 RTLS Assert Error code.
 
#define MAX_SAMPLES_SINGLE_CHUNK   32
 Max number of samples reported in a single chunk when using RAW mode.
 
#define MAX_TOF_SAMPLES_SINGLE_CHUNK   16
 Max Num of Samples.
 
#define RTLS_CMD_AOA_ENABLE   0x14
 RTLS Node Manager command.
 
#define RTLS_CMD_AOA_RESULT_ANGLE   0x23
 RTLS Node Manager command.
 
#define RTLS_CMD_AOA_RESULT_PAIR_ANGLES   0x25
 RTLS Node Manager command.
 
#define RTLS_CMD_AOA_RESULT_RAW   0x24
 RTLS Node Manager command.
 
#define RTLS_CMD_AOA_SET_PARAMS   0x13
 RTLS Node Manager command.
 
#define RTLS_CMD_CONN_INFO   0x27
 RTLS Node Manager command.
 
#define RTLS_CMD_CONN_PARAMS   0x02
 RTLS Node Manager command.
 
#define RTLS_CMD_CONNECT   0x03
 RTLS Node Manager command.
 
#define RTLS_CMD_GET_RTLS_PARAM   0x29
 RTLS Node Manager command.
 
#define RTLS_CMD_IDENTIFY   0x00
 RTLS Node Manager command.
 
#define RTLS_CMD_RESERVED   0x01
 RTLS Node Manager command.
 
#define RTLS_CMD_RESET_DEVICE   0x20
 RTLS Node Manager command.
 
#define RTLS_CMD_SCAN   0x04
 RTLS Node Manager command.
 
#define RTLS_CMD_SCAN_STOP   0x05
 RTLS Node Manager command.
 
#define RTLS_CMD_SET_RTLS_PARAM   0x28
 RTLS Node Manager command.
 
#define RTLS_CMD_TERMINATE_LINK   0x22
 RTLS Node Manager command.
 
#define RTLS_CMD_TOF_CALIB_NV_READ   0x30
 RTLS Node Manager command.
 
#define RTLS_CMD_TOF_CALIBRATE   0x26
 RTLS Node Manager command.
 
#define RTLS_CMD_TOF_ENABLE   0x12
 RTLS Node Manager command.
 
#define RTLS_CMD_TOF_GET_SEC_SEED   0x10
 RTLS Node Manager command.
 
#define RTLS_CMD_TOF_RESULT_DIST   0x06
 RTLS Node Manager command.
 
#define RTLS_CMD_TOF_RESULT_RAW   0x08
 RTLS Node Manager command.
 
#define RTLS_CMD_TOF_RESULT_STAT   0x07
 RTLS Node Manager command.
 
#define RTLS_CMD_TOF_SET_PARAMS   0x11
 RTLS Node Manager command.
 
#define RTLS_CMD_TOF_SET_SEC_SEED   0x09
 RTLS Node Manager command.
 
#define RTLS_CMD_TOF_SWITCH_ROLE   0x31
 RTLS Node Manager command.
 
#define RTLS_CTRL_ALL_EVENTS   (RTLS_QUEUE_EVT)
 RTLS Task configuration.
 
#define RTLS_CTRL_REV   0x2
 
#define RTLS_CTRL_TASK_PRIORITY   2
 RTLS Task configuration variable.
 
#define RTLS_CTRL_TASK_STACK_SIZE   752
 RTLS Task configuration variable.
 
#define RTLS_CTRL_TOF_RSSI_THRESHOLD_HYSTERESIS   -5
 RSSI Hysteresis threshold.
 
#define RTLS_EVT_ASSERT   0x80
 RTLS async event.
 
#define RTLS_EVT_CONN_INFO   0x83
 RTLS async event.
 
#define RTLS_EVT_DEBUG   0x82
 RTLS async event.
 
#define RTLS_EVT_ERROR   0x81
 RTLS async event.
 
#define RTLS_FALSE   0
 FALSE.
 
#define RTLS_PARAM_2   0x02
 RTLS Param type RTLS_CMD_SET_RTLS_PARAM command.
 
#define RTLS_PARAM_3   0x03
 RTLS Param type RTLS_CMD_SET_RTLS_PARAM command.
 
#define RTLS_PARAM_CONNECTION_INTERVAL   0x01
 RTLS Param type RTLS_CMD_SET_RTLS_PARAM command.
 
#define RTLS_QUEUE_EVT   UTIL_QUEUE_EVENT_ID
 Event_Id_30.
 
#define RTLS_REQ_CONN   0x2
 RTLS Application Command Opcode.
 
#define RTLS_REQ_ENABLE_SYNC   0x1
 RTLS Application Command Opcode.
 
#define RTLS_REQ_SCAN   0x3
 RTLS Application Command Opcode.
 
#define RTLS_REQ_SEND_DATA   0x4
 RTLS Application Command Opcode.
 
#define RTLS_REQ_TERMINATE_LINK   0x5
 RTLS Application Command Opcode.
 
#define RTLS_REQ_UPDATE_CONN_INTERVAL   0x6
 RTLS Application Command Opcode.
 
#define RTLS_TOF_FREQ_PER_NV_BLOCK   4
 Max Num of frequencies per NV block.
 
#define RTLS_TRUE   1
 TRUE.
 
#define RTLSUTIL_FREE(pFree)
 RTLSUTIL_FREE memory free without icall. More...
 
#define RTLSUTIL_MALLOC(pAlloc, size)
 RTLSUTIL_MALLOC memory allocation without icall. More...
 
#define SNV_ID_CAL_DATA_SET   BLE_NVID_CUST_START+1
 
#define SNV_ID_CAL_PARAMS   BLE_NVID_CUST_START
 

Typedefs

typedef void(* pfnRtlsAppCb) (uint8_t *cmd)
 Application callback function.
 

Enumerations

enum  rtlsCapabilities_e {
  RTLS_CAP_NOT_INITIALIZED = 0x00000000, RTLS_CAP_CM = 0x00000001, RTLS_CAP_AOA_TX = 0x00000002, RTLS_CAP_AOA_RX = 0x00000004,
  RTLS_CAP_TOF_SLAVE = 0x00000008, RTLS_CAP_TOF_PASSIVE = 0x00000010, RTLS_CAP_TOF_MASTER = 0x00000020, RTLS_CAP_RTLS_SLAVE = 0x00000040,
  RTLS_CAP_RTLS_MASTER = 0x00000080, RTLS_CAP_RTLS_PASSIVE = 0x00000100
}
 Enumeration for RTLS Capabilities.
 
enum  rtlsStatus_e {
  RTLS_SUCCESS, RTLS_FAIL, RTLS_LINK_ESTAB_FAIL, RTLS_LINK_TERMINATED,
  RTLS_OUT_OF_MEMORY, RTLS_CONFIG_NOT_SUPPORTED, RTLS_ILLEGAL_CMD
}
 Enumeration for RTLS Status.
 

Functions

void RTLSCtrl_aoaDisable (void)
 Disables AoA. More...
 
void RTLSCtrl_aoaEnable (rtlsAoa_t *aoaControlBlock)
 Enables AoA passing the relevant parameters. More...
 
void RTLSCtrl_connInfoEvt (uint8_t *connInfo, uint16_t connInfoLen)
 RTLS Control Connection Info. More...
 
void RTLSCtrl_connResultEvt (uint8_t status)
 RTLS Control Connection Results. More...
 
void RTLSCtrl_initAoa (uint8_t startAntenna)
 Initialize AoA - has to be called before running AoA. More...
 
rtlsStatus_e RTLSCtrl_loadAndverifyCalibNVParams (rtlsTof_t *tofControlBlock)
 Verify calibration and load calibration from NV. More...
 
void * RTLSCtrl_malloc (uint32_t sz)
 This function will allocate memory, if we were unable to allocate we will report to RTLS Host. More...
 
void RTLSCtrl_open (rtlsConfiguration_t *rtlsConfig)
 RTLSCtrl_open. More...
 
void RTLSCtrl_outputCalibFromNV (uint8_t cmdId, uint8_t numFreq, uint16_t calibDistance, ToF_BurstStat *pCalibVals)
 Output calibration parameters and values. More...
 
void RTLSCtrl_outputTofStat (uint8_t cmdId, uint16_t numFreq, ToF_BurstStat *tofStatArray, uint8_t rssi)
 Output array of ToF_BurstStat. More...
 
void RTLSCtrl_postProcessAoa (rtlsAoa_t *aoaControlBlock, int8_t rssi, uint8_t channel)
 Called at the end of each connection event to extract I/Q samples. More...
 
void RTLSCtrl_postProcessTof (rtlsTof_t *tofControlBlock, int8_t rssi)
 Post process a ToF run. More...
 
void RTLSCtrl_processDataSent (uint8_t status)
 RTLS Application Data Sent. More...
 
void RTLSCtrl_processRtlsPacket (uint8_t *pPkt)
 RTLSCtrl_processRtlsPacket. More...
 
void RTLSCtrl_readCalibFromNV (rtlsTof_t *tofControlBlock)
 Read calibration From NV. More...
 
void RTLSCtrl_scanResultEvt (rtlsStatus_e status, uint8_t *scanResult, uint8_t size)
 RTLS Control Scan Results. More...
 
void RTLSCtrl_sendDebugEvent (uint8_t *debug_string, uint32_t debug_value)
 RTLSCtrl_sendDebugEvent. More...
 
void RTLSCtrl_syncEventNotify (rtlsStatus_e status, uint32_t timeToNextEvent, int8_t rssi, uint8_t channel)
 RTLSCtrl_syncEventNotify. More...
 
rtlsStatus_e RTLSCtrl_writeCalibToNV (rtlsTofCalibParams_t calibParams, ToF_BurstStat *pCalibVals)
 Write calibration to NV. More...
 
void RTLSHost_openHostIf (pfnRtlsCtrlProcessMsgCb rtlsHostMsgCb)
 This function opens the host interface and registers the application callback. More...
 
uint8_t RTLSHost_sendMsg (uint8_t cmdId, uint8_t cmdType, uint8_t *pData, uint16_t dataLen)
 This function is an abstraction of sending messages to a RTLS Host. More...
 

Detailed Description

This module implements Real Time Localization System (RTLS) Control module.

Macro Definition Documentation

§ RTLSUTIL_FREE

#define RTLSUTIL_FREE (   pFree)
Value:
{ \
volatile uint32_t keyHwi; \
volatile uint32_t keySwi; \
keyHwi = Hwi_disable(); \
keySwi = Swi_disable(); \
free(pFree); \
pFree = NULL; \
Swi_restore(keySwi); \
Hwi_restore(keyHwi); \
}

RTLSUTIL_FREE memory free without icall.

§ RTLSUTIL_MALLOC

#define RTLSUTIL_MALLOC (   pAlloc,
  size 
)
Value:
{ \
volatile uint32_t keyHwi; \
volatile uint32_t keySwi; \
keyHwi = Hwi_disable(); \
keySwi = Swi_disable(); \
pAlloc = malloc(size); \
Swi_restore(keySwi); \
Hwi_restore(keyHwi); \
}

RTLSUTIL_MALLOC memory allocation without icall.

Function Documentation

§ RTLSCtrl_aoaDisable()

void RTLSCtrl_aoaDisable ( void  )

Disables AoA.

Returns
none

§ RTLSCtrl_aoaEnable()

void RTLSCtrl_aoaEnable ( rtlsAoa_t *  aoaControlBlock)

Enables AoA passing the relevant parameters.

Parameters
aoaControlBlock- AoA information saved by RTLS Control
Returns
none

§ RTLSCtrl_connInfoEvt()

void RTLSCtrl_connInfoEvt ( uint8_t *  connInfo,
uint16_t  connInfoLen 
)

RTLS Control Connection Info.

This function sends connection information and parameters to RTLS Control

Parameters
connInfo- Connection information
connInfoLen- Connection Information length (needed to send the packet over NPI)

§ RTLSCtrl_connResultEvt()

void RTLSCtrl_connResultEvt ( uint8_t  status)

RTLS Control Connection Results.

This function notifies the RTLS Control that a connection has been formed

Parameters
status- Whether the connection was formed successfully

§ RTLSCtrl_initAoa()

void RTLSCtrl_initAoa ( uint8_t  startAntenna)

Initialize AoA - has to be called before running AoA.

Parameters
startAntenna- start samples with antenna 1 ro 2
Returns
none

§ RTLSCtrl_loadAndverifyCalibNVParams()

rtlsStatus_e RTLSCtrl_loadAndverifyCalibNVParams ( rtlsTof_t tofControlBlock)

Verify calibration and load calibration from NV.

Parameters
tofControlBlock- pointer to ToF control block
Returns
RTLS status

§ RTLSCtrl_malloc()

void* RTLSCtrl_malloc ( uint32_t  sz)

This function will allocate memory, if we were unable to allocate we will report to RTLS Host.

Parameters
sz- size (Allocated pointer has to be cast)
Returns
none

§ RTLSCtrl_open()

void RTLSCtrl_open ( rtlsConfiguration_t rtlsConfig)

RTLSCtrl_open.

Used to create and initialize the RTLS Control task

Parameters
rtlsConfig- pointer to the RTLS Application callbacks

§ RTLSCtrl_outputCalibFromNV()

void RTLSCtrl_outputCalibFromNV ( uint8_t  cmdId,
uint8_t  numFreq,
uint16_t  calibDistance,
ToF_BurstStat pCalibVals 
)

Output calibration parameters and values.

Parameters
cmdId- RTLS_CMD_TOF_* - command to the host
numFreq- Needed for size calculation
calibrationOffset- The distance at which calibration is being performed (will be subtracted from final result)
tofCalArray- Calibration array
Returns
None

§ RTLSCtrl_outputTofStat()

void RTLSCtrl_outputTofStat ( uint8_t  cmdId,
uint16_t  numFreq,
ToF_BurstStat tofStatArray,
uint8_t  rssi 
)

Output array of ToF_BurstStat.

Parameters
cmdId- RTLS_CMD_TOF_* - command to the host
numFreq- needed for size calculation
tofStatArray- Array to output
rssi- current rssi
Returns
None

§ RTLSCtrl_postProcessAoa()

void RTLSCtrl_postProcessAoa ( rtlsAoa_t *  aoaControlBlock,
int8_t  rssi,
uint8_t  channel 
)

Called at the end of each connection event to extract I/Q samples.

Parameters
aoaControlBlock- AoA information saved by RTLS Control
rssi- rssi to be reported to RTLS Host
channel- Channel used
Returns
none

§ RTLSCtrl_postProcessTof()

void RTLSCtrl_postProcessTof ( rtlsTof_t tofControlBlock,
int8_t  rssi 
)

Post process a ToF run.

Parameters
tofControlBlock- pointer to ToF information
rssi- current rssi
Returns
None

§ RTLSCtrl_processDataSent()

void RTLSCtrl_processDataSent ( uint8_t  status)

RTLS Application Data Sent.

This function is used by the RTLS Application to report the status of a sent packet This is used to let RTLS Control know whether RTLS data has been successfully transmitted

Parameters
status- SUCCESS or FAILURE for sending data to our peer

§ RTLSCtrl_processRtlsPacket()

void RTLSCtrl_processRtlsPacket ( uint8_t *  pPkt)

RTLSCtrl_processRtlsPacket.

This function is used by the RTLS Application to notify RTLS Control that a RTLS packet has been received

Parameters
pPkt- The RTLS packet to parse

§ RTLSCtrl_readCalibFromNV()

void RTLSCtrl_readCalibFromNV ( rtlsTof_t tofControlBlock)

Read calibration From NV.

Parameters
tofControlBlock- pointer to ToF control block
Returns
none

§ RTLSCtrl_scanResultEvt()

void RTLSCtrl_scanResultEvt ( rtlsStatus_e  status,
uint8_t *  scanResult,
uint8_t  size 
)

RTLS Control Scan Results.

This function notifies the RTLS Control that a connection has been formed

Parameters
scanResult- Pointer to scan results array
size- Size of scanResults array
status- scanResults status

§ RTLSCtrl_sendDebugEvent()

void RTLSCtrl_sendDebugEvent ( uint8_t *  debug_string,
uint32_t  debug_value 
)

RTLSCtrl_sendDebugEvent.

Send debug info

Parameters
debug_string- 32 bytes debug string
debug_value- 32 bits debug value

§ RTLSCtrl_syncEventNotify()

void RTLSCtrl_syncEventNotify ( rtlsStatus_e  status,
uint32_t  timeToNextEvent,
int8_t  rssi,
uint8_t  channel 
)

RTLSCtrl_syncEventNotify.

Synchronization function provided to the Application by RTLS Control This is the function that the application will be calling when a sync event is in place e.g BLE Connection Event

Parameters
timeToNextEvent- the time until the next sync event
rssi- rssi measurement against the RTLS Slave
channel- the channel on which the syncEvent was received
status

§ RTLSCtrl_writeCalibToNV()

rtlsStatus_e RTLSCtrl_writeCalibToNV ( rtlsTofCalibParams_t  calibParams,
ToF_BurstStat pCalibVals 
)

Write calibration to NV.

Parameters
pCalibVals- pointer to calibration values
calibParams- calibration parameters
Returns
RTLS status

§ RTLSHost_openHostIf()

void RTLSHost_openHostIf ( pfnRtlsCtrlProcessMsgCb  rtlsHostMsgCb)

This function opens the host interface and registers the application callback.

Parameters
rtlsHostMsgCb- Callback to use when a message arrives
Returns
none

§ RTLSHost_sendMsg()

uint8_t RTLSHost_sendMsg ( uint8_t  cmdId,
uint8_t  cmdType,
uint8_t *  pData,
uint16_t  dataLen 
)

This function is an abstraction of sending messages to a RTLS Host.

Parameters
cmdId- RTLS Cmd Id
cmdType- Async/Sync message
pData- Pointer to message data
dataLen- Length of data in pData
Returns
none
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale