TI BLE5-Stack API Documentation
1.01.08.00
|
This file contains configuration, initialization, and parameter management of Micro BLE Stack. It also contains interfacing between Micro BLE Stack and the application.
Go to the source code of this file.
Macros | |
#define | BLE_TO_RAT 2500 |
1 BLE tick(0.625 ms) = 2500 RAT tick | |
#define | BLE_TO_SYSTICK (625 / Clock_tickPeriod) |
0.625 ms = (625 / Clock_tickPeriod) system tick | |
#define | BYTE_TO_RAT (8 * US_TO_RAT) |
1 byte = 8 us = 32 RAT tick, assuming 1 Mbps PHY | |
#define | MS_TO_RAT 4000 |
1 ms = 4000 RAT tick | |
#define | MS_TO_SYSTICK (1000 / Clock_tickPeriod) |
1 ms = (1000 / Clock_tickPeriod) system tick | |
#define | RF_TIME_CRITICAL 1 |
Critical Timing. | |
#define | RF_TIME_RELAXED 0 |
Relaxed Timing. | |
#define | SYSTICK_TO_RAT (Clock_tickPeriod * US_TO_RAT) |
1 system tick = (Clock_tickPeriod * US_TO_RAT) RAT tick | |
#define | UBLE_ADDRTYPE_BD 4 |
Device that is currently being used. | |
#define | UBLE_ADDRTYPE_NONRESOLVABLE 2 |
Random Private Nonresolvable Address. | |
#define | UBLE_ADDRTYPE_PUBLIC 0 |
Public Address. | |
#define | UBLE_ADDRTYPE_RESOLVABLE 3 |
Random Private Resolvable Address. | |
#define | UBLE_ADDRTYPE_STATIC 1 |
Random Static Address. | |
#define | UBLE_ADV_CHAN_37 0x01 |
Channel 37. | |
#define | UBLE_ADV_CHAN_38 0x02 |
Channel 38. | |
#define | UBLE_ADV_CHAN_39 0x04 |
Channel 39. | |
#define | UBLE_ADV_CHAN_ALL (UBLE_ADV_CHAN_37 | UBLE_ADV_CHAN_38 | UBLE_ADV_CHAN_39) |
All Channels. | |
#define | UBLE_ADVTYPE_ADV_NC 5 |
associated with CMD_BLE_ADV_NC | |
#define | UBLE_ADVTYPE_ADV_SCAN 6 |
associated with CMD_BLE_ADV_SCAN | |
#define | UBLE_EVTDST_GAP 1 |
GAP. | |
#define | UBLE_EVTDST_LL 0 |
LL. More... | |
#define | UBLE_MAX_ADV_INTERVAL 16384 |
Maximum Advertising Interval. | |
#define | UBLE_MAX_ADVDATA_LEN B_MAX_ADV_LEN |
Max Advertising Data Length. | |
#define | UBLE_MAX_CHANNEL_MAP UBLE_ADV_CHAN_ALL |
Maximum Channel Map. | |
#define | UBLE_MAX_MONITOR_CHAN 39 |
Maximum Monitor channel. | |
#define | UBLE_MAX_MONITOR_DURATION 64000 |
Maximum Monitor duration. | |
#define | UBLE_MAX_MONITOR_HANDLE 4 |
Maximum Monitor handle. | |
#define | UBLE_MAX_SCAN_INTERVAL 16384 |
Maximum Scanning Interval. | |
#define | UBLE_MAX_SCAN_WINDOW 16384 |
Maximum Scanning window. | |
#define | UBLE_MAX_TX_POWER TX_POWER_5_DBM |
5 dBm | |
#define | UBLE_MIN_ADV_INTERVAL 160 |
Minimum Advertising interval. | |
#define | UBLE_MIN_CHANNEL_MAP UBLE_ADV_CHAN_37 |
Minimum Channel Map. | |
#define | UBLE_MIN_MONITOR_CHAN 0 |
Minimum Monitor channel. | |
#define | UBLE_MIN_MONITOR_DURATION 0 |
Minimum Monitor duration. | |
#define | UBLE_MIN_MONITOR_HANDLE 0 |
Minimum Monitor handle. | |
#define | UBLE_MIN_SCAN_INTERVAL 4 |
Minimum Scanning interval. | |
#define | UBLE_MIN_SCAN_WINDOW 4 |
Minimum Scanning window. | |
#define | UBLE_MIN_TX_POWER TX_POWER_MINUS_21_DBM |
-21 dBm | |
#define | UBLE_NUM_EVTDST 2 |
Number of Event Destinations. | |
#define | UBLE_PARAM_ADVCHANMAP (UBLE_PARAM_ADV_CMN_START+1) |
Advertising Channel map. More... | |
#define | UBLE_PARAM_ADVDATA (UBLE_PARAM_ADV_CMN_START+4) |
Advertising Data. More... | |
#define | UBLE_PARAM_ADVFLTPOLICY (UBLE_PARAM_ADV_SR_START+1) |
Advertising Filter Policy. More... | |
#define | UBLE_PARAM_ADVINTERVAL (UBLE_PARAM_ADV_CMN_START+0) |
Advertising Interval (n * 0.625 ms) More... | |
#define | UBLE_PARAM_ADVTYPE (UBLE_PARAM_ADV_CMN_START+2) |
Type of Advertising. More... | |
#define | UBLE_PARAM_DFLT_ADVCHANMAP UBLE_ADV_CHAN_ALL |
All Channels. | |
#define | UBLE_PARAM_DFLT_ADVDATA {0} |
No data. | |
#define | UBLE_PARAM_DFLT_ADVFLTPOLICY 0 |
Filter policy TBD. | |
#define | UBLE_PARAM_DFLT_ADVINTERVAL 1600 |
1 sec | |
#define | UBLE_PARAM_DFLT_ADVTYPE UBLE_ADVTYPE_ADV_NC |
ADV_NONCONN_IND. | |
#define | UBLE_PARAM_DFLT_FLTDUPLICATE 0 |
Filter duplicate TBD. | |
#define | UBLE_PARAM_DFLT_MONITOR_ACCESS_ADDR 0x8E89BED6 |
Adv address. | |
#define | UBLE_PARAM_DFLT_MONITOR_CHAN 37 |
Channel monitored. | |
#define | UBLE_PARAM_DFLT_MONITOR_DURATION 320 |
Monitor duration 200 ms. | |
#define | UBLE_PARAM_DFLT_MONITOR_HANDLE 0 |
Monitor session handle. | |
#define | UBLE_PARAM_DFLT_MONITOR_START_TIME 6400 |
Monitor start time 4 s. | |
#define | UBLE_PARAM_DFLT_RFPRIORITY UBLE_RF_PRI_NORMAL |
RF_PriorityNormal. | |
#define | UBLE_PARAM_DFLT_RFTIMECRIT RF_TIME_RELAXED |
Time-relaxed. | |
#define | UBLE_PARAM_DFLT_SCANCHAN UBLE_ADV_CHAN_ALL |
All Channels. | |
#define | UBLE_PARAM_DFLT_SCANFLTPOLICY 0 |
Scan filter policy TBD. | |
#define | UBLE_PARAM_DFLT_SCANINTERVAL 16 |
Scan interval. | |
#define | UBLE_PARAM_DFLT_SCANRSPDATA {0} |
No data. | |
#define | UBLE_PARAM_DFLT_SCANTYPE 0 |
Scan type. | |
#define | UBLE_PARAM_DFLT_SCANWINDOW 16 |
Scan window. | |
#define | UBLE_PARAM_DFLT_TIMETOADV 0 |
Disabled. | |
#define | UBLE_PARAM_DFLT_TXPOWER TX_POWER_0_DBM |
0 dBm | |
#define | UBLE_PARAM_RFPRIORITY (UBLE_PARAM_COMMON_START+0) |
Priority used for RF command scheduling. More... | |
#define | UBLE_PARAM_SCANRSPDATA (UBLE_PARAM_ADV_SR_START+0) |
Scan response Data. More... | |
#define | UBLE_PARAM_TIMETOADV (UBLE_PARAM_ADV_CMN_START+3) |
How early the application wants to get a notification before each advertising event happens (ms) More... | |
#define | UBLE_PARAM_TXPOWER (UBLE_PARAM_COMMON_START+1) |
TX Power. More... | |
#define | UBLE_RF_PRI_HIGH ((uint8) RF_PriorityHigh) |
High Priority. | |
#define | UBLE_RF_PRI_HIGHEST ((uint8) RF_PriorityHighest) |
Highest Priority. | |
#define | UBLE_RF_PRI_NORMAL ((uint8) RF_PriorityNormal) |
Normal Priority. | |
#define | UBLE_TX_POWER_INVALID 0xFFFF |
Invalid TX Power Register value. | |
#define | US_TO_RAT 4 |
1 us = 4 RAT tick More... | |
Typedefs | |
typedef uint8 | ubleAddrType_t |
Address Type. | |
typedef void(* | ubleAntSwitchCB_t) (void) |
Type of the callback to switch antenna in the application. More... | |
typedef uint8 | ubleEvt_t |
Micro BLE Stack Event. | |
typedef uint8 | ubleEvtDst_t |
Recipient of Micro BLE Stack Event. | |
typedef uint8 | ubleMsg_t |
Type of Micro BLE Stack message. | |
typedef void(* | ublePostEvtProxyCB_t) (void) |
Type of the callback to have uble_processMsg called in the application task context. More... | |
typedef void(* | ubleProcessMsg_t) (ubleEvtMsg_t *pEvtMsg) |
Function to process event messages destined to the calle module. | |
Functions | |
bStatus_t | uble_checkAddr (ubleAddrType_t addrType, uint8 *pAddr) |
Check if the given address is valid. More... | |
bStatus_t | uble_getAddr (ubleAddrType_t addrType, uint8 *pAddr) |
Retrieve the address corresponding to the given address type. More... | |
bStatus_t | uble_getParameter (uint8 param, void *pValue) |
Get a Micro BLE Stack parameter. More... | |
void | uble_processMsg (void) |
Let the Micro Stack process the queued messages. More... | |
bStatus_t | uble_registerAntSwitchCB (ubleAntSwitchCB_t pfnAntSwitchCB) |
Register callback for antenna switch. More... | |
void | uble_resetAddr (void) |
Make BD Addr revert to Random Static Address if exists or Public Address otherwise. | |
bStatus_t | uble_setParameter (uint8 param, uint8 len, void *pValue) |
Set a Micro BLE Stack parameter. More... | |
bStatus_t | uble_stackInit (ubleAddrType_t addrType, uint8 *pStaticAddr, ublePostEvtProxyCB_t pfnPostEvtProxyCB, uint8 timeCritical) |
Initialize Micro BLE Stack. More... | |