TI BLE-Stack for Bluetooth API Documentation
3.03.01.00
|
Parameter Structure for the Connection Established Event. More...
Data Fields | |
uint8_t | addressType |
1 Byte Type of initiator address | |
uint16_t | connHandle |
2 Byte Handle of the connection | |
uint16_t | connInterval |
2 Byte More... | |
uint8_t | pAddr [6] |
6 Byte Address of the initiator | |
uint16_t | slaveLatency |
2 Byte More... | |
uint16_t | supervisionTimeout |
2 Byte More... | |
Parameter Structure for the Connection Established Event.
See SNP Event Indication for more information.
This is a packed structure. see Dealing with Parameters and Packed Structures for more information.
uint16_t connInterval |
2 Byte
uint16_t slaveLatency |
2 Byte
uint16_t supervisionTimeout |
2 Byte