TI BLE-Stack for Bluetooth API Documentation
3.03.01.00
|
Macros | |
#define | SNP_BLE_GAP_BOND_REJECTED bleGAPBondRejected |
0x32, General status, The bound information was rejected. | |
#define | SNP_BLE_MEM_ALLOC_ERROR bleMemAllocError |
0x13, General status, Memory allocation error occurred | |
#define | SNP_BLE_NO_RESOURCES bleNoResources |
0x15, General status, There are no resource available | |
#define | SNP_BLE_TIMEOUT bleTimeout |
0x17, General status, Timed out performing function | |
#define | SNP_INVALIDPARAMETER INVALIDPARAMETER |
0x2, General status, Invalid Parameter | |
#define | SNP_LL_CTRL_PKT_TIMEOUT_TERM LL_CTRL_PKT_TIMEOUT_TERM |
0x22, LL status, Link Layer Response Timeout | |
#define | SNP_LL_ENC_KEY_REQ_REJECTED LL_ENC_KEY_REQ_REJECTED |
0x06, LL status, Pin or Key Missing | |
#define | SNP_LL_ENC_KEY_REQ_UNSUPPORTED_FEATURE LL_ENC_KEY_REQ_UNSUPPORTED_FEATURE |
0x1A, LL status, Unsupported Remote Feature | |
#define | SNP_LL_STATUS_ERROR_BAD_PARAMETER LL_STATUS_ERROR_BAD_PARAMETER |
0x12, LL status, Invalid HCI Command Parameters or 0x30: Parameter Out of Mandatory Range? | |
#define | SNP_LL_STATUS_ERROR_COMMAND_DISALLOWED LL_STATUS_ERROR_COMMAND_DISALLOWED |
0x0C, LL status, Command Disallowed | |
#define | SNP_LL_STATUS_ERROR_CTRL_PROC_ALREADY_ACTIVE LL_STATUS_ERROR_CTRL_PROC_ALREADY_ACTIVE |
0x3A, LL status, Controller Busy | |
#define | SNP_LL_STATUS_ERROR_FEATURE_NOT_SUPPORTED LL_STATUS_ERROR_FEATURE_NOT_SUPPORTED |
0x11, LL status, Unsupported Feature or Parameter Value | |
#define | SNP_LL_STATUS_ERROR_INACTIVE_CONNECTION LL_STATUS_ERROR_INACTIVE_CONNECTION |
0x02, LL status, Unknown Connection Identifier for now; may be needed for multiple connections | |
#define | SNP_SMP_PAIRING_FAILED_AUTH_REQ SMP_PAIRING_FAILED_AUTH_REQ |
0x03, SMP status, The pairing procedure can't be performed as authentication requirements can't be met due to IO capabilities of one or both devices | |
#define | SNP_SMP_PAIRING_FAILED_CMD_NOT_SUPPORTED SMP_PAIRING_FAILED_CMD_NOT_SUPPORTED |
0x07, SMP status, The SMP command received is not supported on this device. | |
#define | SNP_SMP_PAIRING_FAILED_CONFIRM_VALUE SMP_PAIRING_FAILED_CONFIRM_VALUE |
0x04, SMP status, The confirm value doesn't match the calculated compare value | |
#define | SNP_SMP_PAIRING_FAILED_DHKEY_CHECK_FAILED SMP_PAIRING_FAILED_DHKEY_CHECK_FAILED |
0x0B, SMP status, Indicates to the remote device that the DHKey Check value received does not match the one calculated by the local device. | |
#define | SNP_SMP_PAIRING_FAILED_ENC_KEY_SIZE SMP_PAIRING_FAILED_ENC_KEY_SIZE |
0x06, SMP status, The resultant encryption key size is insufficient for the security requirements of this device. | |
#define | SNP_SMP_PAIRING_FAILED_NOT_SUPPORTED SMP_PAIRING_FAILED_NOT_SUPPORTED |
0x05, SMP status, Pairing isn't supported by the device | |
#define | SNP_SMP_PAIRING_FAILED_NUM_COMPARISON_FAILED SMP_PAIRING_FAILED_NUM_COMPARISON_FAILED |
0x0C, SMP status, Indicates that the confirm value in the numeric comparison protocol do not match. | |
#define | SNP_SMP_PAIRING_FAILED_OOB_NOT_AVAIL SMP_PAIRING_FAILED_OOB_NOT_AVAIL |
0x02, SMP status, The OOB data is not available | |
#define | SNP_SMP_PAIRING_FAILED_PASSKEY_ENTRY_FAILED SMP_PAIRING_FAILED_PASSKEY_ENTRY_FAILED |
0x01, SMP status, The user input of the passkey failed, for example, the user cancelled the operation. | |
#define | SNP_SMP_PAIRING_FAILED_UNSPECIFIED SMP_PAIRING_FAILED_UNSPECIFIED |
0x08, SMP status, Pairing failed due to an unspecified reason | |
List of GENERAL status codes that are transfered to the SAP layer. Note: These defines were added after the SAP was not able to understand the statuses that were transfered "as is" to the pGapBondCB->pairStateCB. The values of these defines is copied from the original define status.