![]() |
![]() |
SPICC26X2DMA Object. More...
#include <SPICC26X2DMA.h>
Data Fields | |
HwiP_Struct | hwi |
PIN_Handle | pinHandle |
PIN_State | pinState |
Power_NotifyObj | spiPostObj |
SwiP_Struct | swi |
SemaphoreP_Struct | transferComplete |
SPI_CallbackFxn | transferCallbackFxn |
SPI_Transaction * | headPtr |
SPI_Transaction * | tailPtr |
SPI_Transaction * | completedTransfers |
UDMACC26XX_Handle | udmaHandle |
size_t | framesQueued |
size_t | framesTransferred |
size_t | priTransferSize |
size_t | altTransferSize |
uint32_t | activeChannel |
uint32_t | bitRate |
uint32_t | dataSize |
uint32_t | transferTimeout |
uint32_t | busyBit |
uint16_t | rxScratchBuf |
uint16_t | txScratchBuf |
SPI_TransferMode | transferMode |
SPI_Mode | mode |
uint8_t | format |
PIN_Id | csnPin |
SPICC26X2DMA_ReturnPartial | returnPartial |
bool | isOpen |
SPICC26X2DMA Object.
The application must not access any member variables of this structure!
HwiP_Struct SPICC26X2DMA_Object::hwi |
PIN_Handle SPICC26X2DMA_Object::pinHandle |
PIN_State SPICC26X2DMA_Object::pinState |
Power_NotifyObj SPICC26X2DMA_Object::spiPostObj |
SwiP_Struct SPICC26X2DMA_Object::swi |
SemaphoreP_Struct SPICC26X2DMA_Object::transferComplete |
SPI_CallbackFxn SPICC26X2DMA_Object::transferCallbackFxn |
SPI_Transaction* SPICC26X2DMA_Object::headPtr |
SPI_Transaction* SPICC26X2DMA_Object::tailPtr |
SPI_Transaction* SPICC26X2DMA_Object::completedTransfers |
UDMACC26XX_Handle SPICC26X2DMA_Object::udmaHandle |
size_t SPICC26X2DMA_Object::framesQueued |
size_t SPICC26X2DMA_Object::framesTransferred |
size_t SPICC26X2DMA_Object::priTransferSize |
size_t SPICC26X2DMA_Object::altTransferSize |
uint32_t SPICC26X2DMA_Object::activeChannel |
uint32_t SPICC26X2DMA_Object::bitRate |
uint32_t SPICC26X2DMA_Object::dataSize |
uint32_t SPICC26X2DMA_Object::transferTimeout |
uint32_t SPICC26X2DMA_Object::busyBit |
uint16_t SPICC26X2DMA_Object::rxScratchBuf |
uint16_t SPICC26X2DMA_Object::txScratchBuf |
SPI_TransferMode SPICC26X2DMA_Object::transferMode |
SPI_Mode SPICC26X2DMA_Object::mode |
uint8_t SPICC26X2DMA_Object::format |
PIN_Id SPICC26X2DMA_Object::csnPin |
SPICC26X2DMA_ReturnPartial SPICC26X2DMA_Object::returnPartial |
bool SPICC26X2DMA_Object::isOpen |