Data Fields
PDMCC26XX_I2S_Config Struct Reference

The PDMCC26XX_I2S_Config structure contains a set of pointers used to characterize the PDMCC26XX_I2S driver implementation. More...

#include <PDMCC26XX_util.h>

Data Fields

void * object
 
void const * hwAttrs
 

Detailed Description

The PDMCC26XX_I2S_Config structure contains a set of pointers used to characterize the PDMCC26XX_I2S driver implementation.

Field Documentation

§ object

void* PDMCC26XX_I2S_Config::object

Pointer to a driver specific data object

§ hwAttrs

void const* PDMCC26XX_I2S_Config::hwAttrs

Pointer to a driver specific hardware attributes structure


The documentation for this struct was generated from the following file:
© Copyright 1995-2018, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale