Data Fields
ECDSACC26X2_Object_ Struct Reference

ECDSACC26X2 Object. More...

#include <ECDSACC26X2.h>

Collaboration diagram for ECDSACC26X2_Object_:
Collaboration graph
[legend]

Data Fields

bool isOpen
 
bool operationInProgress
 
bool operationCanceled
 
int_fast16_t operationStatus
 
ECDSA_Operation operation
 
ECDSA_OperationType operationType
 
ECDSA_CallbackFxn callbackFxn
 
ECDSACC26X2_stateMachineFxn fsmFxn
 
ECDSA_ReturnBehavior returnBehavior
 
ECDSACC26X2_FsmState fsmState
 
uint32_t semaphoreTimeout
 
uint32_t resultAddress
 
uint32_t * scratchNumber1
 
uint32_t * scratchNumber2
 

Detailed Description

ECDSACC26X2 Object.

The application must not access any member variables of this structure!

Field Documentation

§ isOpen

bool ECDSACC26X2_Object_::isOpen

§ operationInProgress

bool ECDSACC26X2_Object_::operationInProgress

§ operationCanceled

bool ECDSACC26X2_Object_::operationCanceled

§ operationStatus

int_fast16_t ECDSACC26X2_Object_::operationStatus

§ operation

ECDSA_Operation ECDSACC26X2_Object_::operation

§ operationType

ECDSA_OperationType ECDSACC26X2_Object_::operationType

§ callbackFxn

ECDSA_CallbackFxn ECDSACC26X2_Object_::callbackFxn

§ fsmFxn

ECDSACC26X2_stateMachineFxn ECDSACC26X2_Object_::fsmFxn

§ returnBehavior

ECDSA_ReturnBehavior ECDSACC26X2_Object_::returnBehavior

§ fsmState

ECDSACC26X2_FsmState ECDSACC26X2_Object_::fsmState

§ semaphoreTimeout

uint32_t ECDSACC26X2_Object_::semaphoreTimeout

§ resultAddress

uint32_t ECDSACC26X2_Object_::resultAddress

§ scratchNumber1

uint32_t* ECDSACC26X2_Object_::scratchNumber1

§ scratchNumber2

uint32_t* ECDSACC26X2_Object_::scratchNumber2

The documentation for this struct was generated from the following file:
© Copyright 1995-2018, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale