Data Fields
AESCCM_Config_ Struct Reference

AESCCM Global configuration. More...

#include <AESCCM.h>

Data Fields

void * object
 
void const * hwAttrs
 

Detailed Description

AESCCM Global configuration.

The AESCCM_Config structure contains a set of pointers used to characterize the AESCCM driver implementation.

This structure needs to be defined before calling AESCCM_init() and it must not be changed thereafter.

See also
AESCCM_init()

Field Documentation

§ object

void* AESCCM_Config_::object

Pointer to a driver specific data object

§ hwAttrs

void const* AESCCM_Config_::hwAttrs

Pointer to a driver specific hardware attributes structure


The documentation for this struct was generated from the following file:
© Copyright 1995-2018, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale