Data Structures | Macros | Typedefs | Enumerations
ECJPAKECC26X2.h File Reference

Detailed Description

ECJPAKE driver implementation for the CC26X2 family.

============================================================================

This file should only be included in the board file to fill the ECJPAKE_config struct.

Hardware and Implementation Details

The CC26X2 family has a dedicated public key accelerator. It is capable of multiple mathematical operations including dedicated ECC point addition, doubling, and scalar multiplication. Only one operation can be carried out on the accelerator at a time. Mutual exclusion is implemented at the driver level and coordinated between all drivers relying on the accelerator. It is transparent to the application and only noted ensure sensible access timeouts are set.

The large number maths engine (LNME) uses a dedicated 2kB block of RAM (PKA RAM) for its operations. The operands of the maths operations must be copied into and results out of the PKA ram. This necessitates a significant number of reads and writes for each operation. The bus interface to the RAM only allows for word-aligned reads and writes. The CPU splits the reads and writes from and to general SRAM from unaligned addresses into multiple bus operations while accumulating the data in a register until it is full. The result of this hardware process is that providing buffers such as plaintext CryptoKey keying material to ECC APIs that are word-aligned will significantly speed up the operation and reduce power consumption.

The driver implementation does not perform runtime checks for most input parameters. Only values that are likely to have a stochastic element to them are checked (such as whether a driver is already open). Higher input paramter validation coverage is achieved by turning on assertions when compiling the driver.

Supported Curve Types

The driver implementation supports the following curve types for ECJPAKE:

Curve Type Supported
Short Weierstrass Yes
Montgomery No
Edwards No

Public Key Validation

When performing Schnorr-ZKP verification, the foreign public key will always be validated. The public V is validated implicitly during the operation. The implementation assumes that the cofactor, h, of the curve is 1. This lets us skip the computationally expensive step of multiplying the foreign key by the order and checking if it yields the point at infinity. When the cofactor is 1, this property is implied by validating that the point is not already the point at infinity and that it validates against the curve equation. All curves supplied by default, the NIST and Brainpool curves, have cofactor = 1. While the implementation can use arbitrary curves, you should verify that any other curve used has a cofactor of 1.

#include <stdint.h>
#include <stdbool.h>
#include <ti/drivers/Power.h>
#include <ti/drivers/ECJPAKE.h>
#include <ti/drivers/cryptoutils/ecc/ECCParams.h>
#include <ti/drivers/cryptoutils/cryptokey/CryptoKey.h>
#include <ti/drivers/dpl/HwiP.h>
#include <ti/drivers/dpl/SwiP.h>
#include <ti/drivers/dpl/SemaphoreP.h>
Include dependency graph for ECJPAKECC26X2.h:

Go to the source code of this file.

Data Structures

struct  ECJPAKECC26X2_HWAttrs_
 ECJPAKECC26X2 Hardware Attributes. More...
 
struct  ECJPAKECC26X2_Object_
 ECJPAKECC26X2 Object. More...
 

Macros

#define ECJPAKECC26X2_STATUS_FSM_RUN_PKA_OP   ECJPAKE_STATUS_RESERVED - 0
 
#define ECJPAKECC26X2_STATUS_FSM_RUN_FSM   ECJPAKE_STATUS_RESERVED - 1
 

Typedefs

typedef enum ECJPAKECC26X2_FsmState_ ECJPAKECC26X2_FsmState
 ECJPAKECC26X2 states. More...
 
typedef struct ECJPAKECC26X2_HWAttrs_ ECJPAKECC26X2_HWAttrs
 ECJPAKECC26X2 Hardware Attributes. More...
 
typedef struct ECJPAKECC26X2_Object_ ECJPAKECC26X2_Object
 ECJPAKECC26X2 Object. More...
 

Enumerations

enum  ECJPAKECC26X2_FsmState_ {
  ECJPAKECC26X2_FSM_ERROR = 0, ECJPAKECC26X2_FSM_ROUND_ONE_VALIDATE_MYPRIVATEKEY1, ECJPAKECC26X2_FSM_ROUND_ONE_VALIDATE_MYPRIVATEKEY2, ECJPAKECC26X2_FSM_ROUND_ONE_VALIDATE_MYPRIVATEV1,
  ECJPAKECC26X2_FSM_ROUND_ONE_VALIDATE_MYPRIVATEV2, ECJPAKECC26X2_FSM_ROUND_ONE_GENERATE_MYPUBLICKEY1, ECJPAKECC26X2_FSM_ROUND_ONE_GENERATE_MYPUBLICKEY1_RESULT, ECJPAKECC26X2_FSM_ROUND_ONE_GENERATE_MYPUBLICKEY2,
  ECJPAKECC26X2_FSM_ROUND_ONE_GENERATE_MYPUBLICKEY2_RESULT, ECJPAKECC26X2_FSM_ROUND_ONE_GENERATE_MYPUBLICV1, ECJPAKECC26X2_FSM_ROUND_ONE_GENERATE_MYPUBLICV1_RESULT, ECJPAKECC26X2_FSM_ROUND_ONE_GENERATE_MYPUBLICV2,
  ECJPAKECC26X2_FSM_ROUND_ONE_GENERATE_MYPUBLICV2_RESULT, ECJPAKECC26X2_FSM_ROUND_ONE_GENERATE_RETURN, ECJPAKECC26X2_FSM_GENERATE_ZKP_PRIVATEKEY_X_HASH, ECJPAKECC26X2_FSM_GENERATE_ZKP_PRIVATEKEY_X_HASH_RESULT,
  ECJPAKECC26X2_FSM_GENERATE_ZKP_PRIVATEKEY_X_HASH_MOD_N, ECJPAKECC26X2_FSM_GENERATE_ZKP_PRIVATEKEY_X_HASH_MOD_N_RESULT, ECJPAKECC26X2_FSM_GENERATE_ZKP_ADD_V_TO_N, ECJPAKECC26X2_FSM_GENERATE_ZKP_ADD_V_TO_N_RESULT,
  ECJPAKECC26X2_FSM_GENERATE_ZKP_SUBTRACT_RESULTS, ECJPAKECC26X2_FSM_GENERATE_ZKP_SUBTRACT_RESULTS_RESULT, ECJPAKECC26X2_FSM_GENERATE_ZKP_SUBTRACT_RESULT_MOD_N, ECJPAKECC26X2_FSM_GENERATE_ZKP_SUBTRACT_RESULT_MOD_N_RESULT,
  ECJPAKECC26X2_FSM_ZKP_GENERATE_RETURN, ECJPAKECC26X2_FSM_VERIFY_ZKP_VALIDATE_PUBLIC_KEY, ECJPAKECC26X2_FSM_VERIFY_ZKP_HASH_MOD_N, ECJPAKECC26X2_FSM_VERIFY_ZKP_HASH_MOD_N_RESULT,
  ECJPAKECC26X2_FSM_VERIFY_ZKP_MULT_G_BY_R, ECJPAKECC26X2_FSM_VERIFY_ZKP_MULT_G_BY_R_RESULT, ECJPAKECC26X2_FSM_VERIFY_ZKP_MULT_X_BY_HASH, ECJPAKECC26X2_FSM_VERIFY_ZKP_MULT_X_BY_HASH_RESULT,
  ECJPAKECC26X2_FSM_VERIFY_ZKP_ADD_RESULTS, ECJPAKECC26X2_FSM_VERIFY_ZKP_ADD_RESULTS_RESULT, ECJPAKECC26X2_FSM_VERIFY_ZKP_COMPARE_AGAINST_V, ECJPAKECC26X2_FSM_ROUND_TWO_MULT_MYPRIVATEKEY2_BY_PRESHAREDSECRET,
  ECJPAKECC26X2_FSM_ROUND_TWO_MULT_MYPRIVATEKEY2_BY_PRESHAREDSECRET_RESULT, ECJPAKECC26X2_FSM_ROUND_TWO_MYCOMBINEDPRIVATEKEY_MOD_N, ECJPAKECC26X2_FSM_ROUND_TWO_MYCOMBINEDPRIVATEKEY_MOD_N_RESULT, ECJPAKECC26X2_FSM_ROUND_TWO_ADD_MYPUBLICKEY1_TO_THEIRPUBLICKEY1,
  ECJPAKECC26X2_FSM_ROUND_TWO_ADD_MYPUBLICKEY1_TO_THEIRPUBLICKEY1_RESULT, ECJPAKECC26X2_FSM_ROUND_TWO_ADD_THEIRPUBLICKEY2, ECJPAKECC26X2_FSM_ROUND_TWO_ADD_THEIRPUBLICKEY2_RESULT, ECJPAKECC26X2_FSM_ROUND_TWO_ADD_MYPUBLICKEY2,
  ECJPAKECC26X2_FSM_ROUND_TWO_ADD_MYPUBLICKEY2_RESULT, ECJPAKECC26X2_FSM_ROUND_TWO_MULT_MYCOMBINEDPRIVATEKEY_BY_MYNEWGENERATOR, ECJPAKECC26X2_FSM_ROUND_TWO_MULT_MYCOMBINEDPRIVATEKEY_BY_MYNEWGENERATOR_RESULT, ECJPAKECC26X2_FSM_ROUND_TWO_VALIDATE_MYPRIVATEV,
  ECJPAKECC26X2_FSM_ROUND_TWO_GENERATE_MYPUBLICV, ECJPAKECC26X2_FSM_ROUND_TWO_GENERATE_MYPUBLICV_RESULT, ECJPAKECC26X2_FSM_ROUND_TWO_GENERATE_RETURN, ECJPAKECC26X2_FSM_GENERATE_SHARED_SECRET_MULT_THEIRPUBLICKEY2_BY_MYCOMBINEDPRIVATEKEY,
  ECJPAKECC26X2_FSM_GENERATE_SHARED_SECRET_MULT_THEIRPUBLICKEY2_BY_MYCOMBINEDPRIVATEKEY_RESULT, ECJPAKECC26X2_FSM_GENERATE_SHARED_SECRET_SUB_YCOORDINATE_FROM_PRIME, ECJPAKECC26X2_FSM_GENERATE_SHARED_SECRET_SUB_YCOORDINATE_FROM_PRIME_RESULT, ECJPAKECC26X2_FSM_GENERATE_SHARED_SECRET_ADD_THEIRCOMBINEDPUBLICKEY,
  ECJPAKECC26X2_FSM_GENERATE_SHARED_SECRET_ADD_THEIRCOMBINEDPUBLICKEY_RESULT, ECJPAKECC26X2_FSM_GENERATE_SHARED_SECRET_MULT_BY_MYPRIVATEKEY2, ECJPAKECC26X2_FSM_GENERATE_SHARED_SECRET_MULT_BY_MYPRIVATEKEY2_RESULT, ECJPAKECC26X2_FSM_GENERATE_SHARED_SECRET_RETURN
}
 ECJPAKECC26X2 states. More...
 

Macro Definition Documentation

§ ECJPAKECC26X2_STATUS_FSM_RUN_PKA_OP

#define ECJPAKECC26X2_STATUS_FSM_RUN_PKA_OP   ECJPAKE_STATUS_RESERVED - 0

§ ECJPAKECC26X2_STATUS_FSM_RUN_FSM

#define ECJPAKECC26X2_STATUS_FSM_RUN_FSM   ECJPAKE_STATUS_RESERVED - 1

Typedef Documentation

§ ECJPAKECC26X2_FsmState

ECJPAKECC26X2 states.

The EC-JPAKE operations are implemented using multiple invidividual PKA operations. Since state transitions for these operations are almost always predictable, the state transitions are encoded linearly in this enum. The FSM controller will increment the state counter and iterate through states until it is told to stop or restart.

§ ECJPAKECC26X2_HWAttrs

ECJPAKECC26X2 Hardware Attributes.

ECJPAKECC26X2 hardware attributes should be included in the board file and pointed to by the ECJPAKE_config struct.

§ ECJPAKECC26X2_Object

ECJPAKECC26X2 Object.

The application must not access any member variables of this structure!

Enumeration Type Documentation

§ ECJPAKECC26X2_FsmState_

ECJPAKECC26X2 states.

The EC-JPAKE operations are implemented using multiple invidividual PKA operations. Since state transitions for these operations are almost always predictable, the state transitions are encoded linearly in this enum. The FSM controller will increment the state counter and iterate through states until it is told to stop or restart.

Enumerator
ECJPAKECC26X2_FSM_ERROR 
ECJPAKECC26X2_FSM_ROUND_ONE_VALIDATE_MYPRIVATEKEY1 
ECJPAKECC26X2_FSM_ROUND_ONE_VALIDATE_MYPRIVATEKEY2 
ECJPAKECC26X2_FSM_ROUND_ONE_VALIDATE_MYPRIVATEV1 
ECJPAKECC26X2_FSM_ROUND_ONE_VALIDATE_MYPRIVATEV2 
ECJPAKECC26X2_FSM_ROUND_ONE_GENERATE_MYPUBLICKEY1 
ECJPAKECC26X2_FSM_ROUND_ONE_GENERATE_MYPUBLICKEY1_RESULT 
ECJPAKECC26X2_FSM_ROUND_ONE_GENERATE_MYPUBLICKEY2 
ECJPAKECC26X2_FSM_ROUND_ONE_GENERATE_MYPUBLICKEY2_RESULT 
ECJPAKECC26X2_FSM_ROUND_ONE_GENERATE_MYPUBLICV1 
ECJPAKECC26X2_FSM_ROUND_ONE_GENERATE_MYPUBLICV1_RESULT 
ECJPAKECC26X2_FSM_ROUND_ONE_GENERATE_MYPUBLICV2 
ECJPAKECC26X2_FSM_ROUND_ONE_GENERATE_MYPUBLICV2_RESULT 
ECJPAKECC26X2_FSM_ROUND_ONE_GENERATE_RETURN 
ECJPAKECC26X2_FSM_GENERATE_ZKP_PRIVATEKEY_X_HASH 
ECJPAKECC26X2_FSM_GENERATE_ZKP_PRIVATEKEY_X_HASH_RESULT 
ECJPAKECC26X2_FSM_GENERATE_ZKP_PRIVATEKEY_X_HASH_MOD_N 
ECJPAKECC26X2_FSM_GENERATE_ZKP_PRIVATEKEY_X_HASH_MOD_N_RESULT 
ECJPAKECC26X2_FSM_GENERATE_ZKP_ADD_V_TO_N 
ECJPAKECC26X2_FSM_GENERATE_ZKP_ADD_V_TO_N_RESULT 
ECJPAKECC26X2_FSM_GENERATE_ZKP_SUBTRACT_RESULTS 
ECJPAKECC26X2_FSM_GENERATE_ZKP_SUBTRACT_RESULTS_RESULT 
ECJPAKECC26X2_FSM_GENERATE_ZKP_SUBTRACT_RESULT_MOD_N 
ECJPAKECC26X2_FSM_GENERATE_ZKP_SUBTRACT_RESULT_MOD_N_RESULT 
ECJPAKECC26X2_FSM_ZKP_GENERATE_RETURN 
ECJPAKECC26X2_FSM_VERIFY_ZKP_VALIDATE_PUBLIC_KEY 
ECJPAKECC26X2_FSM_VERIFY_ZKP_HASH_MOD_N 
ECJPAKECC26X2_FSM_VERIFY_ZKP_HASH_MOD_N_RESULT 
ECJPAKECC26X2_FSM_VERIFY_ZKP_MULT_G_BY_R 
ECJPAKECC26X2_FSM_VERIFY_ZKP_MULT_G_BY_R_RESULT 
ECJPAKECC26X2_FSM_VERIFY_ZKP_MULT_X_BY_HASH 
ECJPAKECC26X2_FSM_VERIFY_ZKP_MULT_X_BY_HASH_RESULT 
ECJPAKECC26X2_FSM_VERIFY_ZKP_ADD_RESULTS 
ECJPAKECC26X2_FSM_VERIFY_ZKP_ADD_RESULTS_RESULT 
ECJPAKECC26X2_FSM_VERIFY_ZKP_COMPARE_AGAINST_V 
ECJPAKECC26X2_FSM_ROUND_TWO_MULT_MYPRIVATEKEY2_BY_PRESHAREDSECRET 
ECJPAKECC26X2_FSM_ROUND_TWO_MULT_MYPRIVATEKEY2_BY_PRESHAREDSECRET_RESULT 
ECJPAKECC26X2_FSM_ROUND_TWO_MYCOMBINEDPRIVATEKEY_MOD_N 
ECJPAKECC26X2_FSM_ROUND_TWO_MYCOMBINEDPRIVATEKEY_MOD_N_RESULT 
ECJPAKECC26X2_FSM_ROUND_TWO_ADD_MYPUBLICKEY1_TO_THEIRPUBLICKEY1 
ECJPAKECC26X2_FSM_ROUND_TWO_ADD_MYPUBLICKEY1_TO_THEIRPUBLICKEY1_RESULT 
ECJPAKECC26X2_FSM_ROUND_TWO_ADD_THEIRPUBLICKEY2 
ECJPAKECC26X2_FSM_ROUND_TWO_ADD_THEIRPUBLICKEY2_RESULT 
ECJPAKECC26X2_FSM_ROUND_TWO_ADD_MYPUBLICKEY2 
ECJPAKECC26X2_FSM_ROUND_TWO_ADD_MYPUBLICKEY2_RESULT 
ECJPAKECC26X2_FSM_ROUND_TWO_MULT_MYCOMBINEDPRIVATEKEY_BY_MYNEWGENERATOR 
ECJPAKECC26X2_FSM_ROUND_TWO_MULT_MYCOMBINEDPRIVATEKEY_BY_MYNEWGENERATOR_RESULT 
ECJPAKECC26X2_FSM_ROUND_TWO_VALIDATE_MYPRIVATEV 
ECJPAKECC26X2_FSM_ROUND_TWO_GENERATE_MYPUBLICV 
ECJPAKECC26X2_FSM_ROUND_TWO_GENERATE_MYPUBLICV_RESULT 
ECJPAKECC26X2_FSM_ROUND_TWO_GENERATE_RETURN 
ECJPAKECC26X2_FSM_GENERATE_SHARED_SECRET_MULT_THEIRPUBLICKEY2_BY_MYCOMBINEDPRIVATEKEY 
ECJPAKECC26X2_FSM_GENERATE_SHARED_SECRET_MULT_THEIRPUBLICKEY2_BY_MYCOMBINEDPRIVATEKEY_RESULT 
ECJPAKECC26X2_FSM_GENERATE_SHARED_SECRET_SUB_YCOORDINATE_FROM_PRIME 
ECJPAKECC26X2_FSM_GENERATE_SHARED_SECRET_SUB_YCOORDINATE_FROM_PRIME_RESULT 
ECJPAKECC26X2_FSM_GENERATE_SHARED_SECRET_ADD_THEIRCOMBINEDPUBLICKEY 
ECJPAKECC26X2_FSM_GENERATE_SHARED_SECRET_ADD_THEIRCOMBINEDPUBLICKEY_RESULT 
ECJPAKECC26X2_FSM_GENERATE_SHARED_SECRET_MULT_BY_MYPRIVATEKEY2 
ECJPAKECC26X2_FSM_GENERATE_SHARED_SECRET_MULT_BY_MYPRIVATEKEY2_RESULT 
ECJPAKECC26X2_FSM_GENERATE_SHARED_SECRET_RETURN 
© Copyright 1995-2018, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale