72 #ifndef ti_drivers_aescbc_AESCBCCC26XX__include 73 #define ti_drivers_aescbc_AESCBCCC26XX__include 84 #include <ti/drivers/dpl/SwiP.h>
int_fast16_t returnStatus
Definition: AESCBCCC26XX.h:117
AESCBC_OperationType operationType
Definition: AESCBCCC26XX.h:119
void(* AESCBC_CallbackFxn)(AESCBC_Handle handle, int_fast16_t returnValue, AESCBC_Operation *operation, AESCBC_OperationType operationType)
The definition of a callback function used by the AESCBC driver when used in AESCBC_RETURN_BEHAVIOR_C...
Definition: AESCBC.h:498
struct AESCBCCC26XX_Object AESCBCCC26XX_Object
AESCBCCC26XX Object.
AESCBC_Operation * operation
Definition: AESCBCCC26XX.h:122
uint8_t intPriority
Crypto Peripheral's interrupt priority.
Definition: AESCBCCC26XX.h:105
AESCBCCC26XX Object.
Definition: AESCBCCC26XX.h:113
AESCBCCC26XX Hardware Attributes.
Definition: AESCBCCC26XX.h:92
enum AESCBC_OperationType_ AESCBC_OperationType
Enum for the operation types supported by the driver.
bool isOpen
Definition: AESCBCCC26XX.h:114
Struct containing the parameters required for encrypting/decrypting a message.
Definition: AESCBC.h:430
uint32_t semaphoreTimeout
Definition: AESCBCCC26XX.h:120
bool operationInProgress
Definition: AESCBCCC26XX.h:115
enum AESCBC_ReturnBehavior_ AESCBC_ReturnBehavior
The way in which CBC function calls return after performing an encryption or decryption operation...
struct AESCBCCC26XX_HWAttrs AESCBCCC26XX_HWAttrs
AESCBCCC26XX Hardware Attributes.
AESCBC_ReturnBehavior returnBehavior
Definition: AESCBCCC26XX.h:118
bool operationCanceled
Definition: AESCBCCC26XX.h:116
AESCBC_CallbackFxn callbackFxn
Definition: AESCBCCC26XX.h:121