![]() |
![]() |
The definition of an NVS function table that contains the required set of functions to control a specific NVS driver implementation. More...
#include <NVS.h>
The definition of an NVS function table that contains the required set of functions to control a specific NVS driver implementation.
NVS_CloseFxn NVS_FxnTable::closeFxn |
Function to close the specified NVS region
NVS_ControlFxn NVS_FxnTable::controlFxn |
Function to apply control command to the specified NVS region
NVS_EraseFxn NVS_FxnTable::eraseFxn |
Function to erase a portion of the specified NVS region
NVS_GetAttrsFxn NVS_FxnTable::getAttrsFxn |
Function to get the NVS device-specific attributes
NVS_InitFxn NVS_FxnTable::initFxn |
Function to initialize the NVS module
NVS_LockFxn NVS_FxnTable::lockFxn |
Function to lock the specified NVS flash region
NVS_OpenFxn NVS_FxnTable::openFxn |
Function to open an NVS region
NVS_ReadFxn NVS_FxnTable::readFxn |
Function to read from the specified NVS region
NVS_UnlockFxn NVS_FxnTable::unlockFxn |
Function to unlock the specified NVS flash region
NVS_WriteFxn NVS_FxnTable::writeFxn |
Function to write to the specified NVS region