![]() |
![]() |
Macros | |
#define | CryptoKey_STATUS_SUCCESS (0) |
Successful status code. More... | |
#define | CryptoKey_STATUS_ERROR (-1) |
Generic error status code. More... | |
#define | CryptoKey_STATUS_UNDEFINED_ENCODING (-2) |
Returned if the encoding of a CryptoKey is not a CryptoKey_Encoding value. More... | |
CryptoKey_STATUS_* macros are general status codes returned by CryptoKey_control()
#define CryptoKey_STATUS_SUCCESS (0) |
Successful status code.
CryptoKey_control() returns CryptoKey_STATUS_SUCCESS if the control code was executed successfully.
#define CryptoKey_STATUS_ERROR (-1) |
Generic error status code.
CryptoKey_control() returns CryptoKey_STATUS_ERROR if the control code was not executed successfully.
#define CryptoKey_STATUS_UNDEFINED_ENCODING (-2) |
Returned if the encoding of a CryptoKey is not a CryptoKey_Encoding value.
CryptoKey_control() returns CryptoKey_STATUS_ERROR if the control code was not executed successfully.