![]() |
![]() |
TI BLE-Stack for Bluetooth 4.2 API Documentation
3.02.00.00
|
Macros | |
#define | GAPBOND_AUTO_SYNC_WL 0x40D |
Synchronize the whitelist with bonded devices (Read/Write) More... | |
#define | GAPBOND_BOND_COUNT 0x40E |
Gets the total number of bonds stored in NV (Read-only) More... | |
#define | GAPBOND_BOND_FAIL_ACTION 0x40F |
The action that the device takes after an unsuccessful bonding attempt (Write-only) More... | |
#define | GAPBOND_BONDING_ENABLED 0x406 |
Whether to request bonding during pairing (Read/Write) More... | |
#define | GAPBOND_DEFAULT_PASSCODE 0x408 |
This parameter is only used by the Host Test app Application (network processor) The Id of this parameter is used to store the password locally. the GAP Bond manager is not storing any default password anymore, everytime a password is needed, pfnPasscodeCB_t will be call. More... | |
#define | GAPBOND_ECC_KEYS 0x413 |
The private and public keys to use for Secure Connections pairing (Read/Write) More... | |
#define | GAPBOND_ECCKEY_REGEN_POLICY 0x412 |
ECC Key Regeneration Policy (Read/Write) More... | |
#define | GAPBOND_ERASE_ALLBONDS 0x409 |
Erase all bonds from SNV and remove all bonded devices (Write) More... | |
#define | GAPBOND_ERASE_SINGLEBOND 0x410 |
Erase a single bonded device (Write-only) More... | |
#define | GAPBOND_INITIATE_WAIT 0x401 |
The amount of time (in ms) to wait for a pairing request before sending the slave initiate request (Read/Write) More... | |
#define | GAPBOND_IO_CAPABILITIES 0x403 |
The I/O capabilities of the local device (Read/Write) More... | |
#define | GAPBOND_KEY_DIST_LIST 0x407 |
Key distribution list for pairing (Read/Write) More... | |
#define | GAPBOND_KEYSIZE 0x40C |
Key Size used in pairing. (Read/Write) More... | |
#define | GAPBOND_LOCAL_OOB_SC_DATA 0x417 |
Local OOB Secure Connections Data (Read/Write) More... | |
#define | GAPBOND_LOCAL_OOB_SC_ENABLED 0x416 |
Validate Local OOB Secure Connections Data (Read/Write) More... | |
#define | GAPBOND_LRU_BOND_REPLACEMENT 0x418 |
Enable / Disable LRU Bond Replacement Scheme (Read/Write) More... | |
#define | GAPBOND_MITM_PROTECTION 0x402 |
Whether to use authenticated pairing (Read/Write) More... | |
#define | GAPBOND_OOB_DATA 0x405 |
OOB data to use for pairing (Read/Write) More... | |
#define | GAPBOND_OOB_ENABLED 0x404 |
Whether to use OOB for pairing (Read/Write) More... | |
#define | GAPBOND_PAIRING_MODE 0x400 |
Whether to allow pairing, and if so, whether to initiate pairing. (Read/Write) More... | |
#define | GAPBOND_REMOTE_OOB_SC_DATA 0x415 |
Remote OOB Secure Connections Data (Read/Write) More... | |
#define | GAPBOND_REMOTE_OOB_SC_ENABLED 0x414 |
Validate Remote OOB Secure Connections Data (Read/Write) More... | |
#define | GAPBOND_SECURE_CONNECTION 0x411 |
Define Secure Connections Usage during Pairing (Read/Write) More... | |
Parameters set via GAPBondMgr_SetParameter
#define GAPBOND_AUTO_SYNC_WL 0x40D |
Synchronize the whitelist with bonded devices (Read/Write)
If TRUE, the whitelist will first be cleared. Then, each unique address stored by bonds in SNV will be synched with the whitelist indefinitely or until this is set to FALSE
size: uint8_t
default: FALSE
range: TRUE (sync) or FALSE (don't sync)
#define GAPBOND_BOND_COUNT 0x40E |
Gets the total number of bonds stored in NV (Read-only)
size: uint8_t
range: 0 - 255
#define GAPBOND_BOND_FAIL_ACTION 0x40F |
The action that the device takes after an unsuccessful bonding attempt (Write-only)
size: uint8_t
default: GAPBOND_FAIL_TERMINATE_LINK
range: Bonding Failure Actions
#define GAPBOND_BONDING_ENABLED 0x406 |
Whether to request bonding during pairing (Read/Write)
size: uint8_t
default: FALSE
range: TRUE (request) or FALSE (do not request)
#define GAPBOND_DEFAULT_PASSCODE 0x408 |
This parameter is only used by the Host Test app Application (network processor) The Id of this parameter is used to store the password locally. the GAP Bond manager is not storing any default password anymore, everytime a password is needed, pfnPasscodeCB_t will be call.
size: uint32_t
default: 0
range: 0 - 999999
#define GAPBOND_ECC_KEYS 0x413 |
The private and public keys to use for Secure Connections pairing (Read/Write)
Only applicable for Secure Connections. Allows the application to specify the private and public keys to use pairing. When this is set, the keys are used indefinitely even if a regeneration policy was set with GAPBOND_ECCKEY_REGEN_POLICY. To make the Bond Manager stop using these keys, pass a 1 byte value of 0x00. These keys are stored in RAM and are not retained in non-volatile memory. These keys can be defined by the application, or the application can request them using the SM_GetEccKeys command.
size: gapBondEccKeys_t
default: by default, the keys are generated using GAPBOND_ECCKEY_REGEN_POLICY
range: A valid gapBondEccKeys_t structure
0x00: previously passed keys will no longer be used
#define GAPBOND_ECCKEY_REGEN_POLICY 0x412 |
ECC Key Regeneration Policy (Read/Write)
Only applicable for Secure Connections. Define reuse of the private and public ECC keys for multiple pairings.The default is to always regenerate the keys upon each new pairing. This parameter has no effect when the application specifies the keys using the GAPBOND_ECC_KEYS parameter. The behavior is that upon each pairing the number of recycles remaining is decremented by 1, but if the pairing fails the count is decremented by 3. The specification recommends that this value be set to no higher than 10 to avoid an attacker from learning too much about a private key before it is regenerated.
size: uint8_t
default: 2
range: 0 - 256
#define GAPBOND_ERASE_ALLBONDS 0x409 |
Erase all bonds from SNV and remove all bonded devices (Write)
#define GAPBOND_ERASE_SINGLEBOND 0x410 |
Erase a single bonded device (Write-only)
size: uint8_t[9]
range: A nine-byte array where the first byte is the Address Types and the next 8 are the device address.
#define GAPBOND_INITIATE_WAIT 0x401 |
The amount of time (in ms) to wait for a pairing request before sending the slave initiate request (Read/Write)
size: uint16_t
default: 0 - 65535
range: 1000
#define GAPBOND_IO_CAPABILITIES 0x403 |
The I/O capabilities of the local device (Read/Write)
size: uint8_t
default: GAPBOND_IO_CAP_DISPLAY_ONLY
#define GAPBOND_KEY_DIST_LIST 0x407 |
Key distribution list for pairing (Read/Write)
Multiple values can be used via bitwise ORing
size: uint8_t
default: GAPBOND_KEYDIST_SENCKEY | GAPBOND_KEYDIST_SIDKEY | GAPBOND_KEYDIST_MIDKEY | GAPBOND_KEYDIST_MSIGN
#define GAPBOND_KEYSIZE 0x40C |
Key Size used in pairing. (Read/Write)
size: uint8_t
default: 16
range: TGAP_SM_MIN_KEY_LEN - TGAP_SM_MAX_KEY_LEN
#define GAPBOND_LOCAL_OOB_SC_DATA 0x417 |
Local OOB Secure Connections Data (Read/Write)
Passes Secure Connections data to the bond manager that was sent to the remote device. This is only the 16 bytes of byte OOB data, which is needed to complete pairing. Only applicable for Secure Connections.
size: uint8_t[16]
default: all 0x00's
range: 0x00000000000000000000000000000000 - 0xFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF
#define GAPBOND_LOCAL_OOB_SC_ENABLED 0x416 |
Validate Local OOB Secure Connections Data (Read/Write)
Indicates to the Bond Manager that the local device has valid OOB data it has attempted to send to the remote device, and that the local OOB data supplied to the Bond Manager by the GAPBOND_LOCAL_OOB_SC_DATA parameter is valid. This is needed to determine if the OOB protocol is expected to be used for Secure Connections. Only one device needs to have received OOB data for OOB pairing to be used in Secure Connections. Only applicable for Secure Connections.
size: uint8_t
default: FALSE
range: TRUE (OOB data is valid) or FALSE (OOB data is not valid)
#define GAPBOND_LRU_BOND_REPLACEMENT 0x418 |
Enable / Disable LRU Bond Replacement Scheme (Read/Write)
Whether to enable the least recently used bond scheme so that, when a newly bonded device is added and all the entries are full, the least recently used device’s bond is deleted to make room.
size: uint8_t
default: FALSE
range: TRUE (enable) or FALSE (disable)
#define GAPBOND_MITM_PROTECTION 0x402 |
Whether to use authenticated pairing (Read/Write)
size: uint8_t
default: TRUE
range: TRUE (use) or FALSE (do not use)
#define GAPBOND_OOB_DATA 0x405 |
OOB data to use for pairing (Read/Write)
size: uint8_t[16]
default: 0x00000000000000000000000000000000 -
range: 0x00000000000000000000000000000000 - 0xFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF
#define GAPBOND_OOB_ENABLED 0x404 |
Whether to use OOB for pairing (Read/Write)
size: uint8_t
default: FALSE
range: TRUE (use) or FALSE (do not use)
#define GAPBOND_PAIRING_MODE 0x400 |
Whether to allow pairing, and if so, whether to initiate pairing. (Read/Write)
size: uint8_t
default: GAPBOND_PAIRING_MODE_WAIT_FOR_REQ
#define GAPBOND_REMOTE_OOB_SC_DATA 0x415 |
Remote OOB Secure Connections Data (Read/Write)
Used to pass OOB Secure Connections data to the bond manager that has been received from a remote device. This data is not only the 16 bytes of OOB data, but also the 32-byte ECC Public Key X-Coordinate of the remote device (that it must use when pairing) and a 16-byte confirmation value computed using the said public key, OOB data is used as input to the SM_F4 function. This data can be invalidated by writing 0x00 to the GAPBOND_REMOTE_OOB_SC_ENABLED parameter. Only applicable for Secure Connections.
size: gapBondOobSC_t
default: all 0x00's
range: A valid gapBondOobSC_t structure
#define GAPBOND_REMOTE_OOB_SC_ENABLED 0x414 |
Validate Remote OOB Secure Connections Data (Read/Write)
Indicate to the Bond Manager that any Secure Connections OOB data that has been received from a remote device, which has been supplied to the Bond Manager by the GAPBOND_REMOTE_OOB_SC_DATA parameter, is valid. Only applicable for Secure Connections
size: uint8_t
default: FALSE
range: TRUE (OOB data is valid) or FALSE (OOB data is not valid)
#define GAPBOND_SECURE_CONNECTION 0x411 |
Define Secure Connections Usage during Pairing (Read/Write)
size: uint8_t
default: GAPBOND_SECURE_CONNECTION_ALLOW