![]() |
![]() |
ECDHCC26X2 Object. More...
#include <ECDHCC26X2.h>
Data Fields | |
bool | isOpen |
ECDH_CallbackFxn | callbackFxn |
ECDH_ReturnBehavior | returnBehavior |
uint32_t | semaphoreTimeout |
uint32_t | resultAddress |
uint16_t | publicKeyParamLength |
const ECCParams_CurveParams * | curve |
uint8_t * | generatedKeyingMaterial |
CryptoKey * | privateKey |
SwiP_Struct | callbackSwi |
ECDHCC26X2 Object.
The application must not access any member variables of this structure!
bool ECDHCC26X2_Object_::isOpen |
ECDH_CallbackFxn ECDHCC26X2_Object_::callbackFxn |
ECDH_ReturnBehavior ECDHCC26X2_Object_::returnBehavior |
uint32_t ECDHCC26X2_Object_::semaphoreTimeout |
uint32_t ECDHCC26X2_Object_::resultAddress |
uint16_t ECDHCC26X2_Object_::publicKeyParamLength |
const ECCParams_CurveParams* ECDHCC26X2_Object_::curve |
uint8_t* ECDHCC26X2_Object_::generatedKeyingMaterial |
CryptoKey* ECDHCC26X2_Object_::privateKey |
SwiP_Struct ECDHCC26X2_Object_::callbackSwi |