#include <DisplaySharp.h>
§ spiIndex
uint32_t DisplaySharp_HWAttrs::spiIndex |
§ csPin
PIN_Id DisplaySharp_HWAttrs::csPin |
§ extcominPin
PIN_Id DisplaySharp_HWAttrs::extcominPin |
§ powerPin
PIN_Id DisplaySharp_HWAttrs::powerPin |
§ enablePin
PIN_Id DisplaySharp_HWAttrs::enablePin |
§ pixelHeight
uint16_t DisplaySharp_HWAttrs::pixelHeight |
§ pixelWidth
uint16_t DisplaySharp_HWAttrs::pixelWidth |
§ displayBuf
void* DisplaySharp_HWAttrs::displayBuf |
The documentation for this struct was generated from the following file: