Functions
SensorHdc1000.h File Reference

Detailed Description

Driver for Texas Instruments HCD1000 humidity sensor.

Driver include

This header file should be included in an application as follows:

#include "stdbool.h"
#include "stdint.h"

Go to the source code of this file.

Functions

bool SensorHdc1000_init (void)
 Initialize the sensor. More...
 
void SensorHdc1000_start (void)
 Start measurement. More...
 
bool SensorHdc1000_read (uint16_t *pRawTemp, uint16_t *pRawHum)
 Read humidity sensor data. More...
 
void SensorHdc1000_convert (uint16_t rawTemp, uint16_t rawHum, float *pTemp, float *pHum)
 Convert raw data to temperature and humidity. More...
 
bool SensorHdc1000_test (void)
 Humidity sensor self test. More...
 

Function Documentation

§ SensorHdc1000_init()

bool SensorHdc1000_init ( void  )

Initialize the sensor.

Configure reading of temperature and humidity as one read cycle, and use 14 bit data size.

Returns
true if writing to the sensor succeeds

§ SensorHdc1000_start()

void SensorHdc1000_start ( void  )

Start measurement.

Precondition
SensorHdc1000_init must be called (and succeed first).

§ SensorHdc1000_read()

bool SensorHdc1000_read ( uint16_t *  pRawTemp,
uint16_t *  pRawHum 
)

Read humidity sensor data.

Parameters
pRawTemp- buffer for raw temperature
pRawHum- buffer for raw humidity
Returns
true if I2C read operation succeeds

§ SensorHdc1000_convert()

void SensorHdc1000_convert ( uint16_t  rawTemp,
uint16_t  rawHum,
float *  pTemp,
float *  pHum 
)

Convert raw data to temperature and humidity.

Calculate relative humidity and temperature based on provided raw data.

Parameters
rawTemp- raw temperature value
rawHum- raw humidity value
pTemp- converted temperature [deg. C]
pHum- converted humidity

§ SensorHdc1000_test()

bool SensorHdc1000_test ( void  )

Humidity sensor self test.

Returns
true if test passes
Copyright 2017, Texas Instruments Incorporated