![]() |
![]() |
TI BLE-Stack for Bluetooth 4.2 API Documentation
3.01.00.07
|
Parameter Structure for the response to SNP_getStatus This is a packed structure. see Dealing with Parameters and Packed Structures for more information. More...
Data Fields | |
uint8_t | advStatus |
1 Byte Current state of advertising : More... | |
uint8_t | ATTmethod |
1 Byte Current GATT operation in progress if snpGetStatusCmdRsp_t::ATTstatus is set to TRUE | |
uint8_t | ATTstatus |
1 Byte Current state of the GATT server More... | |
uint8_t | gapRoleStatus |
1 Byte Current state of the GAP Role ( gaprole_States_t) More... | |
Parameter Structure for the response to SNP_getStatus This is a packed structure. see Dealing with Parameters and Packed Structures for more information.
uint8_t advStatus |
1 Byte Current state of advertising :
TRUE= advertisement enable,
FALSE = advertisement disable
uint8_t ATTstatus |
1 Byte Current state of the GATT server
TRUE= operation ongoing, snpGetStatusCmdRsp_t::ATTmethod will indicate the currently running operation
FALSE = no operation
uint8_t gapRoleStatus |
1 Byte Current state of the GAP Role ( gaprole_States_t)
Currently, Only Peripheral:
is the only possible GAP Peripheral Role State