![]() |
![]() |
|
TI BLE-Stack for Bluetooth 4.2 API Documentation
3.01.00.05
|
Macros | |
| #define | ICALL_CUSTOM_INIT_PARAMS { USER0_CFG } |
| #define | ICALL_ERRNO_CORRUPT_MSG -6 |
| ICall function return value for corrupt message error. | |
| #define | ICALL_ERRNO_INVALID_FUNCTION -2 |
| ICall function return value in case the function id is unknown to the registered handler of the service. | |
| #define | ICALL_ERRNO_INVALID_PARAMETER -3 |
| ICall function return value for invalid parameter value. | |
| #define | ICALL_ERRNO_INVALID_SERVICE -1 |
| ICall function return value in case the service corresponding to a passed service id is not registered and hence is unknown. | |
| #define | ICALL_ERRNO_NO_RESOURCE -4 |
| ICall function return value for no resource error. | |
| #define | ICALL_ERRNO_NOMSG 2 |
| ICall function return value for no message error. | |
| #define | ICALL_ERRNO_OVERFLOW -7 |
| ICall function return value for counter overflow. | |
| #define | ICALL_ERRNO_SUCCESS 0 |
| ICall function return value for successful operation. | |
| #define | ICALL_ERRNO_TIMEOUT 1 |
| ICall function return value for timeout error. | |
| #define | ICALL_ERRNO_UNDERFLOW -8 |
| ICall function return value for counter underflow. | |
| #define | ICALL_ERRNO_UNKNOWN_THREAD -5 |
| ICall function return value in case the calling thread context is not a registered thread, or the entity id passed is not a registered entity. | |
| #define | ICALL_INVALID_ENTITY_ID 0xffu |
| Entity ID used to indicate invalid entity. | |
| #define | ICALL_INVALID_TIMER_ID NULL |
| Timer ID used to indicate invalid ID. | |
| #define | ICALL_LITE_DIRECT_API_DONE_CMD_ID 0x42 |
| Message CMD ID to signal DIRECT_API CMD is done. | |
| #define | ICALL_MSG_EVENT_ID Event_Id_31 |
| Event reserved to signal for icall message inbetween application and services. More... | |
| #define | ICALL_MSG_FORMAT_1ST_CHAR_TASK_ID 1 |
| Message format that requires the first byte to be replaced with the src task ID. | |
| #define | ICALL_MSG_FORMAT_3RD_CHAR_TASK_ID 2 |
| Message format that requires the third byte to be replaced with the src task ID. | |
| #define | ICALL_MSG_FORMAT_DIRECT_API_ID 3 |
| Message format indicated a direct API call. | |
| #define | ICALL_MSG_FORMAT_KEEP 0 |
| #define | ICALL_MSG_FUNC_GET_LOCAL_MSG_ENTITY_ID 0 |
| Messaging service function id for translating ICall_entityID to locally understandable id. | |
| #define | ICALL_PWR_AWAKE_FROM_STANDBY 0 |
| #define | ICALL_PWR_AWAKE_FROM_STANDBY_LATE 5 |
| #define | ICALL_PWR_C_IDLE_PD_DISALLOW 0x00000008l |
| #define | ICALL_PWR_C_NEED_FLASH_IN_IDLE 0x00000010l |
| #define | ICALL_PWR_C_SB_DISALLOW 0x00000004l |
| #define | ICALL_PWR_C_SB_VIMS_CACHE_RETAIN 0x00000001l |
| #define | ICALL_PWR_C_SD_DISALLOW 0x00000002l |
| #define | ICALL_PWR_D_DOMAIN_PERIPH 0x00100000l |
| #define | ICALL_PWR_D_DOMAIN_RFCORE 0x00400000l |
| #define | ICALL_PWR_D_DOMAIN_SERIAL 0x00200000l |
| #define | ICALL_PWR_D_DOMAIN_SYSBUS 0x00800000l |
| #define | ICALL_PWR_D_PERIPH_CRYPTO 0x00010000l |
| #define | ICALL_PWR_D_PERIPH_GPIO 0x00004000l |
| #define | ICALL_PWR_D_PERIPH_GPT0 0x00000020l |
| #define | ICALL_PWR_D_PERIPH_GPT1 0x00000040l |
| #define | ICALL_PWR_D_PERIPH_GPT2 0x00000080l |
| #define | ICALL_PWR_D_PERIPH_GPT3 0x00000100l |
| #define | ICALL_PWR_D_PERIPH_I2C0 0x00001000l |
| #define | ICALL_PWR_D_PERIPH_I2S 0x00020000l |
| #define | ICALL_PWR_D_PERIPH_RFCORE 0x00040000l |
| #define | ICALL_PWR_D_PERIPH_SSI0 0x00000200l |
| #define | ICALL_PWR_D_PERIPH_SSI1 0x00000400l |
| #define | ICALL_PWR_D_PERIPH_TRNG 0x00002000l |
| #define | ICALL_PWR_D_PERIPH_UART0 0x00000800l |
| #define | ICALL_PWR_D_PERIPH_UDMA 0x00008000l |
| #define | ICALL_PWR_D_XOSC_HF 0x00080000l |
| #define | ICALL_PWR_ENTER_SHUTDOWN 4 |
| #define | ICALL_PWR_ENTER_STANDBY 2 |
| #define | ICALL_PWR_TRANSITION_ENTERING_SLEEP 2 |
| #define | ICALL_PWR_TRANSITION_EXITING_SLEEP 3 |
| #define | ICALL_PWR_TRANSITION_STAY_IN_ACTIVE 1 |
| #define | ICALL_PWR_TRANSITION_UNKNOWN 0 |
| #define | ICALL_SEMAPHORE_MODE_BINARY 1 |
| Binary semaphore mode. | |
| #define | ICALL_SEMAPHORE_MODE_COUNTING 0 |
| Counting semaphore mode. | |
| #define | ICALL_SERVICE_CLASS_BLE 0x0010 |
| BLE service class enumerated value. | |
| #define | ICALL_SERVICE_CLASS_BLE_BOARD 0x0088 |
| BLE Board dependent service class. More... | |
| #define | ICALL_SERVICE_CLASS_BLE_MSG 0x0050 |
| BLE stack message delivery service. | |
| #define | ICALL_SERVICE_CLASS_CRYPTO 0x0080 |
| Crypto service class. More... | |
| #define | ICALL_SERVICE_CLASS_DUMMY 0x0100 |
| #define | ICALL_SERVICE_CLASS_DUMMY_BOARD 0x0200 |
| Dummy stack board service class enumeration. More... | |
| #define | ICALL_SERVICE_CLASS_MASK 0xFFF8 |
| Bit mask for recommended service id enumeration. More... | |
| #define | ICALL_SERVICE_CLASS_NPI 0x0038 |
| NPI service class enumerated value. | |
| #define | ICALL_SERVICE_CLASS_PRIMITIVE 0x0008 |
| Service class enumerated value for primitive service. More... | |
| #define | ICALL_SERVICE_CLASS_RADIO 0x0098 |
| Radio service class. More... | |
| #define | ICALL_SERVICE_CLASS_REMOTI_RCN 0x0028 |
| RemoTI network layer service class enumerated value. | |
| #define | ICALL_SERVICE_CLASS_REMOTI_RTI 0x0020 |
| RemoTI RTI interface service class enumerated value. | |
| #define | ICALL_SERVICE_CLASS_TIMAC 0x0018 |
| TIMAC service class enumerated value. | |
| #define | ICALL_SERVICE_CLASS_TIMAC_BOARD 0x0090 |
| TIMAC Board dependent service class. More... | |
| #define | ICALL_SERVICE_CLASS_ZSTACK 0x0030 |
| ZStack service class enumerated value. | |
| #define | ICALL_SERVICE_INSTANCE_MASK 0x0007 |
| Bit mask for recommended service id enumeration. More... | |
| #define | ICALL_STACK0_ADDR 0x00005000ul |
| #define | ICALL_TASK_PRIORITIES { 5 } |
| #define | ICALL_TASK_STACK_SIZES { 1000 } |
| #define | ICALL_TIMEOUT_FOREVER 0xfffffffful |
| Time period that indicates infinite time. | |
| #define | ICALL_TIMEOUT_PREDEFINE 5000 |
| Time period that indicates timeout define at build time default is 5s. | |
| #define | ICALL_WAITMATCH_EVENT_ID Event_Id_29 |
| Event reserved to signal a wait match period has ended and the caller may continue exeuction. More... | |
| #define | USER0_CFG &user0Cfg |
| user config | |
| #define ICALL_CUSTOM_INIT_PARAMS { USER0_CFG } |
Initializer for custom initialization parameters. Each element of the array corresponds to initialization parameter (a pointer) specific to the image to be passed to the entry function defined in ICALL_ADDR_MAPS initializer.
| #define ICALL_MSG_EVENT_ID Event_Id_31 |
Event reserved to signal for icall message inbetween application and services.
Used when ICALL_EVENTS compile option is enabled only.
| #define ICALL_MSG_FORMAT_KEEP 0 |
Message format that requires no change
| #define ICALL_PWR_AWAKE_FROM_STANDBY 0 |
Power state transition to active power state from standby power state.
| #define ICALL_PWR_AWAKE_FROM_STANDBY_LATE 5 |
Power state transition to active power state where IOs can be accessed, from standby power state.
| #define ICALL_PWR_C_IDLE_PD_DISALLOW 0x00000008l |
A power API constraint flag that can be added to a bitmap used as the argument to ICall_pwrConfigACAction(), ICall_pwrRequire() and ICall_pwrDispense().
| #define ICALL_PWR_C_NEED_FLASH_IN_IDLE 0x00000010l |
A power API constraint flag that can be added to a bitmap used as the argument to ICall_pwrConfigACAction(), ICall_pwrRequire() and ICall_pwrDispense().
| #define ICALL_PWR_C_SB_DISALLOW 0x00000004l |
A power API constraint flag that can be added to a bitmap used as the argument to ICall_pwrConfigACAction(), ICall_pwrRequire() and ICall_pwrDispense().
| #define ICALL_PWR_C_SB_VIMS_CACHE_RETAIN 0x00000001l |
A power API constraint flag that can be added to a bitmap used as the argument to ICall_pwrConfigACAction(), ICall_pwrRequire() and ICall_pwrDispense().
| #define ICALL_PWR_C_SD_DISALLOW 0x00000002l |
A power API constraint flag that can be added to a bitmap used as the argument to ICall_pwrConfigACAction(), ICall_pwrRequire() and ICall_pwrDispense().
| #define ICALL_PWR_D_DOMAIN_PERIPH 0x00100000l |
A power API dependency flag that can be added to a bitmap used as the argument to ICall_pwrConfigACAction(), ICall_pwrRequire() and ICall_pwrDispense().
| #define ICALL_PWR_D_DOMAIN_RFCORE 0x00400000l |
A power API dependency flag that can be added to a bitmap used as the argument to ICall_pwrConfigACAction(), ICall_pwrRequire() and ICall_pwrDispense().
| #define ICALL_PWR_D_DOMAIN_SERIAL 0x00200000l |
A power API dependency flag that can be added to a bitmap used as the argument to ICall_pwrConfigACAction(), ICall_pwrRequire() and ICall_pwrDispense().
| #define ICALL_PWR_D_DOMAIN_SYSBUS 0x00800000l |
A power API dependency flag that can be added to a bitmap used as the argument to ICall_pwrConfigACAction(), ICall_pwrRequire() and ICall_pwrDispense().
| #define ICALL_PWR_D_PERIPH_CRYPTO 0x00010000l |
A power API dependency flag that can be added to a bitmap used as the argument to ICall_pwrConfigACAction(), ICall_pwrRequire() and ICall_pwrDispense().
| #define ICALL_PWR_D_PERIPH_GPIO 0x00004000l |
A power API dependency flag that can be added to a bitmap used as the argument to ICall_pwrConfigACAction(), ICall_pwrRequire() and ICall_pwrDispense().
| #define ICALL_PWR_D_PERIPH_GPT0 0x00000020l |
A power API dependency flag that can be added to a bitmap used as the argument to ICall_pwrConfigACAction(), ICall_pwrRequire() and ICall_pwrDispense().
| #define ICALL_PWR_D_PERIPH_GPT1 0x00000040l |
A power API dependency flag that can be added to a bitmap used as the argument to ICall_pwrConfigACAction(), ICall_pwrRequire() and ICall_pwrDispense().
| #define ICALL_PWR_D_PERIPH_GPT2 0x00000080l |
A power API dependency flag that can be added to a bitmap used as the argument to ICall_pwrConfigACAction(), ICall_pwrRequire() and ICall_pwrDispense().
| #define ICALL_PWR_D_PERIPH_GPT3 0x00000100l |
A power API dependency flag that can be added to a bitmap used as the argument to ICall_pwrConfigACAction(), ICall_pwrRequire() and ICall_pwrDispense().
| #define ICALL_PWR_D_PERIPH_I2C0 0x00001000l |
A power API dependency flag that can be added to a bitmap used as the argument to ICall_pwrConfigACAction(), ICall_pwrRequire() and ICall_pwrDispense().
| #define ICALL_PWR_D_PERIPH_I2S 0x00020000l |
A power API dependency flag that can be added to a bitmap used as the argument to ICall_pwrConfigACAction(), ICall_pwrRequire() and ICall_pwrDispense().
| #define ICALL_PWR_D_PERIPH_RFCORE 0x00040000l |
A power API dependency flag that can be added to a bitmap used as the argument to ICall_pwrConfigACAction(), ICall_pwrRequire() and ICall_pwrDispense().
| #define ICALL_PWR_D_PERIPH_SSI0 0x00000200l |
A power API dependency flag that can be added to a bitmap used as the argument to ICall_pwrConfigACAction(), ICall_pwrRequire() and ICall_pwrDispense().
| #define ICALL_PWR_D_PERIPH_SSI1 0x00000400l |
A power API dependency flag that can be added to a bitmap used as the argument to ICall_pwrConfigACAction(), ICall_pwrRequire() and ICall_pwrDispense().
| #define ICALL_PWR_D_PERIPH_TRNG 0x00002000l |
A power API dependency flag that can be added to a bitmap used as the argument to ICall_pwrConfigACAction(), ICall_pwrRequire() and ICall_pwrDispense().
| #define ICALL_PWR_D_PERIPH_UART0 0x00000800l |
A power API dependency flag that can be added to a bitmap used as the argument to ICall_pwrConfigACAction(), ICall_pwrRequire() and ICall_pwrDispense().
| #define ICALL_PWR_D_PERIPH_UDMA 0x00008000l |
A power API dependency flag that can be added to a bitmap used as the argument to ICall_pwrConfigACAction(), ICall_pwrRequire() and ICall_pwrDispense().
| #define ICALL_PWR_D_XOSC_HF 0x00080000l |
A power API dependency flag that can be added to a bitmap used as the argument to ICall_pwrConfigACAction(), ICall_pwrRequire() and ICall_pwrDispense().
| #define ICALL_PWR_ENTER_SHUTDOWN 4 |
Power state transition to shut down power state from active power state
| #define ICALL_PWR_ENTER_STANDBY 2 |
Power state transition to standby power state from active power state.
| #define ICALL_PWR_TRANSITION_ENTERING_SLEEP 2 |
Return value of ICall_pwrGetTransitionState(). Transitioning into sleep.
| #define ICALL_PWR_TRANSITION_EXITING_SLEEP 3 |
Return value of ICall_pwrGetTransitionState(). Transitioning out of sleep.
| #define ICALL_PWR_TRANSITION_STAY_IN_ACTIVE 1 |
Return value of ICall_pwrGetTransitionState(). Power state transition not happening.
| #define ICALL_PWR_TRANSITION_UNKNOWN 0 |
Return value of ICall_pwrGetTransitionState(). Power state transition cannot be retrieved.
| #define ICALL_SERVICE_CLASS_BLE_BOARD 0x0088 |
BLE Board dependent service class.
This service is intended for BLE stack software's use only.
| #define ICALL_SERVICE_CLASS_CRYPTO 0x0080 |
Crypto service class.
Crypto service is intended for stack software to use.
| #define ICALL_SERVICE_CLASS_DUMMY 0x0100 |
Dummy stack service class enumeration. Dummy stack service is used as an example stack port on top of ICall module.
| #define ICALL_SERVICE_CLASS_DUMMY_BOARD 0x0200 |
Dummy stack board service class enumeration.
Dummy stack board service is used as an example board service for a stack.
| #define ICALL_SERVICE_CLASS_MASK 0xFFF8 |
Bit mask for recommended service id enumeration.
These bits can be used to identify a service class.
| #define ICALL_SERVICE_CLASS_PRIMITIVE 0x0008 |
Service class enumerated value for primitive service.
Primitive service includes heap service and messaging service.
| #define ICALL_SERVICE_CLASS_RADIO 0x0098 |
Radio service class.
Radio service is intended for stack software to use.
| #define ICALL_SERVICE_CLASS_TIMAC_BOARD 0x0090 |
TIMAC Board dependent service class.
This service is intended for TIMAC stack software's use only.
| #define ICALL_SERVICE_INSTANCE_MASK 0x0007 |
Bit mask for recommended service id enumeration.
These bits can be used to identify an instance among stack instances of the same service class.
| #define ICALL_STACK0_ADDR 0x00005000ul |
An entry function address of an external image. Note that it is not necessary to define this macro in this header file. The macro is internally used to expand ICALL_ADDR_MAPS and also used for the sample DummyStack code.
| #define ICALL_TASK_PRIORITIES { 5 } |
Initializer for an array of thread priorities. Each element of the array corresponds to TI-RTOS specific thread priority value given to a thread to be created per the entry function defined in ICALL_ADDR_MAPS initializer, in the same sequence.
| #define ICALL_TASK_STACK_SIZES { 1000 } |
Initializer for an array of thread stack sizes. Each element of the array corresponds to stack depth allocated to a thread to be created per the entry function defined in ICALL_ADDR_MAPS initializer, in the same sequence.
| #define ICALL_WAITMATCH_EVENT_ID Event_Id_29 |
Event reserved to signal a wait match period has ended and the caller may continue exeuction.