TI BLE5-Stack API Documentation
1.00.01.04
|
Parameter Structure for SNP_setGapParam / SNP_SET_GAP_PARAM_REQ. More...
Data Fields | |
uint16_t | paramId |
2 Byte GAP Parameter ID, GAP Parameter IDs or snpSetSecParamReq_t | |
uint16_t | value |
2 Byte Parameter Value set if for SET command | |
Parameter Structure for SNP_setGapParam / SNP_SET_GAP_PARAM_REQ.
This does not mean parameters have been changed, only that the NP has successfully sent the request.
This is a packed structure. see Dealing with Parameters and Packed Structures for more information.