![]() |
![]() |
TI BLE5-Stack API Documentation
1.00.01.04
|
Parameter Structure for response to SNP_getAttrValue / SNP_SET_ATTR_VALUE_RSP. More...
Data Fields | |
uint16_t | attrHandle |
2 Byte Attribute handle of the characteristic value. | |
uint8_t * | pData |
Pointer to data of the value to set. | |
uint8_t | status |
1 Byte Status of the request (SUCCESS or Error, list of status generated by the SNP.) | |
Parameter Structure for response to SNP_getAttrValue / SNP_SET_ATTR_VALUE_RSP.
This is a packed structure. see Dealing with Parameters and Packed Structures for more information.