![]() |
![]() |
TI BLE5-Stack API Documentation
1.00.01.04
|
Parameter Structure used to add a generic attribute descriptor (short UUID) More...
Data Fields | |
uint16_t | maxLen |
uint8_t | perms |
1 Byte Permissions of the attribute, see GATT Attribute Access Permissions Bit Fields, force to Read only | |
uint8_t | UUID [2] |
2 Byte UUID of the attribute. see dealing with UUID | |
Parameter Structure used to add a generic attribute descriptor (short UUID)
Used with snpAddCharDescDeclReq_t
This is a packed structure. see Dealing with Parameters and Packed Structures for more information.
uint16_t maxLen |
2 Byte Reserved for future use Range: 0-512
Since the characteristic value is managed only by the AP, this length field is not useful. Reserved for future use.