![]() |
![]() |
TI BLE5-Stack API Documentation
1.00.01.04
|
SNP GATT Layer API.
This file contains the interface for SNP GATT Layer.
Go to the source code of this file.
Functions | |
uint8_t | SNP_addCharValueDecl (snpAddCharValueDeclReq_t *pReq, uint8_t uuidLen, snpAddCharValueDeclRsp_t *pRsp) |
SNP Add Characteristic Value Declaration. More... | |
uint8_t | SNP_addDescriptionValue (snpAddCharDescDeclReq_t *lDescReq, snpAddCharDescDeclRsp_t *lDescRsp) |
SNP Add Characteristic Descriptor Declaration. More... | |
uint8_t | SNP_addService (snpAddServiceReq_t *pReq, uint8_t uuidLen, snpAddServiceRsp_t *pRsp) |
SNP Add Service. More... | |
uint8_t | SNP_getAttrValue (snpGetAttrValueReq_t *pReq, snpGetAttrValueRsp_t *pRsp, uint16_t *pDataLenght) |
SNP Get Attribute Value. More... | |
uint8_t | SNP_getGATTParam (snpGetGattParamReq_t *pReq, snpGetGattParamRsp_t *pRsp, uint16_t *pDataLen) |
SNP Get GATT Parameter. More... | |
uint8_t | SNP_processCharConfigUpdatedCnf (snpCharCfgUpdatedRsp_t *pReq) |
SNP Characteristic Configuration Update Confirm (0x8B) More... | |
uint8_t | SNP_readCharCnf (snpCharReadCnf_t *pReq, uint16_t dataSize) |
SNP Read Characteristic Confirmation. More... | |
uint8_t | SNP_registerService (snpRegisterServiceRsp_t *pRsp) |
SNP Register Service. More... | |
uint8_t | SNP_sendNotifInd (snpNotifIndReq_t *pCmdStruct, int16_t length) |
SNP Send Notification Indication. More... | |
uint8_t | SNP_setAttrValue (snpSetAttrValueReq_t *pReq, uint16_t dataLenght, snpSetAttrValueRsp_t *pRsp) |
SNP Set Attribute Value. More... | |
uint8_t | SNP_setGATTParam (snpSetGattParamReq_t *pReq, uint16_t reqDataLen, snpSetGattParamRsp_t *pRsp) |
SNP Set GATT Parameter. More... | |
uint8_t | SNP_writeCharCnf (snpCharWriteCnf_t *pReq) |
SNP Write Characteristic Confirmation. More... | |