![]() |
![]() |
TI BLE5-Stack API Documentation
1.00.01.04
|
Data Structures | |
struct | ugBcastCBs_t |
Set of Broadcaster callbacks - must be setup by the application. More... | |
Typedefs | |
typedef void(* | ugbAdvDoneCb_t) (bStatus_t status) |
Callback of when an Advertising Event has just been done. More... | |
typedef void(* | ugbAdvPrepareCb_t) (void) |
Callback of when the next Adverting Event is about to start. More... | |
typedef void(* | ugbStateChangeCb_t) (ugBcastState_t state) |
Callback of when the Broadcaster's state changes. More... | |
typedef void(* ugbAdvDoneCb_t) (bStatus_t status) |
Callback of when an Advertising Event has just been done.
status | status of advertising done event |
typedef void(* ugbAdvPrepareCb_t) (void) |
Callback of when the next Adverting Event is about to start.
The application can use this to update the payload if necessary
typedef void(* ugbStateChangeCb_t) (ugBcastState_t state) |
Callback of when the Broadcaster's state changes.
state | uGAP Broadcaster States |