![]() |
![]() |
TI BLE5-Stack API Documentation
1.00.01.04
|
This module implements the GAP Bond Manager For a detailed usage section describing how to send these commands and receive events, see the GAPBondMgr Section of the User's Guide. More...
Modules | |
GAP Bond Manager Callbacks | |
GAP Bond Manager Constants | |
GAP Bond Manager Structures | |
Files | |
file | gapbondmgr.h |
GAPBondMgr layer interface. | |
Functions | |
uint8 | GAPBondMgr_CheckNVLen (uint8 id, uint8 len) |
This function will check the length of a Bond Manager NV Item. More... | |
bStatus_t | GAPBondMgr_GetParameter (uint16 param, void *pValue) |
Get a GAP Bond Manager parameter. More... | |
bStatus_t | GAPBondMgr_LinkEst (uint8 addrType, uint8 *pDevAddr, uint16 connHandle, uint8 role) |
Notify the Bond Manager that a connection has been made. More... | |
void | GAPBondMgr_LinkTerm (uint16 connHandle) |
Notify the Bond Manager that a connection has been terminated. More... | |
bStatus_t | GAPBondMgr_PasscodeRsp (uint16 connectionHandle, uint8 status, uint32 passcode) |
Respond to a passcode request. More... | |
uint8 | GAPBondMgr_ProcessGAPMsg (gapEventHdr_t *pMsg) |
This is a bypass mechanism to allow the bond manager to process GAP messages. More... | |
bStatus_t | GAPBondMgr_ReadGattChar (uint16 connectionHandle, uint16 uuid) |
Send Read By Type Request to retrieve the value of a characteristic with the specified uuid. More... | |
void | GAPBondMgr_Register (gapBondCBs_t *pCB) |
Register callback functions with the bond manager. More... | |
uint8 | GAPBondMgr_ResolveAddr (uint8 addrType, uint8 *pDevAddr, uint8 *pResolvedAddr) |
Resolve an address from bonding information. More... | |
bStatus_t | GAPBondMgr_ServiceChangeInd (uint16 connectionHandle, uint8 setParam) |
Set/clear the service change indication in a bond record. More... | |
bStatus_t | GAPBondMgr_SetParameter (uint16 param, uint8 len, void *pValue) |
Set a GAP Bond Manager parameter. More... | |
void | GAPBondMgr_SlaveReqSecurity (uint16 connHandle, uint8 authReq) |
Notify the Bond Manager that a Slave Security Request is received. More... | |
uint8 | GAPBondMgr_SupportsEnhancedPriv (uint8 *pPeerIdAddr) |
Determine if peer device supports enhanced privacy by checking the Enhanced Privacy state flag of the bond record that corresponds to the peer's identity address. More... | |
bStatus_t | GAPBondMgr_syncResolvingList (void) |
This function will add all device address and IRK pairs from bond records to the Controller. Used with PRIVACY_1_2_CFG. More... | |
bStatus_t | GAPBondMgr_UpdateCharCfg (uint16 connectionHandle, uint16 attrHandle, uint16 value) |
Update the Characteristic Configuration in a bond record. More... | |
This module implements the GAP Bond Manager For a detailed usage section describing how to send these commands and receive events, see the GAPBondMgr Section of the User's Guide.
uint8 GAPBondMgr_CheckNVLen | ( | uint8 | id, |
uint8 | len | ||
) |
bStatus_t GAPBondMgr_GetParameter | ( | uint16 | param, |
void * | pValue | ||
) |
Get a GAP Bond Manager parameter.
param | - Profile parameter ID: GAP Bond Manager Parameters |
pValue | - pointer to location to get the value. This is dependent on the parameter ID and WILL be cast to the appropriate data type (example: data type of uint16 will be cast to uint16 pointer). |
bStatus_t GAPBondMgr_LinkEst | ( | uint8 | addrType, |
uint8 * | pDevAddr, | ||
uint16 | connHandle, | ||
uint8 | role | ||
) |
Notify the Bond Manager that a connection has been made.
addrType | - Device Address Type |
pDevAddr | - device's address |
connHandle | - connection handle |
role | - GAP Profile Roles |
void GAPBondMgr_LinkTerm | ( | uint16 | connHandle | ) |
Notify the Bond Manager that a connection has been terminated.
connHandle | - connection handle |
bStatus_t GAPBondMgr_PasscodeRsp | ( | uint16 | connectionHandle, |
uint8 | status, | ||
uint32 | passcode | ||
) |
Respond to a passcode request.
connectionHandle | - connection handle of the connected device or 0xFFFF if all devices in database. |
status | - SUCCESS if passcode is available, otherwise see Pairing failure status values. |
passcode | - integer value containing the passcode. |
uint8 GAPBondMgr_ProcessGAPMsg | ( | gapEventHdr_t * | pMsg | ) |
This is a bypass mechanism to allow the bond manager to process GAP messages.
pMsg | - GAP event message |
bStatus_t GAPBondMgr_ReadGattChar | ( | uint16 | connectionHandle, |
uint16 | uuid | ||
) |
Send Read By Type Request to retrieve the value of a characteristic with the specified uuid.
connectionHandle | - connection handle of the connected device |
uuid | - uuid to read. |
void GAPBondMgr_Register | ( | gapBondCBs_t * | pCB | ) |
Register callback functions with the bond manager.
pCB | - pointer to callback function structure. |
uint8 GAPBondMgr_ResolveAddr | ( | uint8 | addrType, |
uint8 * | pDevAddr, | ||
uint8 * | pResolvedAddr | ||
) |
Resolve an address from bonding information.
addrType | - Device Address Type |
pDevAddr | - peer's address |
pResolvedAddr | - pointer to buffer to put the resolved address |
bStatus_t GAPBondMgr_ServiceChangeInd | ( | uint16 | connectionHandle, |
uint8 | setParam | ||
) |
Set/clear the service change indication in a bond record.
connectionHandle | - connection handle of the connected device or 0xFFFF if all devices in database. |
setParam | - TRUE to set the service change indication, FALSE to clear it. |
bStatus_t GAPBondMgr_SetParameter | ( | uint16 | param, |
uint8 | len, | ||
void * | pValue | ||
) |
Set a GAP Bond Manager parameter.
param | - GAP Bond Manager Parameters |
len | - length of data to write |
pValue | - pointer to data to write. This is dependent on the parameter ID and WILL be cast to the appropriate data type (example: data type of uint16 will be cast to uint16 pointer). |
void GAPBondMgr_SlaveReqSecurity | ( | uint16 | connHandle, |
uint8 | authReq | ||
) |
Notify the Bond Manager that a Slave Security Request is received.
connHandle | - connection handle |
authReq | - slave device's authentication requirements |
uint8 GAPBondMgr_SupportsEnhancedPriv | ( | uint8 * | pPeerIdAddr | ) |
Determine if peer device supports enhanced privacy by checking the Enhanced Privacy state flag of the bond record that corresponds to the peer's identity address.
pPeerIdAddr | - peer identity address |
bStatus_t GAPBondMgr_syncResolvingList | ( | void | ) |
bStatus_t GAPBondMgr_UpdateCharCfg | ( | uint16 | connectionHandle, |
uint16 | attrHandle, | ||
uint16 | value | ||
) |
Update the Characteristic Configuration in a bond record.
connectionHandle | - connection handle of the connected device or 0xFFFF if all devices in database. |
attrHandle | - attribute handle. |
value | - characteristic configuration value. |