Elliptic Curve Cryptography driver.
More...
|
file | ECCROMCC26XX.h |
| ECC ROM driver implementation for a CC26XX device.
|
|
|
int8_t | ECCROMCC26XX_genDHKey (uint8_t *privateKey, uint8_t *publicKeyX, uint8_t *publicKeyY, uint8_t *dHKeyX, uint8_t *dHKeyY, ECCROMCC26XX_Params *params) |
| Generate Diffie-Hellman Shared Secret Key X and Y Coordinates. More...
|
|
int8_t | ECCROMCC26XX_genKeys (uint8_t *privateKey, uint8_t *publicKeyX, uint8_t *publicKeyY, ECCROMCC26XX_Params *params) |
| Generate Public Key X and Y Coordinates. More...
|
|
void | ECCROMCC26XX_init (void) |
| Initializes module's synchronization resources. Only needs to be called once, but safe to call multiple times. More...
|
|
void | ECCROMCC26XX_Params_init (ECCROMCC26XX_Params *params) |
| Function to initialize the ECCROMCC26XX_Params struct to its defaults. params should not be modified until after this function is called. Default parameters use the NIST P-256 curve, timeout is set to wait indefinitely, malloc and free are NULL and status is set to ECCROMCC26XX_STATUS_SUCCESS. A client may call this function with the same params instance any number of times. More...
|
|
Elliptic Curve Cryptography driver.
To use the ECC driver in your application you need to:
§ ECCROMCC26XX_NIST_P256_KEY_LEN_IN_BYTES
#define ECCROMCC26XX_NIST_P256_KEY_LEN_IN_BYTES 32 |
ECC key length in bytes for NIST P-256 keys.
§ ECCROMCC26XX_NIST_P256_WORKZONE_LEN_IN_BYTES
#define ECCROMCC26XX_NIST_P256_WORKZONE_LEN_IN_BYTES 684 |
ECC Workzone length in bytes for NIST P-256 key and shared secret generation. For use with ECC Window Size 3 only. Used to store intermediary values in ECC calculations.
§ ECCROMCC26XX_WORKZONE_LEN_IN_BYTES
#define ECCROMCC26XX_WORKZONE_LEN_IN_BYTES |
( |
|
len, |
|
|
|
win |
|
) |
| (4 * ((13 * (len)) + 13 + (3 * (len) * (1 << ((win) - 2))))) |
Compute ECC workzone length in bytes for a generic key length and window size.
len is the length of the key in uint32_t blocks. it must not exceed 255 blocks in length. win is the window size, such that 1 < win < 6. Recommended setting is 3.
This workzone length is only valid for key and shared secret and signature generation. A different workzone length would be used for verification.
§ ECCROMCC26XX_CurveParams
ECCROMCC26XX Curve Parameters.
This holds the ECC Curve information to be used. Offset 0 of each param_* buffer contains the length of each parameter in uint32_t blocks, not including the first offset.
§ ECCROMCC26XX_FreeCB
typedef void(* ECCROMCC26XX_FreeCB) (uint8_t *pBuf) |
ECCROMCC26XX Free Callback.
Required to free temporary key buffers during operation.
- Parameters
-
pBuf | - pointer to buffer to free. |
- Returns
- none
§ ECCROMCC26XX_MallocCB
typedef uint8_t*(* ECCROMCC26XX_MallocCB) (uint16_t len) |
ECCROMCC26XX Malloc Callback.
Required to malloc temporary key buffers during operation.
- Parameters
-
len | - length in bytes of buffer to malloc. |
- Returns
- pointer to allocated buffer
§ ECCROMCC26XX_Params
ECCROMCC26XX Parameters.
Holds a client's parameters for performing an ECC operation.
§ ECCROMCC26XX_genDHKey()
int8_t ECCROMCC26XX_genDHKey |
( |
uint8_t * |
privateKey, |
|
|
uint8_t * |
publicKeyX, |
|
|
uint8_t * |
publicKeyY, |
|
|
uint8_t * |
dHKeyX, |
|
|
uint8_t * |
dHKeyY, |
|
|
ECCROMCC26XX_Params * |
params |
|
) |
| |
Generate Diffie-Hellman Shared Secret Key X and Y Coordinates.
- Precondition
- ECCROMCC26XX_init must be called prior to this and params must be intiliazed with ECCROMCC26XX_Params_init(). Calling context: Task. Swi or Hwi should call only when timeout is set to 0.
- Parameters
-
privateKey | 32 byte input buffer of randomly generated bits. Note, you need to reverse the byte order of this byte array. (Starting with least significant byte) |
publicKeyX | 32 byte input buffer provided by client to store Public Key X Coordinate. Note, you need to reverse the byte order of this byte array. (Starting with least significant byte) |
publicKeyY | 32 byte input buffer provided by client to store Public Key Y Coordinate. Note, you need to reverse the byte order of this byte array. (Starting with least significant byte) |
dHKeyX | 32 byte output buffer provided by client to store Diffie-Hellman Key X Coordinate. Note, you need to reverse the byte order of this byte array. (Starting with least significant byte) |
dHKeyY | 32 byte output buffer provided by client to store Diffie-Hellman Key Y Coordinate. Note, you need to reverse the byte order of this byte array. (Starting with least significant byte) |
params | Pointer to a parameter block, if NULL operation will fail |
- Returns
- status
§ ECCROMCC26XX_genKeys()
int8_t ECCROMCC26XX_genKeys |
( |
uint8_t * |
privateKey, |
|
|
uint8_t * |
publicKeyX, |
|
|
uint8_t * |
publicKeyY, |
|
|
ECCROMCC26XX_Params * |
params |
|
) |
| |
Generate Public Key X and Y Coordinates.
- Precondition
- ECCROMCC26XX_init must be called prior to this and params must be intiliazed with ECCROMCC26XX_Params_init(). Calling context: Task. Swi or Hwi should call only when timeout is set to 0.
- Parameters
-
privateKey | 32 byte input buffer of randomly generated bits. This key needs to contain the length (4 bytes) and the private key in a byte-wise little endian format. |
publicKeyX | 32 byte output buffer provided by client to store Public Key X Coordinate. This key needs to contain the length (4 bytes) and the private key in a byte-wise little endian format. |
publicKeyY | 32 byte output buffer provided by client to store Public Key Y Coordinate. This key needs to contain the length (4 bytes) and the private key in a byte-wise little endian format. |
params | Pointer to a parameter block, if NULL operation will fail. |
- Returns
- status
§ ECCROMCC26XX_init()
void ECCROMCC26XX_init |
( |
void |
| ) |
|
Initializes module's synchronization resources. Only needs to be called once, but safe to call multiple times.
- Precondition
- This function must be called before any other ECCROMCC26XX driver APIs. Calling context: Task.
§ ECCROMCC26XX_Params_init()
Function to initialize the ECCROMCC26XX_Params struct to its defaults. params should not be modified until after this function is called. Default parameters use the NIST P-256 curve, timeout is set to wait indefinitely, malloc and free are NULL and status is set to ECCROMCC26XX_STATUS_SUCCESS. A client may call this function with the same params instance any number of times.
- Precondition
- Calling context: Hwi, Swi and Task.
- Parameters
-
params | Parameter structure to initialize. |