![]() |
![]() |
|
Z-Stack API Reference
7.40.00.20
|
This group defines the IDs for the Protocol Interfaces Clusters defined in the ZCL v7 specification. More...
This group defines the IDs for the Protocol Interfaces Clusters defined in the ZCL v7 specification.
| #define ZCL_CLUSTER_ID_GENERAL_PARTITION 0x0016 |
Partition Cluster. The commands and attributes for enabling partitioning of a large frame between devices.
| #define ZCL_CLUSTER_ID_PI_11073_PROTOCOL_TUNNEL 0x0614 |
11073 Protocol Tunnel Cluster. Interface for 11073 Protocol Tunnel used in health care applications
| #define ZCL_CLUSTER_ID_PI_ANALOG_INPUT_BACNET_EXT 0x0603 |
Analog input (BACnet extended). An interface for accessing a number of BACnet based attributes of an analog measurement.
| #define ZCL_CLUSTER_ID_PI_ANALOG_INPUT_BACNET_REG 0x0602 |
Analog input (BACnet regular) Cluster. An interface for accessing a number of commonly used BACnet based attributes of an analog measurement.
| #define ZCL_CLUSTER_ID_PI_ANALOG_OUTPUT_BACNET_EXT 0x0605 |
Analog output (BACnet extended) Cluster. An interface for accessing a number of BACnet based attributes of an analog output.
| #define ZCL_CLUSTER_ID_PI_ANALOG_OUTPUT_BACNET_REG 0x0604 |
Analog output (BACnet regular). An interface for accessing a number of commonly used BACnet based attributes of an analog output.
| #define ZCL_CLUSTER_ID_PI_ANALOG_VALUE_BACNET_EXT 0x0607 |
Analog value(BACnet extended) Cluster. An interface for accessing a number of BACnet based attributes of an analog value, typically used as a control system parameter.
| #define ZCL_CLUSTER_ID_PI_ANALOG_VALUE_BACNET_REG 0x0606 |
Analog value(BACnet regular) Cluster. An interface for accessing a number of commonly used BACnet based attributes of an analog value, typically used as a control system parameter.
| #define ZCL_CLUSTER_ID_PI_BACNET_PROTOCOL_TUNNEL 0x0601 |
BACnet protocol tunnel Cluster. Commands and attributes required to tunnel the BACnet protocol.
| #define ZCL_CLUSTER_ID_PI_BINARY_INPUT_BACNET_EXT 0x0609 |
Binary input (BACnet extended) Cluster. An interface for accessing a number of BACnet based attributes of a binary measurement.
| #define ZCL_CLUSTER_ID_PI_BINARY_INPUT_BACNET_REG 0x0608 |
Binary input (BACnet regular) Cluster. An interface for accessing a number of commonly used BACnet based attributes of a binary measurement.
| #define ZCL_CLUSTER_ID_PI_BINARY_OUTPUT_BACNET_EXT 0x060B |
Binary output (BACnet extended) Cluster. An interface for accessing a number of BACnet based attributes of a binary output.
| #define ZCL_CLUSTER_ID_PI_BINARY_OUTPUT_BACNET_REG 0x060A |
Binary output (BACnet regular) Cluster. An interface for accessing a number of commonly used BACnet based attributes of a binary output.
| #define ZCL_CLUSTER_ID_PI_BINARY_VALUE_BACNET_EXT 0x060D |
Binary value (BACnet extended) Cluster. An interface for accessing a number of BACnet based attributes of a binary value, typically used as a control system parameter.
| #define ZCL_CLUSTER_ID_PI_BINARY_VALUE_BACNET_REG 0x060C |
Binary value (BACnet regular) Cluster. An interface for accessing a number of commonly used BACnet based attributes of a binary value, typically used as a control system parameter.
| #define ZCL_CLUSTER_ID_PI_GENERIC_TUNNEL 0x0600 |
Generic tunnel Cluster. The minimum common commands and attributes required to tunnel any protocol.
| #define ZCL_CLUSTER_ID_PI_ISO7818_PROTOCOL_TUNNEL 0x0615 |
ISO7816 Tunnel Cluster. Commands and attributes for mobile office solutions using devices.
| #define ZCL_CLUSTER_ID_PI_MULTISTATE_INPUT_BACNET_EXT 0x060F |
Multistate input (BACnet extended) Cluster. An interface for accessing a number of BACnet based attributes of a multistate measurement.
| #define ZCL_CLUSTER_ID_PI_MULTISTATE_INPUT_BACNET_REG 0x060E |
Multistate input (BACnet regular) Cluster. An interface for accessing a number of commonly used BACnet based attributes of a multistate measurement.
| #define ZCL_CLUSTER_ID_PI_MULTISTATE_OUTPUT_BACNET_EXT 0x0611 |
Multistate output (BACnet extended) Cluster. An interface for accessing a number of BACnet based attributes of a multistate output.
| #define ZCL_CLUSTER_ID_PI_MULTISTATE_OUTPUT_BACNET_REG 0x0610 |
Multistate output (BACnet regular) Cluster. An interface for accessing a number of commonly used BACnet based attributes of a multistate output.
| #define ZCL_CLUSTER_ID_PI_MULTISTATE_VALUE_BACNET_EXT 0x0613 |
Multistate value (BACnet extended) Cluster. An interface for accessing a number of BACnet based attributes of a multistate value, typically used as a control system parameter.
| #define ZCL_CLUSTER_ID_PI_MULTISTATE_VALUE_BACNET_REG 0x0612 |
Multistate value (BACnet regular) Cluster. An interface for accessing a number of commonly used BACnet based attributes of a multistate value, typically used as a control system parameter.