#include <stdbool.h>#include <stdint.h>#include "../inc/hw_types.h"#include "../inc/hw_flash.h"#include "../inc/hw_memmap.h"#include "../inc/hw_ints.h"#include "../inc/hw_aon_pmctl.h"#include "../inc/hw_fcfg1.h"#include "interrupt.h"#include "debug.h"Macros | |
| #define | FAPI_STATUS_SUCCESS 0x00000000 |
| #define | FAPI_STATUS_FSM_BUSY 0x00000001 |
| #define | FAPI_STATUS_FSM_READY 0x00000002 |
| #define | FAPI_STATUS_INCORRECT_DATABUFFER_LENGTH 0x00000003 |
| #define | FAPI_STATUS_FSM_ERROR 0x00000004 |
| #define | FLASH_INT_FSM_DONE 0x00400000 |
| #define | FLASH_INT_RV 0x00010000 |
| #define | FLASH_PWR_ACTIVE_MODE 0x00000000 |
| #define | FLASH_PWR_OFF_MODE 0x00000001 |
| #define | FLASH_PWR_DEEP_STDBY_MODE 0x00000002 |
| #define | FLASH_NO_PROTECT 0x00000000 |
| #define | FLASH_WRITE_PROTECT 0x00000001 |
| #define | ADDR_OFFSET (0x1F800000 - FLASHMEM_BASE) |
| #define | FCFG1_OFFSET 0x1000 |
| #define | FLASH_MODULE_CLK_FREQ 48 |
| #define | FSM_REG_WRT_ENABLE 5 |
| #define | FSM_REG_WRT_DISABLE 2 |
| #define | FBFALLBACK_SLEEP 0 |
| #define | FBFALLBACK_DEEP_STDBY 1 |
| #define | FBFALLBACK_ACTIVE 3 |
| #define | FLASH_BAGP 0x14 |
| #define | FLASH_PAGP 0x14 |
| #define | PATTERN_BITS 0x20 |
| #define | FW_WRT_TRIMMED 0x00000001 |
| #define | FW_PWRMODE_DEPRECATED 0x00000002 |
| #define | FWPWRITE_BYTE_ADDRESS ((tFwpWriteByte *)((FLASH_BASE + FLASH_O_FWPWRITE0))) |
| #define | DUMPWORD_INSTR 0x04 |
| #define | FLASH_CMD_EXEC 0x15 |
Typedefs | |
| typedef volatile uint8_t | tFwpWriteByte |
Enumerations | |
| enum | tFlashStateCommandsType { FAPI_PROGRAM_DATA = 0x0002, FAPI_ERASE_SECTOR = 0x0006, FAPI_ERASE_BANK = 0x0008, FAPI_VALIDATE_SECTOR = 0x000E, FAPI_CLEAR_STATUS = 0x0010, FAPI_PROGRAM_RESUME = 0x0014, FAPI_ERASE_RESUME = 0x0016, FAPI_CLEAR_MORE = 0x0018, FAPI_PROGRAM_SECTOR = 0x0020, FAPI_ERASE_OTP = 0x0030 } |
| Defined values for Flash State Machine commands. More... | |
Functions | |
| static uint32_t | FlashSectorSizeGet (void) |
| Get size of a flash sector in number of bytes. More... | |
| static uint32_t | FlashSizeGet (void) |
| Get the size of the flash. More... | |
| void | FlashPowerModeSet (uint32_t ui32PowerMode, uint32_t ui32BankGracePeriod, uint32_t ui32PumpGracePeriod) |
| Set power mode. More... | |
| uint32_t | FlashPowerModeGet (void) |
| Get current configured power mode. More... | |
| void | FlashProtectionSet (uint32_t ui32SectorAddress, uint32_t ui32ProtectMode) |
| Set sector protection. More... | |
| uint32_t | FlashProtectionGet (uint32_t ui32SectorAddress) |
| Get sector protection. More... | |
| uint32_t | FlashProtectionSave (uint32_t ui32SectorAddress) |
| Save sector protection to make it permanent. More... | |
| static uint32_t | FlashCheckFsmForError (void) |
| Checks if the Flash state machine has detected an error. More... | |
| static uint32_t | FlashCheckFsmForReady (void) |
| Checks if the Flash state machine is ready. More... | |
| static void | FlashIntRegister (void(*pfnHandler)(void)) |
| Registers an interrupt handler for the flash interrupt in the dynamic interrupt table. More... | |
| static void | FlashIntUnregister (void) |
| Unregisters the interrupt handler for the flash interrupt in the dynamic interrupt table. More... | |
| static void | FlashIntEnable (uint32_t ui32IntFlags) |
| Enables flash controller interrupt sources. More... | |
| static void | FlashIntDisable (uint32_t ui32IntFlags) |
| Disables individual flash controller interrupt sources. More... | |
| static uint32_t | FlashIntStatus (void) |
| Gets the current interrupt status. More... | |
| static void | FlashIntClear (uint32_t ui32IntFlags) |
| Clears flash controller interrupt source. More... | |
| uint32_t | FlashSectorErase (uint32_t ui32SectorAddress) |
| Erase a flash sector. More... | |
| uint32_t | FlashProgram (uint8_t *pui8DataBuffer, uint32_t ui32Address, uint32_t ui32Count) |
| Programs unprotected flash sectors in the main bank. More... | |
| bool | FlashEfuseReadRow (uint32_t *pui32EfuseData, uint32_t ui32RowAddress) |
| Reads efuse data from specified row. More... | |
| void | FlashDisableSectorsForWrite (void) |
| Disables all sectors for erase and programming on the active bank. More... | |