![]() |
![]() |
SYS/BIOS
7.00
|
Cortex V8M TimestampProvider.
The SysTick timer is used as the timestamp source.
Function | Hwi | Swi | Task | Main** | Startup*** |
---|---|---|---|---|---|
get32 | Y | Y | Y | Y | N |
get64 | Y | Y | Y | Y | N |
getFreq | Y | Y | Y | Y | N |
#include <xdc/std.h>
#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
#include <ti/sysbios/runtime/Types.h>
#include <ti/sysbios/family/arm/v8m/Timer.h>
#include "TimestampProvider_defs.h"
Go to the source code of this file.
Functions | |
uint32_t | TimestampProvider_get32 (void) |
Return a 32-bit timestamp. More... | |
void | TimestampProvider_get64 (Types_Timestamp64 *timestamp64) |
Return a 64-bit timestamp. More... | |
void | TimestampProvider_getFreq (Types_FreqHz *freq) |
Get the timestamp timer's frequency (in Hz) More... | |
uint32_t TimestampProvider_get32 | ( | void | ) |
Return a 32-bit timestamp.
Returns a 32-bit timestamp value. Use TimestampProvider_getFreq to convert this value into units of real time.
32-bit | timestamp |
void TimestampProvider_get64 | ( | Types_Timestamp64 * | timestamp64 | ) |
Return a 64-bit timestamp.
This parameter is a pointer to a structure representing a 64-bit wide timestamp value where the current timestamp is written.
If the underlying hardware does not support 64-bit resolution, the hi
field of result
is always set to 0 So, it is possible for the lo
field to wrap around without any change to the hi
field. Use TimestampProvider_getFreq to convert this value into units of real time.
timestamp64 | pointer to 64-bit result |
void TimestampProvider_getFreq | ( | Types_FreqHz * | freq | ) |
Get the timestamp timer's frequency (in Hz)
This parameter is a pointer to a structure representing a 64-bit wide frequency value where the timer's frequency (in Hz) is written This function provides a way of converting timestamp values into units of real time.
freq | pointer to a 64-bit result |