#include </home/developer/.conan/data/tirtos/7.05.00.01/library-sb/ga/build/5ab84d6acfe1f23c4fae0ab88f26e3a396351ac9/kernel/tirtos7/packages/ti/sysbios/knl/Task.h>
§ priority
§ stack
Task stack pointer. Default = null.
Null indicates that the stack is to be allocated by create().
§ stackSize
size_t Task_Stat::stackSize |
§ stackHeap
IHeap_Handle Task_Stat::stackHeap |
Mem heap used for dynamically created task stack.
The default value of NULL means that BIOS heap is used.
§ env
Global environment struct.
§ mode
§ sp
Task's current stack pointer.
§ used
The documentation for this struct was generated from the following file:
- /home/developer/.conan/data/tirtos/7.05.00.01/library-sb/ga/build/5ab84d6acfe1f23c4fae0ab88f26e3a396351ac9/kernel/tirtos7/packages/ti/sysbios/knl/Task.h