SYS/BIOS
7.00
|
Data Fields | |
Semaphore_Mode | mode |
Semaphore mode. More... | |
Event_Handle | event |
Event instance to use if non-NULL. More... | |
unsigned int | eventId |
eventId if using Events More... | |
Semaphore_Mode Semaphore_Params::mode |
Semaphore mode.
When mode is BINARY, the semaphore has only two states, available and unavailable. When mode is COUNTING, the semaphore keeps track of number of times a semaphore is posted.
The default for this parameter is COUNTING.
Event_Handle Semaphore_Params::event |
Event instance to use if non-NULL.
The default value of this parameter is null. If event is non-null:
unsigned int Semaphore_Params::eventId |
eventId if using Events
The default for this parameters is 1.