#include </home/developer/.conan/data/tirtos/7.05.00.01/library-sb/ga/build/5ab84d6acfe1f23c4fae0ab88f26e3a396351ac9/kernel/tirtos7/packages/ti/sysbios/knl/Clock.h>
§ objElem
§ timeout
uint32_t Clock_Struct::timeout |
§ currTimeout
uint32_t Clock_Struct::currTimeout |
§ period
uint32_t Clock_Struct::period |
Period of this instance (in clock ticks)
This parameter is used to set the subsequent timeout interval (in Clock ticks) for periodic instances.
The default value of this parameter is 0, which indicates this is a one- shot Clock object.
A non zero value for this parameter specifies that the Clock object is to be called periodically, and also specifies the rate (in Clock ticks) that the Clock function will be called AFTER the initial 'timeout' argument period.
For one-shot Clock instances, this parameter must be set to zero.
§ active
volatile bool Clock_Struct::active |
§ fxn
§ arg
uintptr_t Clock_Struct::arg |
Uninterpreted argument passed to instance function.
The default is null.
§ timeoutTicks
uint32_t Clock_Struct::timeoutTicks |
The documentation for this struct was generated from the following file:
- /home/developer/.conan/data/tirtos/7.05.00.01/library-sb/ga/build/5ab84d6acfe1f23c4fae0ab88f26e3a396351ac9/kernel/tirtos7/packages/ti/sysbios/knl/Clock.h