SYS/BIOS  7.00
Data Structures | Macros | Typedefs | Functions
GateMutex.h File Reference

Detailed Description

Mutex Gate.

GateMutex uses a Semaphore as the resource locking mechanism. Each GateMutex instance has its own unique Semaphore. This gate can only be used by a Task as a gate can potentially block. This gate cannot be used by a Hwi or Swi.

The task that uses a gate can call enter() any number of times without risk of being blocked, although relinquishing ownership of the gate requires a balanced number of calls to leave().

Calling Context

Function Hwi Swi Task Main Startup
Params_init Y Y Y Y Y
query Y Y Y Y Y
construct N N Y Y N
create N* N* Y Y N
delete N* N* Y Y N
destruct N N Y Y N
enter N N Y N N
leave N N Y N N
Definitions:
  • Hwi: API is callable from a Hwi thread.
  • Swi: API is callable from a Swi thread.
  • Task: API is callable from a Task thread.
  • Main: API is callable during any of these phases:
    • In your module startup after this module is started (e.g. GateMutex_Module_startupDone() returns true).
    • During xdc.runtime.Startup.lastFxns.
    • During main().
    • During BIOS.startupFxns.
  • Startup: API is callable during any of these phases:
    • During xdc.runtime.Startup.firstFxns.
    • In your module startup before this module is started (e.g. GateMutex_Module_startupDone() returns false).
  • *: Assuming blocking Heap is used for creation.
  • **: Must be used in enter/leave pairs.

#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
#include <ti/sysbios/knl/Queue.h>
#include <ti/sysbios/knl/Semaphore.h>
#include <ti/sysbios/knl/Task.h>
#include <ti/sysbios/runtime/Error.h>
Include dependency graph for GateMutex.h:

Go to the source code of this file.

Data Structures

struct  GateMutex_Params
 
struct  GateMutex_Struct
 

Macros

#define GateMutex_A_badContext   "bad calling context"
 Assert when GateMutex_enter() is not called from correct context. GateMutex_enter() can only be called from main() or Task context (not Hwi or Swi). More...
 

Typedefs

typedef struct GateMutex_Params GateMutex_Params
 
typedef struct GateMutex_Struct GateMutex_Struct
 
typedef struct GateMutex_Struct GateMutex_Object
 
typedef GateMutex_ObjectGateMutex_Handle
 

Functions

bool GateMutex_canBePreempted (void)
 query Gate 'preempt' characteristics More...
 
bool GateMutex_canBlock (void)
 query Gate 'blocking' characteristics More...
 
GateMutex_Handle GateMutex_create (const GateMutex_Params *prms, Error_Block *eb)
 Create a GateMutex gate. More...
 
GateMutex_Handle GateMutex_construct (GateMutex_Struct *obj, const GateMutex_Params *prms)
 Construct a GateMutex gate. More...
 
void GateMutex_delete (GateMutex_Handle *gate)
 Delete a GateMutex gate. More...
 
void GateMutex_destruct (GateMutex_Struct *obj)
 Destruct a GateMutex gate. More...
 
void GateMutex_Params_init (GateMutex_Params *prms)
 Initialize the GateMutex_Params structure with default values. More...
 
intptr_t GateMutex_enter (GateMutex_Handle gate)
 enter the GateMutex gate More...
 
void GateMutex_leave (GateMutex_Handle gate, intptr_t key)
 leave the GateMutex gate More...
 
GateMutex_Handle GateMutex_Object_first (void)
 return handle of the first GateMutex on GateMutex list More...
 
GateMutex_Handle GateMutex_Object_next (GateMutex_Handle gate)
 return handle of the next GateMutex on GateMutex list More...
 

Macro Definition Documentation

§ GateMutex_A_badContext

#define GateMutex_A_badContext   "bad calling context"

Assert when GateMutex_enter() is not called from correct context. GateMutex_enter() can only be called from main() or Task context (not Hwi or Swi).

Common causes and workarounds for hitting this Assert:

  • Calling printf() from a Hwi or Swi thread. Use System_printf (with SysMin) instead.
  • Calling Memory_alloc() from a Hwi or Swi thread. Use a different Heap manager or change the memory manager's gate type.

Typedef Documentation

§ GateMutex_Params

§ GateMutex_Struct

§ GateMutex_Object

§ GateMutex_Handle

Function Documentation

§ GateMutex_canBePreempted()

bool GateMutex_canBePreempted ( void  )

query Gate 'preempt' characteristics

GateMutex can be preempted. This API always returns true.

Return values
true

§ GateMutex_canBlock()

bool GateMutex_canBlock ( void  )

query Gate 'blocking' characteristics

GateMutex enter can block if another task owns the gate. This API always returns true.

Return values
true

§ GateMutex_create()

GateMutex_Handle GateMutex_create ( const GateMutex_Params prms,
Error_Block eb 
)

Create a GateMutex gate.

Parameters
prmsoptional parameters
eberror block
Return values
GateMutexhandle (NULL on failure)

§ GateMutex_construct()

GateMutex_Handle GateMutex_construct ( GateMutex_Struct obj,
const GateMutex_Params prms 
)

Construct a GateMutex gate.

GateMutex_construct is equivalent to GateMutex_create except that the GateMutex_Struct is pre-allocated.

Parameters
objpointer to a GateMutex object
prmsoptional parameters
Return values
GateMutexhandle (NULL on failure)

§ GateMutex_delete()

void GateMutex_delete ( GateMutex_Handle gate)

Delete a GateMutex gate.

Note that GateMutex_delete takes a pointer to a GateMutex_Handle which enables GateMutex_delete to set the GateMutex handle to NULL.

Parameters
gatepointer to a GateMutex handle

§ GateMutex_destruct()

void GateMutex_destruct ( GateMutex_Struct obj)

Destruct a GateMutex gate.

Parameters
objpointer to a GateMutex objects

§ GateMutex_Params_init()

void GateMutex_Params_init ( GateMutex_Params prms)

Initialize the GateMutex_Params structure with default values.

GateMutex_Params_init initializes the GateMutex_Params structure with default values. GateMutex_Params_init should always be called before setting individual parameter fields. This allows new fields to be added in the future with compatible defaults – existing source code does not need to change when new fields are added.

Parameters
prmspointer to uninitialized params structure

§ GateMutex_enter()

intptr_t GateMutex_enter ( GateMutex_Handle  gate)

enter the GateMutex gate

GateMutex_enter enters the GateMutex gate and returns a key for use by GateMutex_enter. GateMutex_enter calls can be nested and the key is used to unlock the gate on the final call to GateMutex_leave.

Parameters
gateGateMutex handle
Return values
opaquekey to be passed to GateMutex_leave()

§ GateMutex_leave()

void GateMutex_leave ( GateMutex_Handle  gate,
intptr_t  key 
)

leave the GateMutex gate

GateMutex_leave exits the GateMutex gate if key matches the outermost call to GateMutex_enter. If GateMutex_enter calls are nested, the key will keep the nested calls from leaving the gate.

Parameters
gateGateMutex handle
keyopaque key to unlock the gate

§ GateMutex_Object_first()

GateMutex_Handle GateMutex_Object_first ( void  )

return handle of the first GateMutex on GateMutex list

Return the handle of the first GateMutex on the create/construct list. NULL if no GateMutex instances have been created or constructed.

Return values
GateMutexhandle

§ GateMutex_Object_next()

GateMutex_Handle GateMutex_Object_next ( GateMutex_Handle  gate)

return handle of the next GateMutex on GateMutex list

Return the handle of the next GateMutex on the create/construct list. NULL if no more GateMutexs are on the list.

Parameters
gateGateMutex handle
Return values
GateMutexhandle
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale