SYS/BIOS  7.00
Data Structures | Typedefs | Functions
GateHwi.h File Reference

Detailed Description

Hardware Interrupt Gate.

GateHwi uses disabling and enabling of interrupts as the resource locking mechanism. Such a gate guarantees exclusive access to the CPU. This gate can be used whenever the resource is being shared by Tasks, Swis, and/or Hwis.

The duration between the enter and leave should be as short as possible to minimize Hwi latency.

GateHwi inherits from xdc.runtime.IGateProvider, therefore supports nesting.

Calling Context

Function Hwi Swi Task Main Startup
Params_init Y Y Y Y Y
query Y Y Y Y Y
construct Y Y Y Y N
create N* N* Y Y N
delete N* N* Y Y N
destruct Y Y Y Y N
enter Y Y Y Y** Y**
leave Y Y Y Y** Y**
Definitions:
  • Hwi: API is callable from a Hwi thread.
  • Swi: API is callable from a Swi thread.
  • Task: API is callable from a Task thread.
  • Main: API is callable during any of these phases:
    • In your module startup after this module is started (e.g. GateHwi_Module_startupDone() returns true).
    • During xdc.runtime.Startup.lastFxns.
    • During main().
    • During BIOS.startupFxns.
  • Startup: API is callable during any of these phases:
    • During xdc.runtime.Startup.firstFxns.
    • In your module startup before this module is started (e.g. GateHwi_Module_startupDone() returns false).
  • *: Assuming blocking Heap is used for creation.
  • **: Must be used in enter/leave pairs.

#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
#include <ti/sysbios/runtime/Error.h>
Include dependency graph for GateHwi.h:

Go to the source code of this file.

Data Structures

struct  GateHwi_Params
 
struct  GateHwi_Struct
 

Typedefs

typedef struct GateHwi_Params GateHwi_Params
 
typedef struct GateHwi_Struct GateHwi_Struct
 
typedef struct GateHwi_Struct GateHwi_Object
 
typedef GateHwi_ObjectGateHwi_Handle
 

Functions

bool GateHwi_canBePreempted (void)
 query Gate 'preempt' characteristics More...
 
bool GateHwi_canBlock (void)
 query Gate 'blocking' characteristics More...
 
GateHwi_Handle GateHwi_create (const GateHwi_Params *prms, Error_Block *eb)
 Create a GateHwi gate. More...
 
GateHwi_Handle GateHwi_construct (GateHwi_Struct *obj, const GateHwi_Params *prms)
 Construct a GateHwi gate. More...
 
void GateHwi_delete (GateHwi_Handle *gate)
 Delete a GateHwi gate. More...
 
void GateHwi_destruct (GateHwi_Struct *obj)
 Destruct a GateHwi gate. More...
 
void GateHwi_Params_init (GateHwi_Params *prms)
 Initialize the GateHwi_Params structure with default values. More...
 
intptr_t GateHwi_enter (GateHwi_Handle gate)
 enter the GateHwi gate More...
 
void GateHwi_leave (GateHwi_Handle gate, intptr_t key)
 leave the GateHwi gate More...
 

Typedef Documentation

§ GateHwi_Params

§ GateHwi_Struct

§ GateHwi_Object

§ GateHwi_Handle

Function Documentation

§ GateHwi_canBePreempted()

bool GateHwi_canBePreempted ( void  )

query Gate 'preempt' characteristics

GateHwi cannot be preempted. This API always returns false.

Return values
false

§ GateHwi_canBlock()

bool GateHwi_canBlock ( void  )

query Gate 'blocking' characteristics

GateHwi enter will never block. This API always returns false.

Return values
false

§ GateHwi_create()

GateHwi_Handle GateHwi_create ( const GateHwi_Params prms,
Error_Block eb 
)

Create a GateHwi gate.

Parameters
prmsoptional parameters
eberror block
Return values
GateHwihandle (NULL on failure)

§ GateHwi_construct()

GateHwi_Handle GateHwi_construct ( GateHwi_Struct obj,
const GateHwi_Params prms 
)

Construct a GateHwi gate.

GateHwi_construct is equivalent to GateHwi_create except that the GateHwi_Struct is pre-allocated.

Parameters
objpointer to a GateHwi object
prmsoptional parameters
Return values
GateHwihandle (NULL on failure)

§ GateHwi_delete()

void GateHwi_delete ( GateHwi_Handle gate)

Delete a GateHwi gate.

Note that GateHwi_delete takes a pointer to a GateHwi_Handle which enables GateHwi_delete to set the GateHwi handle to NULL.

Parameters
gatepointer to a GateHwi handle

§ GateHwi_destruct()

void GateHwi_destruct ( GateHwi_Struct obj)

Destruct a GateHwi gate.

Parameters
objpointer to a GateHwi objects

§ GateHwi_Params_init()

void GateHwi_Params_init ( GateHwi_Params prms)

Initialize the GateHwi_Params structure with default values.

GateHwi_Params_init initializes the GateHwi_Params structure with default values. GateHwi_Params_init should always be called before setting individual parameter fields. This allows new fields to be added in the future with compatible defaults – existing source code does not need to change when new fields are added.

Parameters
prmspointer to uninitialized params structure

§ GateHwi_enter()

intptr_t GateHwi_enter ( GateHwi_Handle  gate)

enter the GateHwi gate

GateHwi_enter enters the GateHwi gate and returns a key for use by GateHwi_enter. GateHwi_enter calls can be nested and the key is used to unlock the gate on the final call to GateHwi_leave.

Parameters
gateGateHwi handle
Return values
opaquekey to be passed to GateHwi_leave()

§ GateHwi_leave()

void GateHwi_leave ( GateHwi_Handle  gate,
intptr_t  key 
)

leave the GateHwi gate

GateHwi_leave exits the GateHwi gate if key matches the outermost call to GateHwi_enter. If GateHwi_enter calls are nested, the key will keep the nested calls from leaving the gate.

Parameters
gateGateHwi handle
keyopaque key to unlock the gate
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale