![]() |
![]() |
rflib
|
#include <rf_bt5_iq_autocopy.h>
Data Fields | |
struct { | |
uint8_t bCrcErr:1 | |
1 if the samples came from a packet received with CRC error; 0 otherwise More... | |
uint8_t bCopyTrunk:1 | |
1 if the entry was too short to hold all the samples in RF core RAM; 0 otherwise More... | |
uint8_t bSamplTrunk:1 | |
1 if the entry contains samples of a CTE that was too long for the available RF core RAM; 0 otherwise More... | |
uint8_t rfRamInfo:2 | |
0: Reserved 1: Packet was contained in MCE RAM only 2: Packet was contained in RFE RAM only 3: Packet was contained in both RAMs More... | |
uint8_t rfPhy:1 | |
PHY of the packet containing the samples 0: 1 Mbps 1: 2 Mbps. More... | |
uint8_t rfGainStep:1 | |
RF gain of the received samples 0: High gain 1: Low gain. More... | |
} | status |
uint8_t rfc_statusIqSamplesEntry_s::bCrcErr |
1 if the samples came from a packet received with CRC error; 0 otherwise
uint8_t rfc_statusIqSamplesEntry_s::bCopyTrunk |
1 if the entry was too short to hold all the samples in RF core RAM; 0 otherwise
uint8_t rfc_statusIqSamplesEntry_s::bSamplTrunk |
1 if the entry contains samples of a CTE that was too long for the available RF core RAM; 0 otherwise
uint8_t rfc_statusIqSamplesEntry_s::rfRamInfo |
0: Reserved
1: Packet was contained in MCE RAM only
2: Packet was contained in RFE RAM only
3: Packet was contained in both RAMs
uint8_t rfc_statusIqSamplesEntry_s::rfPhy |
PHY of the packet containing the samples
0: 1 Mbps
1: 2 Mbps.
uint8_t rfc_statusIqSamplesEntry_s::rfGainStep |
RF gain of the received samples
0: High gain
1: Low gain.
struct { ... } rfc_statusIqSamplesEntry_s::status |