#include <rf_ble_cmd.h>
§ nTxAdvInd
uint16_t rfc_bleAdvOutput_s::nTxAdvInd |
Number of ADV*_IND packets completely transmitted.
§ nTxScanRsp
uint8_t rfc_bleAdvOutput_s::nTxScanRsp |
Number of AUX_SCAN_RSP or SCAN_RSP packets transmitted.
§ nRxScanReq
uint8_t rfc_bleAdvOutput_s::nRxScanReq |
Number of AUX_SCAN_REQ or SCAN_REQ packets received OK and not ignored.
§ nRxConnectReq
uint8_t rfc_bleAdvOutput_s::nRxConnectReq |
Number of AUX_CONNECT_REQ or CONNECT_IND (CONNECT_REQ) packets received OK and not ignored.
§ nTxConnectRsp
uint8_t rfc_bleAdvOutput_s::nTxConnectRsp |
Number of AUX_CONNECT_RSP packets transmitted.
§ nRxNok
uint16_t rfc_bleAdvOutput_s::nRxNok |
Number of packets received with CRC error.
§ nRxIgnored
uint16_t rfc_bleAdvOutput_s::nRxIgnored |
Number of packets received with CRC OK, but ignored.
§ nRxBufFull
uint8_t rfc_bleAdvOutput_s::nRxBufFull |
Number of packets received that did not fit in Rx queue.
§ lastRssi
int8_t rfc_bleAdvOutput_s::lastRssi |
The RSSI of the last received packet (signed)
§ timeStamp
ratmr_t rfc_bleAdvOutput_s::timeStamp |
Time stamp of the last received packet.
The documentation for this struct was generated from the following file: