rflib
Data Fields
rfc_ble5AdvAuxPar_s Struct Reference

#include <rf_ble_cmd.h>

Collaboration diagram for rfc_ble5AdvAuxPar_s:
Collaboration graph
[legend]

Data Fields

dataQueue_tpRxQ
 Pointer to receive queue. More...
 
struct {
   uint8_t   bAutoFlushIgnored:1
 If 1, automatically remove ignored packets from Rx queue. More...
 
   uint8_t   bAutoFlushCrcErr:1
 If 1, automatically remove packets with CRC error from Rx queue. More...
 
   uint8_t   bAutoFlushEmpty:1
 If 1, automatically remove empty packets from Rx queue. More...
 
   uint8_t   bIncludeLenByte:1
 If 1, include the received length byte in the stored packet; otherwise discard it. More...
 
   uint8_t   bIncludeCrc:1
 If 1, include the received CRC field in the stored packet; otherwise discard it. More...
 
   uint8_t   bAppendRssi:1
 If 1, append an RSSI byte to the packet in the Rx queue. More...
 
   uint8_t   bAppendStatus:1
 If 1, append a status word to the packet in the Rx queue. More...
 
   uint8_t   bAppendTimestamp:1
 If 1, append a timestamp to the packet in the Rx queue. More...
 
rxConfig
 Configuration bits for the receive queue entries. More...
 
struct {
   uint8_t   advFilterPolicy:2
 Advertiser filter policy
0: Process scan and connect requests from all devices
1: Process connect requests from all devices and only scan requests from devices that are in the white list
2: Process scan requests from all devices and only connect requests from devices that are in the white list
3: Process scan and connect requests only from devices in the white list. More...
 
   uint8_t   deviceAddrType:1
 The type of the device address – public (0) or random (1) More...
 
   uint8_t   targetAddrType:1
 Directed secondary advertiser: The type of the target address – public (0) or random (1) More...
 
   uint8_t   bStrictLenFilter:1
 0: Accept any packet with a valid advertising packet length
1: Discard messages with illegal length for the given packet type More...
 
   uint8_t   bDirected:1
 0: Advertiser is undirected: pWhiteList points to a white list 1: Advertiser is directed: pWhiteList points to a single device address More...
 
   uint8_t   privIgnMode:1
 0: Filter on bPrivIgn only when white list is used 1: Filter on bPrivIgn always More...
 
   uint8_t   rpaMode:1
 Resolvable private address mode
0: Normal operation
1: Use white list for a received RPA regardless of filter policy. More...
 
advConfig
 
struct {
   uint8_t   scanRspEndType:1
 Command status at end if AUX_SCAN_RSP was sent:
0: End with BLE_DONE_OK and result True
1: End with BLE_DONE_SCAN_RSP and result False. More...
 
behConfig
 
uint8_t auxPtrTargetType
 Number indicating reference for auxPtrTargetTime. Takes same values as trigger types, but only TRIG_ABSTIME and TRIG_REL_* are allowed. More...
 
ratmr_t auxPtrTargetTime
 Time of start of packet to which auxPtr points. More...
 
uint8_t * pAdvPkt
 Pointer to extended advertising packet for the ADV_AUX_IND packet. More...
 
uint8_t * pRspPkt
 Pointer to extended advertising packet for the AUX_SCAN_RSP or AUX_CONNECT_RSP packet (may be NULL if not applicable) More...
 
uint16_t * pDeviceAddress
 Pointer (with least significant bit set to 0) to device address used for this device. If least significant bit is 1, the address type given by advConfig.deviceAddrType is inverted. More...
 
rfc_bleWhiteListEntry_tpWhiteList
 Pointer (with least significant bit set to 0) to white list or peer address (directed advertiser). If least significant bit is 1, the address type given by advConfig.peerAddrType is inverted. More...
 
struct {
   uint8_t   bAutoFlushIgnored:1
 If 1, automatically remove ignored packets from Rx queue. More...
 
   uint8_t   bAutoFlushCrcErr:1
 If 1, automatically remove packets with CRC error from Rx queue. More...
 
   uint8_t   bAutoFlushEmpty:1
 If 1, automatically remove empty packets from Rx queue. More...
 
   uint8_t   bIncludeLenByte:1
 If 1, include the received length byte in the stored packet; otherwise discard it. More...
 
   uint8_t   bIncludeCrc:1
 If 1, include the received CRC field in the stored packet; otherwise discard it. More...
 
   uint8_t   bAppendRssi:1
 If 1, append an RSSI byte to the packet in the Rx queue. More...
 
   uint8_t   bAppendStatus:1
 If 1, append a status word to the packet in the Rx queue. More...
 
   uint8_t   bAppendTimestamp:1
 If 1, append a timestamp to the packet in the Rx queue. More...
 
rxConfig
 Configuration bits for the receive queue entries. More...
 
struct {
   uint8_t   advFilterPolicy:2
 Advertiser filter policy
0: Process scan and connect requests from all devices
1: Process connect requests from all devices and only scan requests from devices that are in the white list
2: Process scan requests from all devices and only connect requests from devices that are in the white list
3: Process scan and connect requests only from devices in the white list. More...
 
   uint8_t   deviceAddrType:1
 The type of the device address – public (0) or random (1) More...
 
   uint8_t   targetAddrType:1
 Directed secondary advertiser: The type of the target address – public (0) or random (1) More...
 
   uint8_t   bStrictLenFilter:1
 0: Accept any packet with a valid advertising packet length
1: Discard messages with illegal length for the given packet type More...
 
   uint8_t   bDirected:1
 0: Advertiser is undirected: pWhiteList points to a white list 1: Advertiser is directed: pWhiteList points to a single device address More...
 
   uint8_t   privIgnMode:1
 0: Filter on bPrivIgn only when white list is used 1: Filter on bPrivIgn always More...
 
   uint8_t   rpaMode:1
 Resolvable private address mode
0: Normal operation
1: Use white list for a received RPA regardless of filter policy. More...
 
advConfig
 
struct {
   uint8_t   scanRspEndType:1
 Command status at end if AUX_SCAN_RSP was sent:
0: End with BLE_DONE_OK and result True
1: End with BLE_DONE_SCAN_RSP and result False. More...
 
behConfig
 
struct {
   uint8_t   bAutoFlushIgnored:1
 If 1, automatically remove ignored packets from Rx queue. More...
 
   uint8_t   bAutoFlushCrcErr:1
 If 1, automatically remove packets with CRC error from Rx queue. More...
 
   uint8_t   bAutoFlushEmpty:1
 If 1, automatically remove empty packets from Rx queue. More...
 
   uint8_t   bIncludeLenByte:1
 If 1, include the received length byte in the stored packet; otherwise discard it. More...
 
   uint8_t   bIncludeCrc:1
 If 1, include the received CRC field in the stored packet; otherwise discard it. More...
 
   uint8_t   bAppendRssi:1
 If 1, append an RSSI byte to the packet in the Rx queue. More...
 
   uint8_t   bAppendStatus:1
 If 1, append a status word to the packet in the Rx queue. More...
 
   uint8_t   bAppendTimestamp:1
 If 1, append a timestamp to the packet in the Rx queue. More...
 
rxConfig
 Configuration bits for the receive queue entries. More...
 
struct {
   uint8_t   advFilterPolicy:2
 Advertiser filter policy
0: Process scan and connect requests from all devices
1: Process connect requests from all devices and only scan requests from devices that are in the white list
2: Process scan requests from all devices and only connect requests from devices that are in the white list
3: Process scan and connect requests only from devices in the white list. More...
 
   uint8_t   deviceAddrType:1
 The type of the device address – public (0) or random (1) More...
 
   uint8_t   targetAddrType:1
 Directed secondary advertiser: The type of the target address – public (0) or random (1) More...
 
   uint8_t   bStrictLenFilter:1
 0: Accept any packet with a valid advertising packet length
1: Discard messages with illegal length for the given packet type More...
 
   uint8_t   bDirected:1
 0: Advertiser is undirected: pWhiteList points to a white list 1: Advertiser is directed: pWhiteList points to a single device address More...
 
   uint8_t   privIgnMode:1
 0: Filter on bPrivIgn only when white list is used 1: Filter on bPrivIgn always More...
 
   uint8_t   rpaMode:1
 Resolvable private address mode
0: Normal operation
1: Use white list for a received RPA regardless of filter policy. More...
 
advConfig
 
struct {
   uint8_t   scanRspEndType:1
 Command status at end if AUX_SCAN_RSP was sent:
0: End with BLE_DONE_OK and result True
1: End with BLE_DONE_SCAN_RSP and result False. More...
 
behConfig
 

Field Documentation

§ pRxQ

dataQueue_t * rfc_ble5AdvAuxPar_s::pRxQ

Pointer to receive queue.

§ bAutoFlushIgnored

uint8_t rfc_ble5AdvAuxPar_s::bAutoFlushIgnored

If 1, automatically remove ignored packets from Rx queue.

§ bAutoFlushCrcErr

uint8_t rfc_ble5AdvAuxPar_s::bAutoFlushCrcErr

If 1, automatically remove packets with CRC error from Rx queue.

§ bAutoFlushEmpty

uint8_t rfc_ble5AdvAuxPar_s::bAutoFlushEmpty

If 1, automatically remove empty packets from Rx queue.

§ bIncludeLenByte

uint8_t rfc_ble5AdvAuxPar_s::bIncludeLenByte

If 1, include the received length byte in the stored packet; otherwise discard it.

§ bIncludeCrc

uint8_t rfc_ble5AdvAuxPar_s::bIncludeCrc

If 1, include the received CRC field in the stored packet; otherwise discard it.

§ bAppendRssi

uint8_t rfc_ble5AdvAuxPar_s::bAppendRssi

If 1, append an RSSI byte to the packet in the Rx queue.

§ bAppendStatus

uint8_t rfc_ble5AdvAuxPar_s::bAppendStatus

If 1, append a status word to the packet in the Rx queue.

§ bAppendTimestamp

uint8_t rfc_ble5AdvAuxPar_s::bAppendTimestamp

If 1, append a timestamp to the packet in the Rx queue.

§ rxConfig [1/3]

struct { ... } rfc_ble5AdvAuxPar_s::rxConfig

Configuration bits for the receive queue entries.

§ advFilterPolicy

uint8_t rfc_ble5AdvAuxPar_s::advFilterPolicy

Advertiser filter policy
0: Process scan and connect requests from all devices
1: Process connect requests from all devices and only scan requests from devices that are in the white list
2: Process scan requests from all devices and only connect requests from devices that are in the white list
3: Process scan and connect requests only from devices in the white list.

§ deviceAddrType

uint8_t rfc_ble5AdvAuxPar_s::deviceAddrType

The type of the device address – public (0) or random (1)

§ targetAddrType

uint8_t rfc_ble5AdvAuxPar_s::targetAddrType

Directed secondary advertiser: The type of the target address – public (0) or random (1)

§ bStrictLenFilter

uint8_t rfc_ble5AdvAuxPar_s::bStrictLenFilter

0: Accept any packet with a valid advertising packet length
1: Discard messages with illegal length for the given packet type

§ bDirected

uint8_t rfc_ble5AdvAuxPar_s::bDirected

0: Advertiser is undirected: pWhiteList points to a white list 1: Advertiser is directed: pWhiteList points to a single device address

§ privIgnMode

uint8_t rfc_ble5AdvAuxPar_s::privIgnMode

0: Filter on bPrivIgn only when white list is used 1: Filter on bPrivIgn always

§ rpaMode

uint8_t rfc_ble5AdvAuxPar_s::rpaMode

Resolvable private address mode
0: Normal operation
1: Use white list for a received RPA regardless of filter policy.

§ advConfig [1/3]

struct { ... } rfc_ble5AdvAuxPar_s::advConfig

§ scanRspEndType

uint8_t rfc_ble5AdvAuxPar_s::scanRspEndType

Command status at end if AUX_SCAN_RSP was sent:
0: End with BLE_DONE_OK and result True
1: End with BLE_DONE_SCAN_RSP and result False.

§ behConfig [1/3]

struct { ... } rfc_ble5AdvAuxPar_s::behConfig

§ auxPtrTargetType

uint8_t rfc_ble5AdvAuxPar_s::auxPtrTargetType

Number indicating reference for auxPtrTargetTime. Takes same values as trigger types, but only TRIG_ABSTIME and TRIG_REL_* are allowed.

§ auxPtrTargetTime

ratmr_t rfc_ble5AdvAuxPar_s::auxPtrTargetTime

Time of start of packet to which auxPtr points.

§ pAdvPkt

uint8_t * rfc_ble5AdvAuxPar_s::pAdvPkt

Pointer to extended advertising packet for the ADV_AUX_IND packet.

§ pRspPkt

uint8_t * rfc_ble5AdvAuxPar_s::pRspPkt

Pointer to extended advertising packet for the AUX_SCAN_RSP or AUX_CONNECT_RSP packet (may be NULL if not applicable)

§ pDeviceAddress

uint16_t * rfc_ble5AdvAuxPar_s::pDeviceAddress

Pointer (with least significant bit set to 0) to device address used for this device. If least significant bit is 1, the address type given by advConfig.deviceAddrType is inverted.

§ pWhiteList

rfc_bleWhiteListEntry_t * rfc_ble5AdvAuxPar_s::pWhiteList

Pointer (with least significant bit set to 0) to white list or peer address (directed advertiser). If least significant bit is 1, the address type given by advConfig.peerAddrType is inverted.

§ rxConfig [2/3]

struct { ... } rfc_ble5AdvAuxPar_s::rxConfig

Configuration bits for the receive queue entries.

§ advConfig [2/3]

struct { ... } rfc_ble5AdvAuxPar_s::advConfig

§ behConfig [2/3]

struct { ... } rfc_ble5AdvAuxPar_s::behConfig

§ rxConfig [3/3]

struct { ... } rfc_ble5AdvAuxPar_s::rxConfig

Configuration bits for the receive queue entries.

§ advConfig [3/3]

struct { ... } rfc_ble5AdvAuxPar_s::advConfig

§ behConfig [3/3]

struct { ... } rfc_ble5AdvAuxPar_s::behConfig

The documentation for this struct was generated from the following file:
© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale