![]() |
![]() |
rflib
|
IEEE 802.15.4 Energy Detect Scan Command. More...
#include <rf_ieee_cmd.h>
Data Fields | |
uint16_t | commandNo |
The command ID number 0x2802. More... | |
uint16_t | status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More... | |
rfc_radioOp_t * | pNextOp |
Pointer to the next operation to run after this operation is done. More... | |
ratmr_t | startTime |
Absolute or relative start time (depending on the value of startTrigger ) More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | startTrigger |
Identification of the trigger that starts the operation. More... | |
struct { | |
uint8_t rule:4 | |
Condition for running next command: Rule for how to proceed. More... | |
uint8_t nSkip:4 | |
Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More... | |
} | condition |
uint8_t | channel |
Channel to tune to in the start of the operation 0: Use existing channel 11–26: Use as IEEE 802.15.4 channel, i.e. frequency is (2405 + 5 × (channel - 11)) MHz 60–207: Frequency is (2300 + channel) MHz Others: Reserved More... | |
struct { | |
uint8_t ccaEnEnergy:1 | |
Enable energy scan as CCA source. More... | |
uint8_t ccaEnCorr:1 | |
Enable correlator based carrier sense as CCA source. More... | |
uint8_t ccaEnSync:1 | |
Enable sync found based carrier sense as CCA source. More... | |
uint8_t ccaCorrOp:1 | |
Operator to use between energy based and correlator based CCA 0: Report busy channel if either ccaEnergy or ccaCorr are busy 1: Report busy channel if both ccaEnergy and ccaCorr are busy. More... | |
uint8_t ccaSyncOp:1 | |
Operator to use between sync found based CCA and the others 0: Always report busy channel if ccaSync is busy 1: Always report idle channel if ccaSync is idle. More... | |
uint8_t ccaCorrThr:2 | |
Threshold for number of correlation peaks in correlator based carrier sense. More... | |
} | ccaOpt |
CCA options. More... | |
int8_t | ccaRssiThr |
RSSI threshold for CCA. More... | |
uint8_t | __dummy0 |
int8_t | maxRssi |
The maximum RSSI recorded during the ED scan. More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | endTrigger |
Trigger that causes the device to end the Rx operation. More... | |
ratmr_t | endTime |
Time used together with endTrigger that causes the device to end the Rx operation. More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | startTrigger |
Identification of the trigger that starts the operation. More... | |
struct { | |
uint8_t rule:4 | |
Condition for running next command: Rule for how to proceed. More... | |
uint8_t nSkip:4 | |
Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More... | |
} | condition |
struct { | |
uint8_t ccaEnEnergy:1 | |
Enable energy scan as CCA source. More... | |
uint8_t ccaEnCorr:1 | |
Enable correlator based carrier sense as CCA source. More... | |
uint8_t ccaEnSync:1 | |
Enable sync found based carrier sense as CCA source. More... | |
uint8_t ccaCorrOp:1 | |
Operator to use between energy based and correlator based CCA 0: Report busy channel if either ccaEnergy or ccaCorr are busy 1: Report busy channel if both ccaEnergy and ccaCorr are busy. More... | |
uint8_t ccaSyncOp:1 | |
Operator to use between sync found based CCA and the others 0: Always report busy channel if ccaSync is busy 1: Always report idle channel if ccaSync is idle. More... | |
uint8_t ccaCorrThr:2 | |
Threshold for number of correlation peaks in correlator based carrier sense. More... | |
} | ccaOpt |
CCA options. More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | endTrigger |
Trigger that causes the device to end the Rx operation. More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | startTrigger |
Identification of the trigger that starts the operation. More... | |
struct { | |
uint8_t rule:4 | |
Condition for running next command: Rule for how to proceed. More... | |
uint8_t nSkip:4 | |
Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More... | |
} | condition |
struct { | |
uint8_t ccaEnEnergy:1 | |
Enable energy scan as CCA source. More... | |
uint8_t ccaEnCorr:1 | |
Enable correlator based carrier sense as CCA source. More... | |
uint8_t ccaEnSync:1 | |
Enable sync found based carrier sense as CCA source. More... | |
uint8_t ccaCorrOp:1 | |
Operator to use between energy based and correlator based CCA 0: Report busy channel if either ccaEnergy or ccaCorr are busy 1: Report busy channel if both ccaEnergy and ccaCorr are busy. More... | |
uint8_t ccaSyncOp:1 | |
Operator to use between sync found based CCA and the others 0: Always report busy channel if ccaSync is busy 1: Always report idle channel if ccaSync is idle. More... | |
uint8_t ccaCorrThr:2 | |
Threshold for number of correlation peaks in correlator based carrier sense. More... | |
} | ccaOpt |
CCA options. More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | endTrigger |
Trigger that causes the device to end the Rx operation. More... | |
IEEE 802.15.4 Energy Detect Scan Command.
uint16_t rfc_CMD_IEEE_ED_SCAN_s::commandNo |
The command ID number 0x2802.
uint16_t rfc_CMD_IEEE_ED_SCAN_s::status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.
rfc_radioOp_t * rfc_CMD_IEEE_ED_SCAN_s::pNextOp |
Pointer to the next operation to run after this operation is done.
ratmr_t rfc_CMD_IEEE_ED_SCAN_s::startTime |
Absolute or relative start time (depending on the value of startTrigger
)
uint8_t rfc_CMD_IEEE_ED_SCAN_s::triggerType |
The type of trigger.
uint8_t rfc_CMD_IEEE_ED_SCAN_s::bEnaCmd |
0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger
uint8_t rfc_CMD_IEEE_ED_SCAN_s::triggerNo |
The trigger number of the CMD_TRIGGER command that triggers this action.
uint8_t rfc_CMD_IEEE_ED_SCAN_s::pastTrig |
0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible
struct { ... } rfc_CMD_IEEE_ED_SCAN_s::startTrigger |
Identification of the trigger that starts the operation.
uint8_t rfc_CMD_IEEE_ED_SCAN_s::rule |
Condition for running next command: Rule for how to proceed.
uint8_t rfc_CMD_IEEE_ED_SCAN_s::nSkip |
Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ...
struct { ... } rfc_CMD_IEEE_ED_SCAN_s::condition |
uint8_t rfc_CMD_IEEE_ED_SCAN_s::channel |
Channel to tune to in the start of the operation
0: Use existing channel
11–26: Use as IEEE 802.15.4 channel, i.e. frequency is (2405 + 5 × (channel - 11)) MHz
60–207: Frequency is (2300 + channel) MHz
Others: Reserved
uint8_t rfc_CMD_IEEE_ED_SCAN_s::ccaEnEnergy |
Enable energy scan as CCA source.
uint8_t rfc_CMD_IEEE_ED_SCAN_s::ccaEnCorr |
Enable correlator based carrier sense as CCA source.
uint8_t rfc_CMD_IEEE_ED_SCAN_s::ccaEnSync |
Enable sync found based carrier sense as CCA source.
uint8_t rfc_CMD_IEEE_ED_SCAN_s::ccaCorrOp |
Operator to use between energy based and correlator based CCA
0: Report busy channel if either ccaEnergy or ccaCorr are busy
1: Report busy channel if both ccaEnergy and ccaCorr are busy.
uint8_t rfc_CMD_IEEE_ED_SCAN_s::ccaSyncOp |
Operator to use between sync found based CCA and the others
0: Always report busy channel if ccaSync is busy
1: Always report idle channel if ccaSync is idle.
uint8_t rfc_CMD_IEEE_ED_SCAN_s::ccaCorrThr |
Threshold for number of correlation peaks in correlator based carrier sense.
struct { ... } rfc_CMD_IEEE_ED_SCAN_s::ccaOpt |
CCA options.
int8_t rfc_CMD_IEEE_ED_SCAN_s::ccaRssiThr |
RSSI threshold for CCA.
uint8_t rfc_CMD_IEEE_ED_SCAN_s::__dummy0 |
int8_t rfc_CMD_IEEE_ED_SCAN_s::maxRssi |
The maximum RSSI recorded during the ED scan.
struct { ... } rfc_CMD_IEEE_ED_SCAN_s::endTrigger |
Trigger that causes the device to end the Rx operation.
ratmr_t rfc_CMD_IEEE_ED_SCAN_s::endTime |
Time used together with endTrigger
that causes the device to end the Rx operation.
struct { ... } rfc_CMD_IEEE_ED_SCAN_s::startTrigger |
Identification of the trigger that starts the operation.
struct { ... } rfc_CMD_IEEE_ED_SCAN_s::condition |
struct { ... } rfc_CMD_IEEE_ED_SCAN_s::ccaOpt |
CCA options.
struct { ... } rfc_CMD_IEEE_ED_SCAN_s::endTrigger |
Trigger that causes the device to end the Rx operation.
struct { ... } rfc_CMD_IEEE_ED_SCAN_s::startTrigger |
Identification of the trigger that starts the operation.
struct { ... } rfc_CMD_IEEE_ED_SCAN_s::condition |
struct { ... } rfc_CMD_IEEE_ED_SCAN_s::ccaOpt |
CCA options.
struct { ... } rfc_CMD_IEEE_ED_SCAN_s::endTrigger |
Trigger that causes the device to end the Rx operation.