rflib
Data Fields
rfc_CMD_BUS_REQUEST_s Struct Reference

Request System Bus to be Availbale. More...

#include <rf_common_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x040E. More...
 
uint8_t bSysBusNeeded
 0: System bus may sleep
1: System bus access needed More...
 

Detailed Description

Request System Bus to be Availbale.

Field Documentation

§ commandNo

uint16_t rfc_CMD_BUS_REQUEST_s::commandNo

The command ID number 0x040E.

§ bSysBusNeeded

uint8_t rfc_CMD_BUS_REQUEST_s::bSysBusNeeded

0: System bus may sleep
1: System bus access needed


The documentation for this struct was generated from the following file:
© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale