rflib
Data Fields
rfc_CMD_BLE_MASTER_s Struct Reference

BLE Master Command. More...

#include <rf_ble_cmd.h>

Collaboration diagram for rfc_CMD_BLE_MASTER_s:
Collaboration graph
[legend]

Data Fields

uint16_t commandNo
 The command ID number 0x1802. More...
 
uint16_t status
 An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More...
 
rfc_radioOp_tpNextOp
 Pointer to the next operation to run after this operation is done. More...
 
ratmr_t startTime
 Absolute or relative start time (depending on the value of startTrigger) More...
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
startTrigger
 Identification of the trigger that starts the operation. More...
 
struct {
   uint8_t   rule:4
 Condition for running next command: Rule for how to proceed. More...
 
   uint8_t   nSkip:4
 Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More...
 
condition
 
uint8_t channel
 Channel to use
0–39: BLE advertising/data channel index
60–207: Custom frequency; (2300 + channel) MHz
255: Use existing frequency
Others: Reserved More...
 
struct {
   uint8_t   init:7
 If bOverride = 1 or custom frequency is used:
0: Do not use whitening
Other value: Initialization for 7-bit LFSR whitener. More...
 
   uint8_t   bOverride:1
 0: Use default whitening for BLE advertising/data channels
1: Override whitening initialization with value of init More...
 
whitening
 
rfc_bleMasterPar_tpParams
 Pointer to command specific parameter structure. More...
 
rfc_bleMasterSlaveOutput_tpOutput
 Pointer to command specific output structure. More...
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
startTrigger
 Identification of the trigger that starts the operation. More...
 
struct {
   uint8_t   rule:4
 Condition for running next command: Rule for how to proceed. More...
 
   uint8_t   nSkip:4
 Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More...
 
condition
 
struct {
   uint8_t   init:7
 If bOverride = 1 or custom frequency is used:
0: Do not use whitening
Other value: Initialization for 7-bit LFSR whitener. More...
 
   uint8_t   bOverride:1
 0: Use default whitening for BLE advertising/data channels
1: Override whitening initialization with value of init More...
 
whitening
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
startTrigger
 Identification of the trigger that starts the operation. More...
 
struct {
   uint8_t   rule:4
 Condition for running next command: Rule for how to proceed. More...
 
   uint8_t   nSkip:4
 Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More...
 
condition
 
struct {
   uint8_t   init:7
 If bOverride = 1 or custom frequency is used:
0: Do not use whitening
Other value: Initialization for 7-bit LFSR whitener. More...
 
   uint8_t   bOverride:1
 0: Use default whitening for BLE advertising/data channels
1: Override whitening initialization with value of init More...
 
whitening
 

Detailed Description

BLE Master Command.

Field Documentation

§ commandNo

uint16_t rfc_CMD_BLE_MASTER_s::commandNo

The command ID number 0x1802.

§ status

uint16_t rfc_CMD_BLE_MASTER_s::status

An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.

§ pNextOp

rfc_radioOp_t * rfc_CMD_BLE_MASTER_s::pNextOp

Pointer to the next operation to run after this operation is done.

§ startTime

ratmr_t rfc_CMD_BLE_MASTER_s::startTime

Absolute or relative start time (depending on the value of startTrigger)

§ triggerType

uint8_t rfc_CMD_BLE_MASTER_s::triggerType

The type of trigger.

§ bEnaCmd

uint8_t rfc_CMD_BLE_MASTER_s::bEnaCmd

0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger

§ triggerNo

uint8_t rfc_CMD_BLE_MASTER_s::triggerNo

The trigger number of the CMD_TRIGGER command that triggers this action.

§ pastTrig

uint8_t rfc_CMD_BLE_MASTER_s::pastTrig

0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible

§ startTrigger [1/3]

struct { ... } rfc_CMD_BLE_MASTER_s::startTrigger

Identification of the trigger that starts the operation.

§ rule

uint8_t rfc_CMD_BLE_MASTER_s::rule

Condition for running next command: Rule for how to proceed.

§ nSkip

uint8_t rfc_CMD_BLE_MASTER_s::nSkip

Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ...

§ condition [1/3]

struct { ... } rfc_CMD_BLE_MASTER_s::condition

§ channel

uint8_t rfc_CMD_BLE_MASTER_s::channel

Channel to use
0–39: BLE advertising/data channel index
60–207: Custom frequency; (2300 + channel) MHz
255: Use existing frequency
Others: Reserved

§ init

uint8_t rfc_CMD_BLE_MASTER_s::init

If bOverride = 1 or custom frequency is used:
0: Do not use whitening
Other value: Initialization for 7-bit LFSR whitener.

§ bOverride

uint8_t rfc_CMD_BLE_MASTER_s::bOverride

0: Use default whitening for BLE advertising/data channels
1: Override whitening initialization with value of init

§ whitening [1/3]

struct { ... } rfc_CMD_BLE_MASTER_s::whitening

§ pParams

rfc_bleMasterPar_t * rfc_CMD_BLE_MASTER_s::pParams

Pointer to command specific parameter structure.

§ pOutput

rfc_bleMasterSlaveOutput_t * rfc_CMD_BLE_MASTER_s::pOutput

Pointer to command specific output structure.

§ startTrigger [2/3]

struct { ... } rfc_CMD_BLE_MASTER_s::startTrigger

Identification of the trigger that starts the operation.

§ condition [2/3]

struct { ... } rfc_CMD_BLE_MASTER_s::condition

§ whitening [2/3]

struct { ... } rfc_CMD_BLE_MASTER_s::whitening

§ startTrigger [3/3]

struct { ... } rfc_CMD_BLE_MASTER_s::startTrigger

Identification of the trigger that starts the operation.

§ condition [3/3]

struct { ... } rfc_CMD_BLE_MASTER_s::condition

§ whitening [3/3]

struct { ... } rfc_CMD_BLE_MASTER_s::whitening

The documentation for this struct was generated from the following file:
© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale