Migrating from CC1101¶
Introduction¶
Welcome to the CC1101 migration guide. This guide is written for users that use CC1101 today and want to migrate over to CC13xx. This guide consists of 4 main parts:
“How do I get a link between CC1101 and CC13xx?”
“Where are my registers?”: A short introduction to software on CC13xx
“How do I make CC13xx do anything”: Drivers and software
“I use feature <> on CC1101, how do I do it on CC13xx?”
This document refers to the following material:
The device datasheet: The datasheet for the device you are working with.
The CC13x2 CC26x2 SimpleLink Wireless MCU Technical Reference Manual
“How do I get a link between CC1101 and CC13xx”¶
Note
38.4 kbps is used for these examples. Other data rates supported by genfsk may be used.
For the following examples, SmartRF Studio is used.
CC1101 <-> CC13xx Using Non Return to Zero (NRZ)¶
On CC1101:
Select the predefined 38.4 kbps setting
Figure 28. CC1101 configuration NRZ¶
On CC13xx:
Select the 50 kbps setting. Change the data rate and deviation to the same as CC1101 uses.
CC1101 uses a 16 bit sync word that is repeated to generate a 32 bit sync word. On CC13xx the sync word then has to be set to 0xD391D391.
Figure 29. CC13xx configuration NRZ¶
CC1101 <-> CC13xx Using Manchester Coding¶
- On CC1101:
Select the predefined 38.4 kbps setting
Tick the Manchester Enable box
Set MDMCFG2.SYNC_MODE = 2.
On CC13xx:
Select the 50 kbps setting. Change the data rate and deviation to the same as CC1101 uses.
CC1101 does manchester coding on preamble and sync word, CC13xx only does manchester coding on the payload. The CC1101 sync word manchester encoded is 0xA65A9656. Set the CC13xx sync word equal to this.
Enable manchester coding by setting PROP_RADIO_DIV_SETUP.formatConf.fecMode = 0xA
The following override has to be added to get the bytes in the correct order: HW_REG_OVERRIDE(0x5328,0x2047)
The following override has to be added: HW_REG_OVERRIDE(0x5320, 0x1000)
Manchester coding has only been functionally verified on CC13xx.
Figure 30. CC13xx configuration manchester¶
The strict sync word check in CC13xx is not in use when using manchester coding. To reduce the number of false syncs the sync threshold could be increased. See sync_word_qualifier for details.
General note: It is recommended to use manchester coding only for legacy systems.
How to use the override editor in SmartRF Studio is described in the built-in help in the program.
“Where are my registers?”¶
CC1101 is a transceiver meaning that to make an application CC1101 has to be used together with an MCU. This MCU communicates with CC1101 over an SPI interface and hardware registers on CC1101 has to be written or strobe commands have to be sent to make the radio do anything.
CC13xx is a wireless MCU. This mean that CC13xx is a powerful MCU with a selection of peripheral modules where one of these is the RF core. CC13xx still has registers but most of them are hidden from users. One of the reasons for this is that the meaning of a register on CC13xx changes dependent on which firmware that is running. Instead the communication with the different modules on CC13xx is done via APIs and overrides. All the available modules on CC13xx have a driver. The APIs for the drivers are described in the documentation.
In addition all drivers are documented in the header files. The header files also contain examples of usage. The driver header files are found in TI Driver Source Files. Some drivers also have examples included in the SDK.
An override is a register write. Most of the overrides are provided by TI and should not be changed. These are typically registers setting up one or more internal modules and are the result of a lot of testing. The registers users can change freely are typically documented here. Required overrides are given by SmartRF Studio.
“How Do I Make CC13xx Do Anything?”: Drivers and Software¶
To control CC1101 you can use anything from a simple 8 bits MCU to a multi core Arm processor, all depending on the complexity of your application. CC13xx is a wireless MCU with more than one core hence programming CC13xx is different from using a simple 8 bit controller. CC13xx has a number of internal voltage and clock domains. To use (as an example) the RF core the clocks used by the RF core have to be turned on and the voltage domain the RF core is powered from has to be turned on. When the RF core is not in use the clocks and the voltage domain should be turned off to save power. The power on and off needs to be done in a given sequence to ensure that everything is in the correct state.
To simplify the use of CC13xx drivers are available. The driver sets up the clock and power domains and offer an API. The driver documentation can be found here:
The drivers are written in c and it is therefore possible to walk through the code to get a better understanding of what a given driver does if this is wanted and/ or required. In addition, this document describes the power driver requirements: Power Management User’s Guide.
Both the TI-RTOS7 and the NoRTOS solution go to the IDLE state whenever possible. In IDLE state the Power_idleFunc() is called which takes the chip to the lowest power state possible.
For a comprehensive TI-RTOS course, see the TI RTOS Workshop Series.
The NoRTOS solution is documented here: NoRTOS Driver Porting Layer.
For CC13xx a Software Development Kit (SDK) is provided.
The Customer Configuration (CCFG)¶
CC13xx has a part of flash called Customer Configuration (CCFG). The CCFG parameters are set at compile time in the ccfg.c file in the SDK. The ccfg.c file contains settings for (not a complete list):
CCFG_FORCE_VDDR_HH: Sets it 12.5 dBm or 14 dBm is maximum output power.
SET_CCFG_MODE_CONF_DCDC_ACTIVE: Sets if the DCDC should be used in active or not.
SET_CCFG_MODE_CONF_SCLK_LF_OPTION: Sets the source for the low frequency clock.
SET_CCFG_MODE_CONF_XOSC_CAP_MOD: Sets if the internal crystal load capacitor array should be used. The default is that the internal array is in use.
SET_CCFG_EXT_LF_CLK_DIO: The DIO used if using an external clock source for the LF
SET_CCFG_BL_CONFIG_BL<>: Settings for the boot loader.
“I Use Feature <> on CC1101, How Do I Do it on CC13xx?”¶
This part of the migration guide aims to describe how CC1101 features map to the CC13xx. The numbering of the sections follows the CC1101 datasheet. If you wonder how to implement a given thing on CC13xx, find which section in the CC1101 datasheet this is covered and look up the section number in the guide.
4 Electrical Specifications¶
4.1 Current Consumption¶
The CC13xx current consumption numbers are summarized in 5.4 and 6.7 in the device datasheet.
State |
CC1101 |
CC1310 |
CC1312 |
|---|---|---|---|
Tx (10 dBm) |
30.0 mA |
13.4 mA |
14 mA |
Rx |
14.7 mA |
5.5 mA |
5.7 mA |
Sleep |
0.2 uA |
0.185 uA |
0.13 uA |
4.2 Receive Section¶
The CC13xx receive parameters are stated in 5.6 and 5.7 in the device datasheet.
4.3 RF Transmit Section¶
The CC13xx transmit parameters are stated in 5.8 and 5.9 in the device datasheet.
4.4 Crystal Oscillator¶
CC13xx has 2 crystal oscillators, 48 MHz and 32.768 kHz. The internal 32.768
kHz RC oscillator can be used instead of the 32.768 crystal. This is done in the
ccfg.c file.
4.5 Low Power RC Oscillator¶
The CC13xx 32 kHz RC oscillator is covered in the “Clock Specifications” section in chapter 5 in the device datasheet.
4.6 Frequency Synthesizer Characteristics¶
The CC13xx PLL parameters are covered in chapter 5 in the datasheet.
4.7 Analog Temperature Sensor¶
The CC13xx has a build in temperature sensor and battery monitor. An API is provided, see AONBATMON API.
The “Battery Monitor and Temperature Sensor” chapter in the CC13x2 CC26x2 SimpleLink Wireless MCU Technical Reference Manual describes how the module is implemented on CC13xx.
4.8 DC Characteristics¶
The CC13xx DC characteristics are covered in chapter 5 in the datasheet.
4.9 Power-On Reset¶
CC13xx has built in power supply supervision that ensures that the chip first starts when the supply voltage to the chip has a valid level. When the voltage drops below a given voltage the voltage supply supervision module take the chip down in a controlled reset to ensure that the chip does not enter an undefined state.
In the ccfg.c file it’s possible to set the reset level to 1.78 V (1.65 V if
external regulator mode is used) or 2.0 V, see
SET_CCFG_MODE_CONF_VDDS_BOD_LEVEL in The Customer Configuration (CCFG).
5 Pin Configuration¶
See section 4 in the device datasheet for pin configurations.
Note
CC13x0 comes in 3 different packet sizes (4x4, 5x5 and 7x7) where the main difference between the packet sizes is the number of available IOs.
CC13x2 is only available in 7x7.
6 Circuit Description¶
See the device datasheet and section 1 in the CC13x2 CC26x2 SimpleLink Wireless MCU Technical Reference Manual.
7 Application Circuit¶
This section will not cover the CC13xx application circuit but some of the differences between CC1101 and CC13xx. For CC13xx application circuits see under Design files in “Technical Documents” on the device page.
7.1 Bias Resistor¶
CC13xx doesn’t use an external bias resistor
7.2 Balun and RF Matching¶
Similar to CC1101, CC13xx has differential RF pins, RF_P and RF_N. In addition the RXTX pin may be used. The LNA can be biased internally or externally. If the latter is the case the RXTX pin is used. In addition, the RF_P and RF_N pins are possible to use single ended. Possible use cases are two single ended paths on two different frequencies or one path for TX and one for RX. The latter could typically be the case when using a front-end module (FEM).
For 868 MHz, it is also possible to use an integrated passive component (IPC) instead of discrete components. See CC13xx/CC26xx Hardware Configuration and PCB Design Considerations for a list of IPCs possible to use.
7.3 Crystal¶
CC13xx has an internal capacitor array used as load capacitors for the crystal. This cap-array is possible to adjust, see chapter 6 in CC13xx/CC26xx Hardware Configuration and PCB Design Considerations.
Some CC13xx launchpads have load capacitors mounted and the internal load capacitors turned off to improve performance.
7.4 Reference Signal¶
CC13xx is designed to be able to use a (TCXO). Official support for TCXO and narrow band will be added, check on E2E to get the up to date status.
7.5 Additional Filtering¶
Not applicable for CC13xx. Please look for a reference design under the “Technical Documents” tab on the CC13xx page on ti.com.
7.6 Power Supply Decoupling¶
It is important that the power decoupling is done as in the reference design. In addition the network connected to the DCDC_SW pin should be done as close as possible to the reference design if the DCDC converter is used. Pay close attention to the grounding and to have a short as possible return path from the decoupling to the die paddle.
7.7 Antenna Considerations¶
Please take a look the CC-Antenna-DK2 and Antenna Measurements Summary for the latest recommended PCB antennas.
7.8 PCB Layout Recommendations¶
The layout considerations for CC1101 are also valid for CC13xx. See CC13xx/CC26xx Hardware Configuration and PCB Design Considerations for general hardware design guidelines. See the device datasheet, the reference designs and your manufacturer on solder paste coverage. See the CC13xx reference designs for the number of vias under the chip.
8 Configuration Overview¶
CC1101 is a transceiver where the transitions between the different states are controlled by a hardware module.
CC13xx is a wireless module where the radio is one of the peripherals. The states on CC1101 can therefore not be compared directly. The Power Management section in the device datasheet describe the main power modes.
The RF driver controls which state the RF core is in.
9 Configuration Software¶
It’s highly recommended to use the code export feature in SmartRF Studio to get the recommended settings.
For details, press help in SmartRF Studio and scroll down to “Command Code Export” in the contents pan.
10 4-wire Serial Configuration and Data Interface¶
CC1101 is programmed and controlled over a SPI interface. This section of the CC1101 datasheet covers how to use the SPI interface. The CC13xx is a wireless MCU and therefore is not directly controlled over an interface. Programming the CC13xx is done over the JTAG interface using XDS100V3, XDS110 or XDS200. The CC13xx or CC26xx LaunchPad has a built-in XDS110 that can be used to program the CC13xx on the Launchpad or on a custom board using either Flash Programmer 2 or UniFlash.
11 General Control and Status Pins¶
The pins described in this section of the CC1101 datasheet are related to the SPI interface controlling CC1101. Since CC13xx is controlled differently than CC1101, CC13xx doesn’t have the pin control described in this section of the CC1101 datasheet.
12 Data Rate Programming¶
On CC1101 the wanted data rate is set by writing to the MDMCFG3.DRATE_M and
MDMCFG4.DRATE_E registers. On CC13xx the data rate is set via the
CMD_PROP_RADIO_DIV_SETUP command. See 23-139 in the CC13x2 CC26x2 SimpleLink Wireless MCU Technical Reference Manual for details. It is
recommended to use SmartRF Studio to calculate the required values and export
the code. SmartRF Studio also contains a set of characterized settings for data
rates used in CC1101 systems.
13 Receiver Channel Filter Bandwidth¶
Receiver bandwidth is set via the CMD_PROP_RADIO_DIV_SETUP command.
On CC13xx or CC26xx the RX BW can’t be set independently of the data rate, the actual RX bandwidth is a function of the RF frequency.
Note
For datarates below 20 kbps the frequency tolerance will be low and the system will be difficult to use with crystals as reference. For CC13x0, see CC13x0 Low Data Rate Operation. CC13x2 has this patch built-in.
For a given RX bandwidth it’s only possible to use data rates within a certain range. SmartRF Studio will give a warning if the combination you try to use is not possible.
14 Demodulator, Symbol Synchronizer and Data Decision¶
14.1 Frequency Offset Compensation¶
When using (G)FSK and data rates under 500 kbps the frequency offset estimate is available as
fdev is the programmed deviation and has unit Hz.
DEMMAFC0[7:0] is on address 0x4004 51C0 and should be read after a packet is received. The result is a signed value. The snippets below shows the required code:
//frequency_dev is the deviation given in Hz.
static int16_t offset = 0;
rfc_CMD_READ_RFREG_t RF_cmdReadRfregFreqOffset =
{
.commandNo = 0x0601,
.address = 0x5154,
.value = 0,
};
// Place in the RX part of the code.
RF_runImmediateCmd(rfHandle, (uint32_t*)&RF_cmdReadRfregFreqOffset);
offset = (RF_cmdReadRfregFreqOffset.value) * frequency_dev/ 64;
On CC13xx it’s also possible to append the frequency offset to the received packet as extra status bytes.
Figure 32. Extra Status bytes format¶
To append freq offset information to the packet buffer, add the following to the override list:
(uint32_t)0x000488E3
To append LQI information to the packet buffer, add to the override list:
(uint32_t)0x000288E3
If both LQI and freq offset are wanted, add:
(uint32_t)0x000688E3
14.2 Bit Synchronization¶
From a user standpoint this is done in the same way on CC1101 and CC13xx.
14.3 Byte Synchronization¶
From a user standpoint this is done in the same way on CC1101 and CC13xx.
15 Packet Handling Hardware Support¶
15.1 Data Whitening¶
CC13xx can be set up to use the same whitening as CC1101 by setting
CMD_PROP_RADIO_DIV_SETUP.whitenMode = 0x1.
15.2 Packet Format¶
The CC13xx standard packet format shown in figure 23-9 in CC13x2 CC26x2 SimpleLink Wireless MCU Technical Reference Manual is the same packet format as used on CC1101, but the packet format on CC13xx is made more flexible.
The length of the preamble is possible to set in
CMD_PROP_RADIO_DIV_SETUP.nPreamByteswith the possibility to set the length of the preamble to most values between 1 and 32 byte in addition to 1 and 4 bit. See table 23-139 for details. On CC13xx it’s possible to use other preambles than 0xAA or 0x55.The preamble can be set using Overrides:
//Preamble: 0x33 (uint32_t) 0x33330043 //Preamble: 0xCC (uint32_t) 0xCCCC0043The length of the sync word is possible to set in
CMD_PROP_RADIO_DIV_SETUP.nSwBitswith the possibility to set number of bits from 8 to 32.
Note that the CC1101 sync search is purely bit based (the bits in the received data stream are compared one by one with the programmed sync word). CC13xx on the other hand uses a combination of correlator based sync search and a bit based search (strict sync search). A correlator based sync search compares patterns and does not limit sensitivity. This difference in how the CC1101 and CC13xx search for sync means that it’s not possible to accept 1 bit error per 16 bits on CC13xx as on CC1101 (MDMCFG2.SYNCMODE). Since the sync search on CC13xx doesn’t limit sensitivity there is no need for a 15/16 or 30/32 sync mode setting on CC13xx.
Note that by using CMD_PROP_RX_ADV it is possible to search for two
different sync words at the same time.
CMD_PROP_RXsupports up to 255 bytes payload,CMD_PROP_RX_ADVsupports unlimited length (CMD_PROP_RX_ADV.maxPktLen= 0).Fixed or variable packet length is set in
CMD_PROP_TX.bVarLen. When using variable packet length mode on CC1101, the length byte must be written to the TX FIFO. On the CC13xx, the length byte is not part of the packet but is set through the API (CMD_PROP_TX.pktLen).
15.3 Packet Filtering in Receive Mode¶
Address filtering can be enabled by setting CMD_PROP_RX.bChkAddress. The
received address is compared against CMD_PROP_RX.address0 and
CMD_PROP_RX.address1. CRC filtering can be enabled by setting CMD_PROP_RX.bUseCrc.
16 Modulation Formats¶
As of today CC13xx supports 2-(G)FSK and 4-(G)FSK. Contact TI if you need a different format.
17.1 Sync Word Qualifier¶
The sync word is selectable to have a length from 8 bits to 32 bits. This is set
in CMD_PROP_RADIO_DIV_SETUP.nSwBits.
The sync word threshold could be set with the following override:
HW_REG_OVERRIDE(0x5114,0xYYZZ)
where YY and ZZ is the threshold for the two correlators. For simplicity the two thresholds can be set equal. Higher value is stricter. The default sync threshold is given by:
If the received sync word has to be bit by bit equal to the programmed sync word, the word search is qualified as a strict sync word search.
17.2 Preamble Quality Threshold (PQT)¶
The CMD_PROP_CS command can be used to monitor the RF activity in a channel and return busy if a preamble is present.
If PQT gating of sync search is wanted CMD_PROP_RX_SNIFF has to be chained
(Conditional execution and chaining) with CMD_PROP_RX.
17.3 RSSI¶
If in Rx, the function RF_getRssi() returns the RSSI value. After
receiving a packet the radio will no longer be in RX mode unless bRepeatOk =
1. The RSSI of a received packet can be read from the rfc_propRxOutput_t
structure.
In the code, add:
static rfc_propRxOutput_t rxStatistics;
int8_t RSSIout;
// Under Modify CMD_PROP_RX command for application needs
RF_cmdPropRx.pOutput = (uint8_t*)&rxStatistics;
// Where you want to read out the RSSI in the code
RSSIout = rxStatistics.lastRssi;
17.4 Carrier Sense (CS)¶
The CMD_PROP_CS command can be used to monitor the RF activity in a channel and return busy if the RSSI is above a given threshold.
17.5 Clear Channel Assessment (CCA)¶
The rfListenBeforeTalk example in the SimpleLink CC13xx/CC26xx SDK shows how listen before talk (LBT) or CCA can be implemented.
17.6 Link Quality Indicator (LQI)¶
It is not possible to output the LQI via the rfc_propRxOutput_t structure or
to append it to the packet meta data.
The LQI for the last received packet when using genfsk can be read from a register if the RF core is not in RX.:
static uint8_t LQI = 0;
rfc_CMD_READ_RFREG_t RF_cmdReadLQI =
{
.commandNo = 0x0601,
.address = 0x5268,
.value = 0,
};
RF_runImmediateCmd(rfHandle, (uint32_t*)&RF_cmdReadLQI);
LQI = (RF_cmdReadLQI.value);
18.1 Forward Error Correction (FEC)¶
The patch required for the CC1101 compatible FEC on CC13xx is not tested. Contact TI if you are interested in using a CC1101 compatible FEC on CC13xx.
19.1 Power-On Start-Up Sequence¶
The CC13xx has a build in POR/ brown out detector (BOD) that ensures that the chip does not boot up before VDDS is above the set minimum voltage (see 4.9 Power-On Reset). The chip also has an external reset pin. Follow the reference design for an external circuit that ensures a pin reset at power-up.
19.2 Crystal Control¶
The high speed XOSC is controlled by the drivers. A user doesn’t need to write code that directly controls the high speed XOSC.
19.3 Voltage Regulator Control¶
The voltage regulators are controlled by the chip.
19.4 Active Modes (RX and TX)¶
The RF core has two active states, RX and TX.
The
CMD_PROP_TXandCMD_PROP_TX_ADVcommands set the radio in TX sending a packet(s) placed in the packet (or TX) queue the command points to.The
CMD_TX_TESTsets the radio in TX and a carrier wave (CW) or a 16 bit Tx word is sent continuously until theendTriggeror an abort command is issued.The
CMD_PROP_RXandCMD_PROP_RX_ADVcommands set the the radio in Rx to receive a packet. The command exits Rx when theendTriggeris reached or a packet is received (optional).The CMD_PROP_CS command sets the radio in RX to check if the RSSI is above a threshold or if a preamble is detected (Preamble Quality Threshold, PQT).
The
CMD_PROP_RX_SNIFFandCMD_PROP_RX_ADV_SNIFFset the radio in Rx and combines the CMD_PROP_CS with normal packet reception.The
CMD_RX_TESTsets the radio in RX for test purposes.
The CMD_PROP_RADIO_SETUP and CMD_FS commands have to be issued before
sending one of the commands above to start and calibrate the voltage controlled
oscillator (VCO)/ phase locked loop (PLL), turn on the needed clocks, do
patching and to configure the radio.
The radio commands are described in section 23 in the CC13x2 CC26x2 SimpleLink Wireless MCU Technical Reference Manual. Some information can also be found in the description of the RF Core .
19.5 Wake On Radio (WOR)¶
Wake On Radio is shown in the example rfWakeOnRadioRx. This example uses
the CMD_PROP_RX_SNIFF command.
19.6 Timing¶
The MCU timing is given in “Timing and Switching Characteristics” section in the device datasheet. The time to turn on the radio code and go either to RX or TX or TX <-> RX is not fixed. Part of the time is related to software and therefore the time will be dependent on how many and which patches are used. To get an accurate number the timing should be measured with the software intended to run on the device. The signal routing intended to control an external LNA or PA could be used to measure the timing (see Routing RF Core Signals to Physical Pins).
19.7 RX Termination Timer¶
The CMD_PROP_RX and CMD_PROP_RX_ADV have endTime as a parameter.
Start and end triggers gives an overview over the possible triggers.
20 Data FIFO¶
Data queues are used for transferring packets from the RF core to the main CPU and vice versa. For documentation, see:
The software examples in the SDK
The “Data Queue Usage” in the Radio chapter in CC13x2 CC26x2 SimpleLink Wireless MCU Technical Reference Manual.
21 Frequency Programming¶
The RF frequency needs to be given as input to two commands:
CMD_PROP_RADIO_DIV_SETUP:
centerFreq: Center frequency of the band.
CMD_FS: Sets up the frequency synthesizer, described in the “Radio core HAL” sub chapter in CC13x2 CC26x2 SimpleLink Wireless MCU Technical Reference Manual.
- The frequency is given in two parts:
frequency: Given in MHz
fractFreq: Fractional part of the frequency
If the frequency given in the CMD_FS command is different from the frequency
given in the CMD_PROP_RADIO_DIV_SETUP command some parameters parameters
will have been calculated with a relative error of up to: (freq - centerFreq)/ centerFreq.
Deviation is one of the parameters that will be scaled with this factor. If this
error is acceptable it is possible to do frequency hopping in the 863 MHz - 870
MHz band by setting the center frequency in the middle of the band, 867 MHz,
using CMD_PROP_RADIO_DIV_SETUP once and the CMD_FS to set the frequencies
when hopping.
SmartRF Studio can be used to calculate the frequency word.
22 Voltage-Controlled Oscillator (VCO)¶
The CMD_FS command starts and calibrate the VCO. On CC13xx a CMD_FS
has to be run for every frequency. It is not possible to pre-calibrate each
channel.
23 Voltage Regulators¶
As with the CC1101, the CC13xx contains internal regulators that are invisible for customers.
The battery voltage on CC13xx is called VDDS (allowed level 1.8 V to 3.8 V). The output of the global low-dropout regulator (LDO)/ internal DCDC converter is called VDDR. When the DCDC is in use the VDDR net should not be connected to anything else than the external components shown in the reference designs. The Power Supply System is described in more detail in 1.3.13 in the CC13x2 CC26x2 SimpleLink Wireless MCU Technical Reference Manual.
Note that on CC13xx it is possible to run different DIO segments on different voltages; see 11.10.2 Digital Input/ Output Power Domains in the CC13x2 CC26x2 SimpleLink Wireless MCU Technical Reference Manual.
24 Output Power Programming¶
The wanted output power is set in CMD_PROP_RADIO_DIV_SETUP.txPower. Max
output power is dependent on the setting in The Customer Configuration (CCFG).
Most PAs have temperature dependent output power. On CC13xx it is possible to compensate for the temperature dependency and get an output power that is close to independent of temperature. The txPower settings found in SmartRF Studio contain the temperature compensation. This compensation is only valid for boards that follow our reference design closely. If a custom board does not follow the reference design the output power will be different and the temperature compensation coefficients have to be calculated for the custom board. See the description under CMD_SET_TX_POWER in the CC13x2 CC26x2 SimpleLink Wireless MCU Technical Reference Manual for equations.
25 Shaping and PA Ramping¶
When using (G)FSK PA ramping is included in the examples.
26 General Purpose / Test Output Control Pins¶
Signal routing describes how to get some internal signal available on external pins.
Packet format contains some more information on how to use of the internal signals to debug packet formats.
27 Asynchronous and Synchronous Serial Operation¶
An asynchronous signal (MCE_GPO1) is available in RX, see Routing RF Core Signals to Physical Pins. This signal is the sign of the instantaneous frequency. This signal is used as input to further data processing and therefore measuring PER will give better sensitivity compared to looking at the asynchronous output.
It is only possible to get one signal from the RF core. It is therefore not possible to generate a clock at the same time as getting the data out.
For Tx it is not possible to apply an external bit stream to CC13xx to be sent
on the air. By using the TX buffer and the CMD_PROP_TX/ CMD_PROP_TX_ADV
commands it is possible to generate the data wanted to send. It is not possible
to turn off preamble (minimum 1 bit) and sync (minimum 8 bit). If the protocol
is not using a sync word the sync word can be set equal to the first 8 bit of
the payload.
28.2 Frequency Hopping and Multi-Channel Systems¶
The 15.4 Stack shows how frequency hopping can be implemented. On CC13xx a
CMD_FS has to be run for every frequency. It is not possible to
pre-calibrate each channel.
28.3 Wide-band Modulation when not Using Spread Spectrum¶
An application note will be released to cover this.
28.4 Wireless MBUS¶
CC13x0 and CC13x2 have full support for C, T and S mode. Download and documentation is available at Wireless M-Bus Protocol Software.
28.7 Battery Operated Systems¶
CC13xx is designed to be used in battery operated system with very low standby current and low active current. The drivers ensure that the chip is in the state that gives lowest power consumption at any given time.
28.8 Increasing Range¶
For increased range (better sensitivity and higher output power), CC13xx can be used together with CC1190 (CC1190 Datasheet). See Using CC1190 Front End With CC13xx Under EN300220 and Using CC1190 Front End With CC13xx Under FCC 15.247.
29 Configuration Registers¶
On CC1101 writing/ reading registers are required to operate the chip. On CC13xx the control of the radio core is done by using drivers and APIs. Therefore no description is given of registers on CC13xx.