Data Fields
TimestampP_Format Union Reference

#include <TimestampP.h>

Data Fields

struct {
   uint32_t   fracBytes:4
 
   uint32_t   intBytes:4
 
   uint32_t   exponent:8
 
   int32_t   multiplier:16
 
format
 
uint32_t value
 

Field Documentation

§ fracBytes

uint32_t TimestampP_Format::fracBytes

§ intBytes

uint32_t TimestampP_Format::intBytes

§ exponent

uint32_t TimestampP_Format::exponent

§ multiplier

int32_t TimestampP_Format::multiplier

§ format

struct { ... } TimestampP_Format::format

§ value

uint32_t TimestampP_Format::value

The documentation for this union was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale