#include <TaskP.h>
|
char * | name |
|
void * | arg |
|
int | priority |
|
size_t | stackSize |
|
void * | stack |
| Task stack pointer. NULL should be used when calling TaskP_create. A pointer to a current stack should be passed for TaskP_construct. Default: NULL. More...
|
|
§ name
§ arg
Task function argument. Default: NULL
§ priority
int TaskP_Params::priority |
Task priority. Higher values represent higher priorities. Default: 0
§ stackSize
size_t TaskP_Params::stackSize |
Task stack size. Default: TaskP_DEFAULT_STACK_SIZE
§ stack
void* TaskP_Params::stack |
Task stack pointer. NULL should be used when calling TaskP_create. A pointer to a current stack should be passed for TaskP_construct. Default: NULL.
The documentation for this struct was generated from the following file: