Basic MutexP Parameters. More...
#include <MutexP.h>
Data Fields | |
void(* | callback )(void) |
Basic MutexP Parameters.
Structure that contains the parameters are passed into MutexP_create when creating a MutexP instance. The MutexP_Params_init function should be used to initialize the fields to default values before the application sets the fields manually. The MutexP default parameters are noted in MutexP_Params_init.
void(* MutexP_Params::callback) (void) |
Callback while waiting for mutex unlock