Data Fields
LogSinkBuf_Instance Struct Reference

#include <LogSinkBuf.h>

Collaboration diagram for LogSinkBuf_Instance:
Collaboration graph
[legend]

Data Fields

uint8_t bufType
 
int8_t advance
 
uint16_t numEntries
 
uint32_t serial
 
LogSinkBuf_Recbuffer
 
LogSinkBuf_ReccurEntry
 
LogSinkBuf_RecendEntry
 

Field Documentation

§ bufType

uint8_t LogSinkBuf_Instance::bufType

§ advance

int8_t LogSinkBuf_Instance::advance

§ numEntries

uint16_t LogSinkBuf_Instance::numEntries

§ serial

uint32_t LogSinkBuf_Instance::serial

§ buffer

LogSinkBuf_Rec* LogSinkBuf_Instance::buffer

§ curEntry

LogSinkBuf_Rec* LogSinkBuf_Instance::curEntry

§ endEntry

LogSinkBuf_Rec* LogSinkBuf_Instance::endEntry

The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale